EAGLE User Support (English) Pad with two holes
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
  • State Not Answered
  • Replies 2 replies
  • Subscribers 178 subscribers
  • Views 816 views
  • Users 0 members are here
  • pads
  • holes
Related

Pad with two holes

Former Member
Former Member over 10 years ago

A simple question but I cannot find an answer, so I hope someone can help.

I have a vertical 20mm PCB mount fuse. It has 4 through-hole pins, connected in two pairs. Can I make a pad with two holes but one schematic connection?

(RS Components 384-083)

 

many thanks

  • Sign in to reply
  • Cancel

Top Replies

  • autodeskguest
    autodeskguest over 10 years ago +1
    On 22/05/2015 7:29 p.m., simon hewitt wrote: A simple question but I cannot find an answer, so I hope someone can help. I have a vertical 20mm PCB mount fuse. It has 4 through-hole pins, connected in two…
  • clem57
    0 clem57 over 10 years ago

    You could extend one and join a second to that one on one side. Repeat for the other pair. schematic solved. But I think the board will still have four holes, Curious what purpose do you have?

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago

    On 22/05/2015 7:29 p.m., simon hewitt wrote:

    A simple question but I cannot find an answer, so I hope someone can

    help.

    I have a vertical 20mm PCB mount fuse. It has 4 through-hole pins,

    connected in two pairs. Can I make a pad with two holes but one

    schematic connection?

    (RS Components 384-083)

     

    many thanks

     

    Hi Simon

     

    Yes you can.

    Create your library package and symbol.

    Then start to build the device.

    When you come to connecting the pins to the pads you connect one pad to

    a pin and then 'append the second pad to the same pin. Repeat for the

    other end of the fuse.

     

    Have a look at the manual that comes with Eagle. In the doc folder.

    Section 8.4 One Pin – Multiple Pads Connections

     

    HTH

    Warren