EAGLE User Support (English) Pad with two holes
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
  • State Not Answered
  • Replies 2 replies
  • Subscribers 179 subscribers
  • Views 824 views
  • Users 0 members are here
  • pads
  • holes
Related

Pad with two holes

Former Member
Former Member over 10 years ago

A simple question but I cannot find an answer, so I hope someone can help.

I have a vertical 20mm PCB mount fuse. It has 4 through-hole pins, connected in two pairs. Can I make a pad with two holes but one schematic connection?

(RS Components 384-083)

 

many thanks

  • Sign in to reply
  • Cancel

Top Replies

  • autodeskguest
    autodeskguest over 10 years ago +1
    On 22/05/2015 7:29 p.m., simon hewitt wrote: A simple question but I cannot find an answer, so I hope someone can help. I have a vertical 20mm PCB mount fuse. It has 4 through-hole pins, connected in two…
Parents
  • autodeskguest
    0 autodeskguest over 10 years ago

    On 22/05/2015 7:29 p.m., simon hewitt wrote:

    A simple question but I cannot find an answer, so I hope someone can

    help.

    I have a vertical 20mm PCB mount fuse. It has 4 through-hole pins,

    connected in two pairs. Can I make a pad with two holes but one

    schematic connection?

    (RS Components 384-083)

     

    many thanks

     

    Hi Simon

     

    Yes you can.

    Create your library package and symbol.

    Then start to build the device.

    When you come to connecting the pins to the pads you connect one pad to

    a pin and then 'append the second pad to the same pin. Repeat for the

    other end of the fuse.

     

    Have a look at the manual that comes with Eagle. In the doc folder.

    Section 8.4 One Pin – Multiple Pads Connections

     

    HTH

    Warren

     

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 10 years ago

    On 22/05/2015 7:29 p.m., simon hewitt wrote:

    A simple question but I cannot find an answer, so I hope someone can

    help.

    I have a vertical 20mm PCB mount fuse. It has 4 through-hole pins,

    connected in two pairs. Can I make a pad with two holes but one

    schematic connection?

    (RS Components 384-083)

     

    many thanks

     

    Hi Simon

     

    Yes you can.

    Create your library package and symbol.

    Then start to build the device.

    When you come to connecting the pins to the pads you connect one pad to

    a pin and then 'append the second pad to the same pin. Repeat for the

    other end of the fuse.

     

    Have a look at the manual that comes with Eagle. In the doc folder.

    Section 8.4 One Pin – Multiple Pads Connections

     

    HTH

    Warren