EAGLE User Support (English) Trying to identify connectors but failing
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
  • State Not Answered
  • Replies 4 replies
  • Subscribers 180 subscribers
  • Views 877 views
  • Users 0 members are here
  • connector
Related

Trying to identify connectors but failing

Former Member
Former Member over 10 years ago

I have two connectors that I need to source and I cannot figure out what they are or who makes them.

image

This one is an LVDS connector which mates to a small touchscreen. It has a 1mm pitch.

 

image

This one is a backlight connector for the same screen. It has a 1.4mm pitch. I cannot for the life of me find anyone who knows what they are. I've even given the cables in the hands of a cable manufacturer to take away and examine and I received a no quote from them.

 

Any ideas?

  • Sign in to reply
  • Cancel
  • shabaz
    0 shabaz over 10 years ago

    For laptop screens check hirose and molex product pages, they are likely candidates. At 1mm pitch the connectors are near impossible to crimp or even solder, without the correct tools (which cost many hundreds of dollars).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to shabaz

    YEs, I jave contacted Molex and Hirose directly and provided them with these pictures. No luck.

    crimp tools are only a couple hundred dollars, this isn't a hobbyist appllication.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to Former Member

    On 12/06/2015 2:05 p.m., Leigh Brady wrote:

    YEs, I jave contacted Molex and Hirose directly and provided them with

    these pictures. No luck.

    crimp tools are only a couple hundred dollars, this isn't a hobbyist

    appllication.

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/152390

     

     

      A quick google to this link gives  the top ten

    http://www.connectorsupplier.com/2012-top-10-connector-manufacturers-090313/

     

    Give some of them a try

     

    All the best

    Warren

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago

    On 11.06.2015 20:05, Leigh Brady wrote:

    I have two connectors that I need to source and I cannot figure out what

    they are or who makes them.

     

    This one is an LVDS connector which mates to a small touchscreen. It has

    a 1mm pitch.

     

     

    This one is a backlight connector for the same screen. It has a 1.4mm

    pitch. I cannot for the life of me find anyone who knows what they are.

    I've even given the cables in the hands of a cable manufacturer to take

    away and examine and I received a no quote from them.

     

    Any ideas?

     

    There is usually a tiny logo on these plugs that can be identified. have

    you got a cheap usb microscope you can look closer with? I would also

    like to see a pic of the locking mechanism.

     

    Have a look at molex. (Are you sure its not 1.25mm pitch? They look like

    a picoblade) They do have some 1mm pitch for the pico-lock system, but

    they seem to stop at 12 pins..

     

    Or I would just google images for lcd lvds plug or connector and see

    what pops up. Since this looks kinda low speed lvds, I'd try ebay as well.