EAGLE User Support (English) Trying to identify connectors but failing
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
  • State Not Answered
  • Replies 4 replies
  • Subscribers 180 subscribers
  • Views 879 views
  • Users 0 members are here
  • connector
Related

Trying to identify connectors but failing

Former Member
Former Member over 10 years ago

I have two connectors that I need to source and I cannot figure out what they are or who makes them.

image

This one is an LVDS connector which mates to a small touchscreen. It has a 1mm pitch.

 

image

This one is a backlight connector for the same screen. It has a 1.4mm pitch. I cannot for the life of me find anyone who knows what they are. I've even given the cables in the hands of a cable manufacturer to take away and examine and I received a no quote from them.

 

Any ideas?

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 10 years ago

    On 11.06.2015 20:05, Leigh Brady wrote:

    I have two connectors that I need to source and I cannot figure out what

    they are or who makes them.

     

    This one is an LVDS connector which mates to a small touchscreen. It has

    a 1mm pitch.

     

     

    This one is a backlight connector for the same screen. It has a 1.4mm

    pitch. I cannot for the life of me find anyone who knows what they are.

    I've even given the cables in the hands of a cable manufacturer to take

    away and examine and I received a no quote from them.

     

    Any ideas?

     

    There is usually a tiny logo on these plugs that can be identified. have

    you got a cheap usb microscope you can look closer with? I would also

    like to see a pic of the locking mechanism.

     

    Have a look at molex. (Are you sure its not 1.25mm pitch? They look like

    a picoblade) They do have some 1mm pitch for the pico-lock system, but

    they seem to stop at 12 pins..

     

    Or I would just google images for lcd lvds plug or connector and see

    what pops up. Since this looks kinda low speed lvds, I'd try ebay as well.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 10 years ago

    On 11.06.2015 20:05, Leigh Brady wrote:

    I have two connectors that I need to source and I cannot figure out what

    they are or who makes them.

     

    This one is an LVDS connector which mates to a small touchscreen. It has

    a 1mm pitch.

     

     

    This one is a backlight connector for the same screen. It has a 1.4mm

    pitch. I cannot for the life of me find anyone who knows what they are.

    I've even given the cables in the hands of a cable manufacturer to take

    away and examine and I received a no quote from them.

     

    Any ideas?

     

    There is usually a tiny logo on these plugs that can be identified. have

    you got a cheap usb microscope you can look closer with? I would also

    like to see a pic of the locking mechanism.

     

    Have a look at molex. (Are you sure its not 1.25mm pitch? They look like

    a picoblade) They do have some 1mm pitch for the pico-lock system, but

    they seem to stop at 12 pins..

     

    Or I would just google images for lcd lvds plug or connector and see

    what pops up. Since this looks kinda low speed lvds, I'd try ebay as well.