Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Using exp-lbrs.ulp
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 187 subscribers
  • Views 1328 views
  • Users 0 members are here
  • eagle
  • library
  • question
Related

Using exp-lbrs.ulp

electrodevab
electrodevab over 11 years ago

Hi,

 

I have just exported all the used devices in a schematic to a single library using the exp-lbrs.ulp program

It seems to work ok. (I can see the new library and its content)

 

After this, when I right-click a component in the schematic editor and select "Open device", I would like to open the device in the newly created directory. Unfortunately the device that is opened is the device in the original library.

 

Can you please advice on how to link the schematics' devices to the newly created library?

 

Best regards

 

Tomas

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 6/23/2015 3:07 AM, Tomas Bergh wrote:

    Hi,

     

    I have just exported all the used devices in a schematic to a single

    library using the exp-lbrs.ulp program

    It seems to work ok. (I can see the new library and its content)

     

    After this, when I right-click a component in the schematic editor and

    select "Open device", I would like to open the device in the newly

    created directory. Unfortunately the device that is opened is the device

    in the original library.

     

     

    Hi Tomas,

     

    I hope you're doing well. When you do a right-click Open device it

    always assumes the library is in the LBR directory. There's no way to

    specify any other location. Once the part is in the schematic it

    maintains no other association to the library other than the library

    name and device name.

     

    To be safe you need to open the library you want to use specifically

    make the changes and then do an update using that library.

     

    Let me know if there's anything else I can do for you.

     

    Best Regards,

    Jorge Garcia

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • electrodevab
    0 electrodevab over 11 years ago in reply to autodeskguest

    Hi Jorge,

    Thank you for the answer.

     

    I also tried to mark the original libraries with "Use none" with hope of that Eagle would choose the created library. What is the purpose of the "Use" and "Use none"?

     

    What is then the purpose of exp-lbrs.ulp if I cannot use the extracted/created library?

     

    Best regards,

     

    Tomas Bergh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • electrodevab
    0 electrodevab over 11 years ago in reply to autodeskguest

    Hi Jorge,

    Thank you for the answer.

     

    I also tried to mark the original libraries with "Use none" with hope of that Eagle would choose the created library. What is the purpose of the "Use" and "Use none"?

     

    What is then the purpose of exp-lbrs.ulp if I cannot use the extracted/created library?

     

    Best regards,

     

    Tomas Bergh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • electrodevab
    0 electrodevab over 11 years ago in reply to autodeskguest

    Hi Richard,

     

    Ok, thanks for your effort!

     

    The only way I can think of is to export the library and modify the part in the exported lib and then use the replace command. Unfortunately this is quite an effort when modifying a whole design.

     

    Thanks,

     

    Have a nice day,

     

    Best regards,

     

    Tomas Bergh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to electrodevab

    Am 24.06.2015 um 08:11 schrieb Tomas Bergh:

    Hi Jorge,

    Thank you for the answer.

     

    I also tried to mark the original libraries with "Use none" with hope of

    that Eagle would choose the created library. What is the purpose of the

    "Use" and "Use none"?

     

    What is then the purpose of exp-lbrs.ulp if I cannot use the

    extracted/created library?

     

    Best regards,

     

    Tomas Bergh

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/153453

     

     

     

    Hi,

     

    with the USE command you can decide which libraries are available

    for ADD. Only libraries in use are visible in the ADD dialog and

    will be available for the search function.

     

    exp-lbrs.ulp is usefull if you have a board or schematic but not

    oroginal the library files. In case you have to do a redesign, for

    example. If you have to change the library definition of one of

    the components, it's good to export from the project files, modify

    the exported libraries and then perform a "library update" in board

    and schematic.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/