Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) How do I create a label on a net
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Answers 1 answer
  • Subscribers 191 subscribers
  • Views 12952 views
  • Users 0 members are here
Related

How do I create a label on a net

Workshopshed
Workshopshed over 11 years ago

I'm happy in naming nets so that they join up but is it possible to create little "tags" or "labels" on the pins as in this example below?

 

image

  • Sign in to reply
  • Cancel
Parents
  • balearicdynamics
    0 balearicdynamics over 11 years ago

    Hello Andy,

     

    I had the same problem too. Naming the nets is useful and I use this method just to have the right coherence in while routing the PCB layout with the advantage to make blocks on the schematics. Well, I usually name the nets, then I put the "name" feature on the wire. It seem that the tag labels are components of the Eagle library but it is a lot I have not used them so I don't remember what library is. At least this is the method I have used when I needed. Maybe there is a script of a function easier but I don't know. Interesting discussion for all I think.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • balearicdynamics
    0 balearicdynamics over 11 years ago

    Hello Andy,

     

    I had the same problem too. Naming the nets is useful and I use this method just to have the right coherence in while routing the PCB layout with the advantage to make blocks on the schematics. Well, I usually name the nets, then I put the "name" feature on the wire. It seem that the tag labels are components of the Eagle library but it is a lot I have not used them so I don't remember what library is. At least this is the method I have used when I needed. Maybe there is a script of a function easier but I don't know. Interesting discussion for all I think.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • Workshopshed
    0 Workshopshed over 11 years ago in reply to balearicdynamics

    Yes, I've just done them like this. But it would be nice if they used the other symbol which seems to be quite standard.