Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) How do I create a label on a net
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Answers 1 answer
  • Subscribers 191 subscribers
  • Views 12953 views
  • Users 0 members are here
Related

How do I create a label on a net

Workshopshed
Workshopshed over 11 years ago

I'm happy in naming nets so that they join up but is it possible to create little "tags" or "labels" on the pins as in this example below?

 

image

  • Sign in to reply
  • Cancel
Parents
  • balearicdynamics
    0 balearicdynamics over 11 years ago

    Hello Andy,

     

    I had the same problem too. Naming the nets is useful and I use this method just to have the right coherence in while routing the PCB layout with the advantage to make blocks on the schematics. Well, I usually name the nets, then I put the "name" feature on the wire. It seem that the tag labels are components of the Eagle library but it is a lot I have not used them so I don't remember what library is. At least this is the method I have used when I needed. Maybe there is a script of a function easier but I don't know. Interesting discussion for all I think.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Workshopshed
    0 Workshopshed over 11 years ago in reply to balearicdynamics

    Yes, I've just done them like this. But it would be nice if they used the other symbol which seems to be quite standard.

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Workshopshed
    0 Workshopshed over 11 years ago in reply to balearicdynamics

    Yes, I've just done them like this. But it would be nice if they used the other symbol which seems to be quite standard.

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • dukepro
    0 dukepro over 8 years ago in reply to robvei45

    On 8/9/18 18:51, robert veitch wrote:

    "mistery", really?? That's mystery image

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/243138

     

     

    It could be that he had a "t" where it shouldn't have been - misery.

     

    Anyway... try the "Label" command, then click on the net.  For the

    fancier off-page reference, try "Label xref" and click on the net.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • robvei45
    0 robvei45 over 8 years ago in reply to balearicdynamics

    "mistery", really?? That's mystery image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Workshopshed
    0 Workshopshed over 11 years ago in reply to Workshopshed

    Brilliant, gave it a quick go, need to give it a bit of practice but looks to be the real thing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 11 years ago in reply to Workshopshed

    Andy, mistery solved !!! image

     

    You (and me too) were wrong as we was searching for a "label", something different than the net's name. Instead Eagle try to be flexible but as much as possible linear in every feature. Observing the things in this way, first of all it is almost logic that if the nets has the name property, giving the option to connect them logically keeping the integrity of the wires routing in the layout side, the solution should be searched just there: in the net name. After this the procedure is very simple:

     

    Select the label button in the vertical toolbar of the schematics view

    image

    At this point the top horizontal button bar shows the net naming options.

    image

    The immeditate two buttons to the right of the selectable layer dropdown list, you can decide if you want the label appearing along the wire or at the end as shown in the image below.

    image

    Note that exactly as the other (default) kind of label you can move the cursor before confirming to decide where it should be positioned (hopefully to one of the end of the wire) as shown in the examples below.

    imageimageimage

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer