EAGLE User Support (English) Autorouter not working
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
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 178 subscribers
  • Views 476 views
  • Users 0 members are here
Related

Autorouter not working

Former Member
Former Member over 10 years ago

I had to switch to a PIC18F87K22 80 pin QFP  from an 18F67K22 64 pin QFP.  I had no issues with the autorouter and the 64 pin device.  With the 80 pin QFP the router makes no attempt to route the pins.  I am at version 7.3.0 and the default router settings.  This was happening using the 7.2.0 version.  The libraries came from the Cadsoft download site.  I hope I just have some setting wrong.  Can someone help?  Thanks.  Juan M. Nuncio

  • Sign in to reply
  • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago

    Am 03.07.2015 um 17:59 schrieb Juan Nuncio:

    I had to switch to a PIC18F87K22 80 pin QFP  from an 18F67K22 64 pin

    QFP.  I had no issues with the autorouter and the 64 pin device.  With

    the 80 pin QFP the router makes no attempt to route the pins.  I am at

    version 7.3.0 and the default router settings.  This was happening using

    the 7.2.0 version.  The libraries came from the Cadsoft download site.

    I hope I just have some setting wrong.  Can someone help?  Thanks.  Juan

    M. Nuncio

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/154064

     

     

     

    Maybe it's a matter of the routing grid.

    for a first check please run the Design Rule Check. Does it report

    errors in the area of your QFP 80? If yes, it's clear why the Autorouter

    can't connect. Please check the Design rule and Net class settings....

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

    Please use the original CadSoft forum at news.cadsoft.de.

    Proper posts and reliable file attachments are taken granted.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago

    That was it.  Changed the routing grid and that fixed it.  Thanks!!!

     

    Juan M. Nunciol