EAGLE User Support (English) Autorouter not working
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
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 178 subscribers
  • Views 475 views
  • Users 0 members are here
Related

Autorouter not working

Former Member
Former Member over 10 years ago

I had to switch to a PIC18F87K22 80 pin QFP  from an 18F67K22 64 pin QFP.  I had no issues with the autorouter and the 64 pin device.  With the 80 pin QFP the router makes no attempt to route the pins.  I am at version 7.3.0 and the default router settings.  This was happening using the 7.2.0 version.  The libraries came from the Cadsoft download site.  I hope I just have some setting wrong.  Can someone help?  Thanks.  Juan M. Nuncio

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 10 years ago

    That was it.  Changed the routing grid and that fixed it.  Thanks!!!

     

    Juan M. Nunciol

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 10 years ago

    That was it.  Changed the routing grid and that fixed it.  Thanks!!!

     

    Juan M. Nunciol