EAGLE User Support (English) How can I change the width of thermal ties
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
  • Replies 7 replies
  • Subscribers 179 subscribers
  • Views 2241 views
  • Users 0 members are here
Related

How can I change the width of thermal ties

autodeskguest
autodeskguest over 16 years ago

By "thermal ties" I mean the copper that connects a pad to a copper pour.

I have a situation with a 0805 chip resistor:

  • the left pad is connected to an 8-mil trace coming into the pad and to an

8-mil trace exiting the pad.

  • the right pad connects to the GND polygon, with 3 16~18-mil traces. 

So this means that there is a LOT more copper on the right end of the

resistor.  I have read that in this type of situation when the board is

reflow soldered that the part can get pulled over to one pad and make poor

connection to the other pad, or that the part can "tombstone".  If what

I've read is correct, how do I make the copper (thermal) ties on the right

pad, narrower?  I played with DRC/Supply values, with no success.

 

BTW, I'd gladly post a pic of a portion of my board, but I don't know how

to save a portion of the board as a graphic.  I use EAGLE v5.6.0 and Win

XP/sp3.

-Dave Pollum

 

 

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    Former Member over 16 years ago

    You can also change the width of the polygon, but this will affect all

    thermals

    r

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 16 years ago

    You can also change the width of the polygon, but this will affect all

    thermals

    r