By "thermal ties" I mean the copper that connects a pad to a copper pour.
I have a situation with a 0805 chip resistor:
the left pad is connected to an 8-mil trace coming into the pad and to an
8-mil trace exiting the pad.
the right pad connects to the GND polygon, with 3 16~18-mil traces.
So this means that there is a LOT more copper on the right end of the
resistor. I have read that in this type of situation when the board is
reflow soldered that the part can get pulled over to one pad and make poor
connection to the other pad, or that the part can "tombstone". If what
I've read is correct, how do I make the copper (thermal) ties on the right
pad, narrower? I played with DRC/Supply values, with no success.
BTW, I'd gladly post a pic of a portion of my board, but I don't know how
to save a portion of the board as a graphic. I use EAGLE v5.6.0 and Win
XP/sp3.
-Dave Pollum