Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Triac track width and clearance advices?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 188 subscribers
  • Views 1853 views
  • Users 0 members are here
Related

Triac track width and clearance advices?

autodeskguest
autodeskguest over 17 years ago

Hi,

 

I�m making the layout for a PCB that uses a triac in TO-220 package. The maximum current in the triac (BTA312Y) is 8 Amp. and the copper thickness 35�m (1 oz/ft2). What track width would you recommend? I�ve seen calculators on the Internet but they ask the allowable temperature rise and I don�t know what value I can choose. On the other hand, I�ve seen that IPC recommends 220mil for 8 Amp., 10�C rise and 1oz/ft2 Cu but it�s very big?

 

What value do you use for track clearance for 220V mains voltages?  I�ve seen 0.75mm (http://www.electronics-project-design.com/PCB-Design.html ) for coated board. But here (http://www.smpspowersupply.com/ipc2221pcbclearance.html ) the values are not the same and I don�t know what to use? Is bare board for PCB without parts on it? So do I have to use assembly and �external components leads, uncoated� if : the board has a solder resist mask, is populated and if there is no coating on component leads?

Is the clearance also needed between the component�s pads (external diameter to external diameter)? If so, is it possible with a standard TO-220 package?

 

 

Thank you.

 

--

Browser access to CadSoft Support Forums at http://www.eaglecentral.ca

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    If your application has to work in low air pressure, such as in

    aviation, then the clearance specs require much wider spacing.  Low

    pressure air arcs over much easier than normal pressure air.

     

     

    Robert Scott

    Real-Time Specialties

    Ypsilanti, Michigan

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

    If your application has to work in low air pressure, such as in

    aviation, then the clearance specs require much wider spacing.  Low

    pressure air arcs over much easier than normal pressure air.

     

     

    Robert Scott

    Real-Time Specialties

    Ypsilanti, Michigan