Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Triac track width and clearance advices?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 188 subscribers
  • Views 1849 views
  • Users 0 members are here
Related

Triac track width and clearance advices?

autodeskguest
autodeskguest over 17 years ago

Hi,

 

I�m making the layout for a PCB that uses a triac in TO-220 package. The maximum current in the triac (BTA312Y) is 8 Amp. and the copper thickness 35�m (1 oz/ft2). What track width would you recommend? I�ve seen calculators on the Internet but they ask the allowable temperature rise and I don�t know what value I can choose. On the other hand, I�ve seen that IPC recommends 220mil for 8 Amp., 10�C rise and 1oz/ft2 Cu but it�s very big?

 

What value do you use for track clearance for 220V mains voltages?  I�ve seen 0.75mm (http://www.electronics-project-design.com/PCB-Design.html ) for coated board. But here (http://www.smpspowersupply.com/ipc2221pcbclearance.html ) the values are not the same and I don�t know what to use? Is bare board for PCB without parts on it? So do I have to use assembly and �external components leads, uncoated� if : the board has a solder resist mask, is populated and if there is no coating on component leads?

Is the clearance also needed between the component�s pads (external diameter to external diameter)? If so, is it possible with a standard TO-220 package?

 

 

Thank you.

 

--

Browser access to CadSoft Support Forums at http://www.eaglecentral.ca

 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 17 years ago

    take a look at this:

    http://www.haeusermann.at/2,product/14,HSMtec/15,Hochstrom--und-Waermemanagement-auf-der-Leiterplatte

     

    if it's in german, an english version is available

    r

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 17 years ago

    take a look at this:

    http://www.haeusermann.at/2,product/14,HSMtec/15,Hochstrom--und-Waermemanagement-auf-der-Leiterplatte

     

    if it's in german, an english version is available

    r