Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Panelizing boards for Manufacture (e.g. Olimex)
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 188 subscribers
  • Views 417 views
  • Users 0 members are here
Related

Panelizing boards for Manufacture (e.g. Olimex)

autodeskguest
autodeskguest over 17 years ago

I am thinking of trying Olimex for new boards

as they throw in the soldermask and silk and

dont ask for tooling charge.

 

Their service looks good, and they can do

160mm x 100mm for very cheap costs.

 

I would like to submit a panel of two boards

100 x 80, using Eagle.

 

Is this possible to make two boards into one

.BRD file for panelizing ?

 

Florian.

 

 

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    Thanks ! Both very helpfull posts.

    I guessed that I would need to reduce size

    by some two mm in each direction - but

    your confirmation was necessary.

     

    F

     

    "Nick de Smith" <nick@desmith.net> wrote in message

    news:h4mcbn$na9$1@cheetah.cadsoft.de...

    "Florian Schmoll" <asro6932@yahoo.com> wrote in message

    news:h4lacv$vqq$1@cheetah.cadsoft.de...

    Is this possible to make two boards into one

    .BRD file for panelizing ?

     

    You do't need to with Olimex - they do that for you. If you read their

    FAQ, you will see that you need to submit all your BRD files together with

    a small diagram showing how you'd like them panelised - in the case of one

    board duplicated or some similar simple layout, then I normally just write

    that in the readme.txt file that you have to send them. I've has dozens of

    boards done by them over the years like this.

     

    Do use their silk-screen checking ULP (on their web site).

     

    Note also that 2 x 80x100 board will NOT fit onto one 160x100 panel - you

    need a few mm between the board for the saw cut - 100x78 or 79 would be

    good. 100x80, not so good!

     

    Cheers

     

    Nick

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • nickds1
    nickds1 over 17 years ago

    "Florian Schmoll" <asro6932@yahoo.com> wrote in message

    news:h4lacv$vqq$1@cheetah.cadsoft.de...

    Is this possible to make two boards into one

    .BRD file for panelizing ?

     

    You do't need to with Olimex - they do that for you. If you read their FAQ,

    you will see that you need to submit all your BRD files together with a

    small diagram showing how you'd like them panelised - in the case of one

    board duplicated or some similar simple layout, then I normally just write

    that in the readme.txt file that you have to send them. I've has dozens of

    boards done by them over the years like this.

     

    Do use their silk-screen checking ULP (on their web site).

     

    Note also that 2 x 80x100 board will NOT fit onto one 160x100 panel - you

    need a few mm between the board for the saw cut - 100x78 or 79 would be

    good. 100x80, not so good!

     

    Cheers

     

    Nick

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 17 years ago

    Florian Schmoll schrieb:

    I am thinking of trying Olimex for new boards

    as they throw in the soldermask and silk and

    dont ask for tooling charge.

     

    Their service looks good, and they can do

    160mm x 100mm for very cheap costs.

     

    I would like to submit a panel of two boards

    100 x 80, using Eagle.

     

    Is this possible to make two boards into one

    ..BRD file for panelizing ?

     

    Florian.

     

     

     

     

    You can use the commands GROUP, CUT and PASTE to generate one big board:

     

    Open the board you want to put into the clipboard and use DISPLAY ALL

    first to activate all layers.

     

    Now:

    GROUP to select all elements

    CUT and a mouse click into the drawing puts it into

         the buffer

    EDIT the "target" layout

    PASTE it now

     

    The same can be done with several boards. Please be aware that the

    silk screen can change. The names of the parts on the layout must

    be unequivocal. Therefore the part names must be changed.

     

    If you need the silkscreen on your boards, you have to use

    panelize.ulp before.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

    CadSoft Support -- hotline@cadsoft.de

    FAQ: http://www.cadsoft.de/faq.htm