EAGLE User Support (English) Missing air wire
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
  • Replies 9 replies
  • Subscribers 177 subscribers
  • Views 727 views
  • Users 0 members are here
Related

Missing air wire

autodeskguest
autodeskguest over 16 years ago

I have a prety much completed board with everything routed and I forgot a connector. I have similar connectors in the schematic so I copied one of the others and placed it and made a connection to it. The second pin of the connector is ground so I copied a grond symbol from elsewhere in the schematic and connected it to the connector. On the board view only the air wire to the non-ground pin is showing. The ground pin has no air wire. All the other ground connections had air-wires before I routed them. I tried deleting the connector and starting over. The connection to ground in the schamatic appears complete becasue I can move the connector or the ground symbol and the connection follows.

I tried "redraw" on the board. No luck. If I try to put a trace on the board to make the ground connection to the connector pin it complains it cannot back annotate and it must be done on the schematic which I guess means the connection is not there.

 

So where is the connection?

 

Sage

 

 

--

Browser access to CadSoft Support Forums at http://www.eaglecentral.ca

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 16 years ago

    Ok. In the end that did it but I had to take the long way around.

     

    Since I didn't know when I was going to get an answer to my question I just placed a wire on the schematic from the connector pin to one of the other grounds as a work around insted of havingf a dedicated gnd for the pin. After I got your message I tried the rename command by selecting a wire on one of the ground connections and the command sucessfully changed all the N$26 nets to GND. But I had left the new connector pin still connected to the other ground. I disconnected that wire and placed a new ground symbol for the connector and connected it to the pin. It became N$22 and it would not rename. The error was something like cannot connect N$22 to GND.

    I had to go back to the other ground symbol and re-issue the command to rename ALL to GND even though the symbol I was working on was already GND from the last rename. It did change the new connection on the new GND symbol to GND net. So mission accomplished.

    Seems to me there a lot of wierd things like this that happen in Eagle that I guess you eventually remember how to work with but it's a bit frustrating for me as a first timer.

     

    THANKS for your help.

     

    Sage

    --

    Browser access to CadSoft Support Forums at http://www.eaglecentral.ca

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 16 years ago

    Ok. In the end that did it but I had to take the long way around.

     

    Since I didn't know when I was going to get an answer to my question I just placed a wire on the schematic from the connector pin to one of the other grounds as a work around insted of havingf a dedicated gnd for the pin. After I got your message I tried the rename command by selecting a wire on one of the ground connections and the command sucessfully changed all the N$26 nets to GND. But I had left the new connector pin still connected to the other ground. I disconnected that wire and placed a new ground symbol for the connector and connected it to the pin. It became N$22 and it would not rename. The error was something like cannot connect N$22 to GND.

    I had to go back to the other ground symbol and re-issue the command to rename ALL to GND even though the symbol I was working on was already GND from the last rename. It did change the new connection on the new GND symbol to GND net. So mission accomplished.

    Seems to me there a lot of wierd things like this that happen in Eagle that I guess you eventually remember how to work with but it's a bit frustrating for me as a first timer.

     

    THANKS for your help.

     

    Sage

    --

    Browser access to CadSoft Support Forums at http://www.eaglecentral.ca