I have a prety much completed board with everything routed and I forgot a connector. I have similar connectors in the schematic so I copied one of the others and placed it and made a connection to it. The second pin of the connector is ground so I copied a grond symbol from elsewhere in the schematic and connected it to the connector. On the board view only the air wire to the non-ground pin is showing. The ground pin has no air wire. All the other ground connections had air-wires before I routed them. I tried deleting the connector and starting over. The connection to ground in the schamatic appears complete becasue I can move the connector or the ground symbol and the connection follows.
I tried "redraw" on the board. No luck. If I try to put a trace on the board to make the ground connection to the connector pin it complains it cannot back annotate and it must be done on the schematic which I guess means the connection is not there.
So where is the connection?
Sage
--
Browser access to CadSoft Support Forums at http://www.eaglecentral.ca