Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Through hole pad definition
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 188 subscribers
  • Views 2054 views
  • Users 0 members are here
Related

Through hole pad definition

e14 Contributor
e14 Contributor over 16 years ago

Hi All,

 

In the wirepad through hole pad library the pads are described as 1,6/0,8

or 3,8/1,4 etc.

 

Is the meaning of these numbers defined?

 

Or even the capacitors lib has numbers. In this case it's easy to cross ref

to the capacitor type and see the hole spacing, diameter, etc.

 

Also, I did a library>use and selected a custom library. How do I get back

to having all the available libraries displayed again? Do I have to select

them one at a time?

 

Thanks,

Mac

--

Browser access to CadSoft Support Forums at http://www.eaglecentral.ca

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 16 years ago

    Mac schreef:

    Greg Erskine wrote on Fri, 11 December 2009 15:17

    "Mac" <suemac@empire.net[/email]> wrote in message

    news:hftitb$b1e$1@cheetah.cadsoft.de...[/email]

    Hi All,

     

    In the wirepad through hole pad library the pads are described as

    1,6/0,8

    or 3,8/1,4 etc.

     

    Is the meaning of these numbers defined?

     

    Diameter / drill sizes in mm.

     

    Or even the capacitors lib has numbers. In this case it's easy to

    cross > ref

    to the capacitor type and see the hole spacing, diameter, etc.

     

    Also, I did a library>use and selected a custom library. How do I

    get back

    to having all the available libraries displayed again? Do I have to

    select

    them one at a time?

     

     

    Use the Control panel. Try right-clicking on "Libraries" and/or the

    directories and libraries below it. Take note of the green/grey dot

    next to each library. You can click on that to. I find the control

    panel is a

    very powerful interface to control projects.

     

    http://www.eaglecentral.ca

     

    Yes, thanks, I know how to select libraries for use one at a time from a

    couple of different windows. I was looking for a way to say: "use them all"

    to get back to the way it was when Eagle was installed.

     

    As for the diameter and drill sizes...so is 1,6 metric speak for 1.6mm (US

    speak)? (I wish the world would agree on decimal points or commas...  image )

     

     

    Maybe the first answer was a bit unclear, but the procedure is correct.

    When you right-click on 'libraries' in the control panel, you can

    choose: "select all" or "select none". At least in 4.09.

     

    And yes, 1,6 metric is 1.6 US. And yes, this can be (a little) annoying.

    (the '.' at the numeric part of the keyboard is usually a decimal point

    but sometimes a comma). But at least with Windows, the support for

    regional settings is a lot better then it used to be.

     

    Richard

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 16 years ago

    Mac schreef:

    Greg Erskine wrote on Fri, 11 December 2009 15:17

    "Mac" <suemac@empire.net[/email]> wrote in message

    news:hftitb$b1e$1@cheetah.cadsoft.de...[/email]

    Hi All,

     

    In the wirepad through hole pad library the pads are described as

    1,6/0,8

    or 3,8/1,4 etc.

     

    Is the meaning of these numbers defined?

     

    Diameter / drill sizes in mm.

     

    Or even the capacitors lib has numbers. In this case it's easy to

    cross > ref

    to the capacitor type and see the hole spacing, diameter, etc.

     

    Also, I did a library>use and selected a custom library. How do I

    get back

    to having all the available libraries displayed again? Do I have to

    select

    them one at a time?

     

     

    Use the Control panel. Try right-clicking on "Libraries" and/or the

    directories and libraries below it. Take note of the green/grey dot

    next to each library. You can click on that to. I find the control

    panel is a

    very powerful interface to control projects.

     

    http://www.eaglecentral.ca

     

    Yes, thanks, I know how to select libraries for use one at a time from a

    couple of different windows. I was looking for a way to say: "use them all"

    to get back to the way it was when Eagle was installed.

     

    As for the diameter and drill sizes...so is 1,6 metric speak for 1.6mm (US

    speak)? (I wish the world would agree on decimal points or commas...  image )

     

     

    Maybe the first answer was a bit unclear, but the procedure is correct.

    When you right-click on 'libraries' in the control panel, you can

    choose: "select all" or "select none". At least in 4.09.

     

    And yes, 1,6 metric is 1.6 US. And yes, this can be (a little) annoying.

    (the '.' at the numeric part of the keyboard is usually a decimal point

    but sometimes a comma). But at least with Windows, the support for

    regional settings is a lot better then it used to be.

     

    Richard