EAGLE User Support (English) would someone mind running me through changing a font?
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
  • Replies 4 replies
  • Subscribers 180 subscribers
  • Views 428 views
  • Users 0 members are here
  • font
Related

would someone mind running me through changing a font?

matelot
matelot over 10 years ago

I would like to use a font I have that gives me numbers in circles.

I have discovered that putting 'change font <name of font> is supposed to alter the font but all I can find in the manual is on page 73 'CHANGE FONT alters the typeface.' and in the tutorial page 40 'CHANGE FONT or CHANGE SIZE changes the font or the text size.' I can't find anywhere that tells me how to do this?

If I put 'change font CombiNumber Ltd' in the line at the top of the screen (where it is supposed to go) it shows a box with the choice of fixed, proportional or vector and insists I choose one. Elsewhere I have found that these three default to one type face each but I cant find out how to change them.

  • Sign in to reply
  • Cancel

Top Replies

  • autodeskguest
    autodeskguest over 10 years ago +1
    On 28/09/15 22:22, matelot m wrote: I would like to use a font I have that gives me numbers in circles. I have discovered that putting 'change font <name of font> is supposed to alter the font but all…
Parents
  • autodeskguest
    autodeskguest over 10 years ago

    On 28/09/15 22:22, matelot m wrote:

    I would like to use a font I have that gives me numbers in circles.

    I have discovered that putting 'change font <name of font> is supposed

    to alter the font but all I can find in the manual is on page 73 'CHANGE

    FONT alters the typeface.' and in the tutorial page 40 'CHANGE FONT or

    CHANGE SIZE changes the font or the text size.' I can't find anywhere

    that tells me how to do this?

    If I put 'change font CombiNumber Ltd' in the line at the top of the

    screen (where it is supposed to go) it shows a box with the choice of

    fixed, proportional or vector and insists I choose one. Elsewhere I have

    found that these three default to one type face each but I cant find out

    how to change them.

     

    I think the latest version 7.4 might allow customisation of fonts for

    certain elements but in general, no, you can't do that. The "CHANGE

    FONT" command is for selecting between fixed, proportional or vector.

     

    Note that on the board you should ALWAYS use vector, because you're

    going to end up exporting Gerber files and all fonts will be converted

    to vector for that step anyway.

     

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • matelot
    matelot over 10 years ago in reply to autodeskguest

    That's a shame. I really could have benefited from using numbers in circles to label components on my board.

    The only other way I can think of doing it is with a number then put a circle round it.

    Thanks for the reply.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • lbrer
    lbrer over 10 years ago in reply to matelot

    use own library

    create a circle in symbol

    write centered : >Value

    additional create same in package editor

    create device with boths

    switch VALUE ON

     

    there's possible doing a automation by using  >Name   in the circle

    then you must in device switch VALUE OFF and for PREFIX use . (dot) because the non required space

     

    hans

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • lbrer
    lbrer over 10 years ago in reply to matelot

    use own library

    create a circle in symbol

    write centered : >Value

    additional create same in package editor

    create device with boths

    switch VALUE ON

     

    there's possible doing a automation by using  >Name   in the circle

    then you must in device switch VALUE OFF and for PREFIX use . (dot) because the non required space

     

    hans

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • matelot
    matelot over 10 years ago in reply to lbrer

    Thank you for that Hans.

    In fact since I wrote the thread I have gone through the circuit diagram I am copying from an old pen drawn circuit diagram and adding numbers in circles by using the circle command in the schematic page and then copying it alongside the original, moving one copy where I need it and then using text to make a number that I can put inside the circle, copying the circle again, moving it and putting another number inside. It looks right and is what I am wanting.