Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Open Sch & Brd files together
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 72 replies
  • Subscribers 190 subscribers
  • Views 9285 views
  • Users 0 members are here
Related

Open Sch & Brd files together

k.portman
k.portman over 16 years ago

Is there a way to open an existing Sch & Brd file together, by default.

When I double click either Sch or Brd file name on the Eagle Control

Panel it asks "Do you also want to load xxx.brd?" (or xxx.sch). I always

respond Yes, sofar never had a need to respond No.

 

Is there a eaglerc.usr setting to force (or make as default behaviour)

the opening of Brd & Sch files together. If not, could it be

implemented. Much requested for!!!

 

Kim

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 16 years ago

    Olin Lathrop schrieb:

    Alexander Horst wrote on Wed, 24 February 2010 15:38

    Usually I want them to be opened together. Tomorrow I may want to do

    it

    differently for whatever reason.

     

    OK, what reason?

     

    Quote:

    So why not make it switchable?

     

    Because it's just silly superstition unless you can come up with a valid

    reason to ever open one file without the other.

     

    I can think of alot of things that would never make sense for Eagle to do,

    and I don't want a switch to disable each one.

     

    Assuming that both files exist and open I don't need a swich for the

    reason that it is the same amount of "work" to click on the switch or

    just to close one file.

    And for this sos (single open switch) image  you need a selector whether

    to open the board or the sheet and a switch to select whether the

    control panel should be opened... image

     

    --

    Gruß / regards

     

    Joern

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 16 years ago

    Olin Lathrop schrieb:

    Alexander Horst wrote on Wed, 24 February 2010 15:38

    Usually I want them to be opened together. Tomorrow I may want to do

    it

    differently for whatever reason.

     

    OK, what reason?

     

    Quote:

    So why not make it switchable?

     

    Because it's just silly superstition unless you can come up with a valid

    reason to ever open one file without the other.

     

    I can think of alot of things that would never make sense for Eagle to do,

    and I don't want a switch to disable each one.

     

    Assuming that both files exist and open I don't need a swich for the

    reason that it is the same amount of "work" to click on the switch or

    just to close one file.

    And for this sos (single open switch) image  you need a selector whether

    to open the board or the sheet and a switch to select whether the

    control panel should be opened... image

     

    --

    Gruß / regards

     

    Joern