Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Open Sch & Brd files together
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 72 replies
  • Subscribers 190 subscribers
  • Views 9262 views
  • Users 0 members are here
Related

Open Sch & Brd files together

k.portman
k.portman over 16 years ago

Is there a way to open an existing Sch & Brd file together, by default.

When I double click either Sch or Brd file name on the Eagle Control

Panel it asks "Do you also want to load xxx.brd?" (or xxx.sch). I always

respond Yes, sofar never had a need to respond No.

 

Is there a eaglerc.usr setting to force (or make as default behaviour)

the opening of Brd & Sch files together. If not, could it be

implemented. Much requested for!!!

 

Kim

 

  • Sign in to reply
  • Cancel
Parents
  • k.portman
    k.portman over 16 years ago

    Il 25/02/2010 22.09, Gary Gofstein ha scritto:

    I agree with the suggestion that eagle tree should be able to open files

    of other applications. but this does not mean that EAGLE itself must

    have pdf viewer at all. just needs to pass the open command to the OS

    and let it launch the user's choice of viewer. That's all we are asking

    for.

     

    Agree. Enough to open an external Pdf viewer (Adobe, Foxit...). This

    would greatly help in navigating documentation (datasheets, project docs

    etc.). Currently though the Pdf files are not shown in the Eagle CP.

    Maybe an option in eaglerc to specify what files to show and howto open

    the viewer.

     

    Interface.FileViewer = ".pdf:AcroRd32.exe %1;.txt:Notepad.exe %1"

     

    As far as the opening of single board/schema, I think it is a dangerous

    pitfall for the new user. As Joern points out, no need for yet another

    option, you don't want both windows, just close one.

     

    You are saying to make Eagle open both sch/brd as defasult, no questions

    asked? This is the way I would like Eagle to behave. Then close the file

    you don't want/need (remember the dangers). In extreme cases where you

    really don't want the other file opened just rename the sch/brd pair to

    different names and only one file will be opened.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • k.portman
    k.portman over 16 years ago

    Il 25/02/2010 22.09, Gary Gofstein ha scritto:

    I agree with the suggestion that eagle tree should be able to open files

    of other applications. but this does not mean that EAGLE itself must

    have pdf viewer at all. just needs to pass the open command to the OS

    and let it launch the user's choice of viewer. That's all we are asking

    for.

     

    Agree. Enough to open an external Pdf viewer (Adobe, Foxit...). This

    would greatly help in navigating documentation (datasheets, project docs

    etc.). Currently though the Pdf files are not shown in the Eagle CP.

    Maybe an option in eaglerc to specify what files to show and howto open

    the viewer.

     

    Interface.FileViewer = ".pdf:AcroRd32.exe %1;.txt:Notepad.exe %1"

     

    As far as the opening of single board/schema, I think it is a dangerous

    pitfall for the new user. As Joern points out, no need for yet another

    option, you don't want both windows, just close one.

     

    You are saying to make Eagle open both sch/brd as defasult, no questions

    asked? This is the way I would like Eagle to behave. Then close the file

    you don't want/need (remember the dangers). In extreme cases where you

    really don't want the other file opened just rename the sch/brd pair to

    different names and only one file will be opened.