Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Open Sch & Brd files together
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 72 replies
  • Subscribers 190 subscribers
  • Views 9262 views
  • Users 0 members are here
Related

Open Sch & Brd files together

k.portman
k.portman over 16 years ago

Is there a way to open an existing Sch & Brd file together, by default.

When I double click either Sch or Brd file name on the Eagle Control

Panel it asks "Do you also want to load xxx.brd?" (or xxx.sch). I always

respond Yes, sofar never had a need to respond No.

 

Is there a eaglerc.usr setting to force (or make as default behaviour)

the opening of Brd & Sch files together. If not, could it be

implemented. Much requested for!!!

 

Kim

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 16 years ago

    Gary Gofstein wrote:

     

    I agree with the suggestion that eagle tree should be able to open files

    of other applications. but this does not mean that EAGLE itself must

     

    There seem to be two groups of users: The "one task one tool" group

    and those who want to have a "do it all" Eagle.

     

    I don't want to use one more file manager with different user

    interface. It will never match the maturity of a "real" file manager.

     

    I would prefer a better integration of Eagle to be used with the OS

    means.

     

    My programming editor ("IDE"), HTML editor, office software etc. all

    do not have file manager functionality and I doubt anyone asks for

    such a feature.

     

    IMO the real benefit of the Eagle control panel is the library

    handling (browse, copy elements between libraries)!

     

    have pdf viewer at all. just needs to pass the open command to the OS

    and let it launch the user's choice of viewer. That's all we are asking

    for.

     

    You open a can of worms. Eagle had to handle all the file

    associations, shell extensions etc. to do it well. That's not the task

    of a development software.

     

    As far as the opening of single board/schema, I think it is a dangerous

    pitfall for the new user. As Joern points out, no need for yet another

    option, you don't want both windows, just close one.

     

    maybe when directed to open a .sch or .brd from the OS, EAGLE should

    check the folder for a project file and just open, or ask to open, the

    project. otherwise just view the file.

     

    Since the epf is in the same folder, the user could open the epf file

    instead of the brd or sch.

     

    And keep in mind that opening the epf file also means changing it if

    the epf file is set to "auto save".

     

    Oliver

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 16 years ago

    Gary Gofstein wrote:

     

    I agree with the suggestion that eagle tree should be able to open files

    of other applications. but this does not mean that EAGLE itself must

     

    There seem to be two groups of users: The "one task one tool" group

    and those who want to have a "do it all" Eagle.

     

    I don't want to use one more file manager with different user

    interface. It will never match the maturity of a "real" file manager.

     

    I would prefer a better integration of Eagle to be used with the OS

    means.

     

    My programming editor ("IDE"), HTML editor, office software etc. all

    do not have file manager functionality and I doubt anyone asks for

    such a feature.

     

    IMO the real benefit of the Eagle control panel is the library

    handling (browse, copy elements between libraries)!

     

    have pdf viewer at all. just needs to pass the open command to the OS

    and let it launch the user's choice of viewer. That's all we are asking

    for.

     

    You open a can of worms. Eagle had to handle all the file

    associations, shell extensions etc. to do it well. That's not the task

    of a development software.

     

    As far as the opening of single board/schema, I think it is a dangerous

    pitfall for the new user. As Joern points out, no need for yet another

    option, you don't want both windows, just close one.

     

    maybe when directed to open a .sch or .brd from the OS, EAGLE should

    check the folder for a project file and just open, or ask to open, the

    project. otherwise just view the file.

     

    Since the epf is in the same folder, the user could open the epf file

    instead of the brd or sch.

     

    And keep in mind that opening the epf file also means changing it if

    the epf file is set to "auto save".

     

    Oliver