Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Open Sch & Brd files together
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 72 replies
  • Subscribers 190 subscribers
  • Views 9143 views
  • Users 0 members are here
Related

Open Sch & Brd files together

k.portman
k.portman over 16 years ago

Is there a way to open an existing Sch & Brd file together, by default.

When I double click either Sch or Brd file name on the Eagle Control

Panel it asks "Do you also want to load xxx.brd?" (or xxx.sch). I always

respond Yes, sofar never had a need to respond No.

 

Is there a eaglerc.usr setting to force (or make as default behaviour)

the opening of Brd & Sch files together. If not, could it be

implemented. Much requested for!!!

 

Kim

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 16 years ago

     

    "Tilmann Reh" <usenet2007nospam@autometer.de> wrote in message

    news:hm8hvh$3gg$1@cheetah.cadsoft.de...

    Silviu Epure schrieb:

     

    I prefere an other way: "I want to make a board, for a schematic. I need

    5

    datasheet, informations from the boardhouse, and some pictures. I want to

    be

    able to access all this from only one IDE, the one used for creating

    boards".

     

    Perhaps you got used to this method because you don't have a

    useful/powerful file manager? (This is not meant offensive - but I just

    can't imagine doing it that way could be considered as effective.)

     

    We have hundreds of projects organised in a hierarchical tree. Not all

    projects contain EAGLE data, and some contain several revisions of EAGLE

    files. Of course we have everything that is really related to the

    project in that particular project folder - however datasheets or

    boardhouse information definitely belongs at other places, since these

    are not project related (at least we use the same parts and boardhouses

    for more than one project...).

     

    I don't want to open (by hand, one after an other) half of the programs

    installed on my HDD to complete this simple project.; I don't want to

    swim

    in backup files to find my 3 usefull files.

     

    You think of EAGLE as a shell, from where you want to process/manage the

    whole workflow. I think this is not what EAGLE was developed for. You

    should think about using a shell that is meant for exactly this task.

    Then you can do everything you mentioned above from that single program.

    You activate the /documents/ (not the programs!) and the OS calls the

    needed programs to open them, regardless of document type (EAGLE, PDF,

    Word, Picture or whatever else). Of course all project related

    documents/files are arranged in the same folder (or related subfolders),

    so you have them all at hand when you open that folder.

     

    Please take the time to really think about this. I'm pretty sure your

    workflow would be much more efficient (and the needed programs much less

    bloated) if your concept was more "object oriented" and less "program

    oriented" - perhaps after a short time of getting used to it.

     

    Tilmann

     

    1. I do have a usefull file manager (totalcmd), and I know how to use-it.

    But a full folder is a full foder no matter what file browser you use.

    2. My concept is not "program oriented", but "project oriented"

    3. and be honest... would you be bothered if Eagle could open pdf with

    external application?

    It is allready support writing pdf's....

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 16 years ago in reply to autodeskguest

    3. and be honest... would you be bothered if Eagle could open pdf with

    external application?

    It is allready support writing pdf's....

     

     

    Absolutely I Would Be Bothered if Eagle could open pdf files, partly

    because you then want more.

     

    But mostly, this bothers me because my project tree as viewed from Eagle

    gets as cluttered as when viewed from XYplorer. I can see tons of files,

    related to the project but NOT part of Eagle and then have lots more

    hunting and scrolling when switching between schematics in multiple

    projects. It would really annoy me.

     

    That said, If we had a setting in the CP to create custom filters so we

    only see the file types we want to see, it's not a problem for me

    anymore and I say go ahead, just so everyone stops complaining.

     

    By the time Klaus has read this entire thread, he could have implemented

    the suggestion with a filter setting. Talk about wasting developer's

    time...  image

     

    Travis

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 16 years ago in reply to autodeskguest

    3. and be honest... would you be bothered if Eagle could open pdf with

    external application?

    It is allready support writing pdf's....

     

     

    Absolutely I Would Be Bothered if Eagle could open pdf files, partly

    because you then want more.

     

    But mostly, this bothers me because my project tree as viewed from Eagle

    gets as cluttered as when viewed from XYplorer. I can see tons of files,

    related to the project but NOT part of Eagle and then have lots more

    hunting and scrolling when switching between schematics in multiple

    projects. It would really annoy me.

     

    That said, If we had a setting in the CP to create custom filters so we

    only see the file types we want to see, it's not a problem for me

    anymore and I say go ahead, just so everyone stops complaining.

     

    By the time Klaus has read this entire thread, he could have implemented

    the suggestion with a filter setting. Talk about wasting developer's

    time...  image

     

    Travis