EAGLE User Support (English) Doubling up tracks on different layers
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
  • Replies 10 replies
  • Subscribers 179 subscribers
  • Views 1892 views
  • Users 0 members are here
Related

Doubling up tracks on different layers

autodeskguest
autodeskguest over 15 years ago

Guys,

 

I've got a problem I hope someone can help me out with.  I have some

very high current traces on my PCB (15A and 30A).  I'm using 2oz copper

but in order to get track widths that aren't completely ridiculous I

need to double up the tracks on two layers.  I'm new at Eagle (last used

OrCAD PCB editor which is a stripped down version of Allegro) and I

can't seem to make this happen.  When I route the initial track on the

first layer naturally the ratsnest for this route disappears (since it

is now connected).  Eagle won't allow me to start a track on the second

layer because there is no longer an active ratsnest.  How do I get

around this?

 

This is also a generic issue.  If I want to start routing on a pin that

the ratsnest currently isn't touching (but it is unrouted, the ratsnest

is just terminated on a different unrouted pin) Eagle won't let me.

This is different from Allegro where I could start routing on any pin

and if it was unrouted the ratsnest would immediately snap to that pin.

  This is somewhat annoying since it is forcing me to route nets in the

order that Eagle decides to snap the ratsnest to instead of routing in

the order that is most logical to me.  I'm sure there is a way around

this, but I've yet to find it.

 

Thanks,

 

Michael

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 15 years ago

    Indeed Doug was correct, you can double up a track by starting it by

    holding the CTRL key down.  However, you have to remember to release

    the CTRL key before making the next connection (otherwise it will just

    literally "throw a curve" into your track).  Very useful information.

    Thanks guys.

     

    Thanks,

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 15 years ago

    Indeed Doug was correct, you can double up a track by starting it by

    holding the CTRL key down.  However, you have to remember to release

    the CTRL key before making the next connection (otherwise it will just

    literally "throw a curve" into your track).  Very useful information.

    Thanks guys.

     

    Thanks,