EAGLE User Support (English) Doubling up tracks on different layers
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
  • Replies 10 replies
  • Subscribers 178 subscribers
  • Views 1881 views
  • Users 0 members are here
Related

Doubling up tracks on different layers

autodeskguest
autodeskguest over 15 years ago

Guys,

 

I've got a problem I hope someone can help me out with.  I have some

very high current traces on my PCB (15A and 30A).  I'm using 2oz copper

but in order to get track widths that aren't completely ridiculous I

need to double up the tracks on two layers.  I'm new at Eagle (last used

OrCAD PCB editor which is a stripped down version of Allegro) and I

can't seem to make this happen.  When I route the initial track on the

first layer naturally the ratsnest for this route disappears (since it

is now connected).  Eagle won't allow me to start a track on the second

layer because there is no longer an active ratsnest.  How do I get

around this?

 

This is also a generic issue.  If I want to start routing on a pin that

the ratsnest currently isn't touching (but it is unrouted, the ratsnest

is just terminated on a different unrouted pin) Eagle won't let me.

This is different from Allegro where I could start routing on any pin

and if it was unrouted the ratsnest would immediately snap to that pin.

  This is somewhat annoying since it is forcing me to route nets in the

order that Eagle decides to snap the ratsnest to instead of routing in

the order that is most logical to me.  I'm sure there is a way around

this, but I've yet to find it.

 

Thanks,

 

Michael

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 15 years ago

    David Ingebretsen wrote:

    Michael Sansom wrote on Thu, 01 April 2010 09:24

    Guys,

     

    I've got a problem I hope someone can help me out with.  I have some

    very high current traces on my PCB (15A and 30A).  I'm using 2oz copper

     

    but in order to get track widths that aren't completely ridiculous I

    need to double up the tracks on two layers.  I'm new at Eagle (last

    used OrCAD PCB editor which is a stripped down version of Allegro) and

    I can't seem to make this happen.  When I route the initial track on the

     

    first layer naturally the ratsnest for this route disappears (since it

     

    is now connected).  Eagle won't allow me to start a track on the second

     

    layer because there is no longer an active ratsnest.  How do I get

    around this?

     

    This is also a generic issue.  If I want to start routing on a pin that

     

    the ratsnest currently isn't touching (but it is unrouted, the ratsnest

     

    is just terminated on a different unrouted pin) Eagle won't let me.

    This is different from Allegro where I could start routing on any pin

    and if it was unrouted the ratsnest would immediately snap to that pin.

     

      This is somewhat annoying since it is forcing me to route nets in the

     

    order that Eagle decides to snap the ratsnest to instead of routing in

     

    the order that is most logical to me.  I'm sure there is a way around

    this, but I've yet to find it.

     

    Thanks,

     

    Michael

     

    I can't help on the first issue, but for the second one, press and hold

    ctrl when you are starting your trace and you can start at any location on

    the net.

    Also, remember, too, you can press down alt as well to use the alternate

    grid spacing temporarily.

     

    DAvid

     

    Thanks to both of you.  Yes, I use the ALT key a lot to switch to my

    minimum grid spacing and that works well but I wasn't aware of the CTL

    key allowing me to start a line on a pin/pad that wasn't terminated in a

    ratsnest line.

     

    That first question is really important.  The ability to run the same

    track on different layers is a key ability when doing layouts with high

    current nets.  Doug seems to imply that using CTL might work in that

    situation as well.  I'll try it and see what happens.

     

    Moving from one layout package to another is always a pain as you get

    trained to think in terms of whatever package you have the most

    experience with.  After using Eagle for a week or so it seems that there

    are many fine attributes of this package.  The ability to alter a

    schematic and have the results show up immediately in the pcb layout

    package is a huge plus.  And in terms of pure execution speed it seems

    faster than Allegro in many places.  However, there are a few things

    that I really miss.  Allegro would let me constrain my tracks to be

    purely orthogonal with 45 degree bends, and would automatically keep

    tracks vertical/horizontal as you routed across the board.  Also, it

    would enforce spacing requirements in real time as you routed a trace

    (so you didn't find out that you have tracks closer than your design

    rules permit only after running a DRC).

     

    All and all it is a very good value.  However, I would think that with

    the addition of a few key features it could compete with anything out

    there.  Would be interesting to know what sort of features are on the

    road map for future releases.

     

    -Michael

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 15 years ago in reply to autodeskguest

    Quote:

    Allegro would let me constrain my tracks to be

    purely orthogonal with 45 degree bends, and would automatically keep

    tracks vertical/horizontal as you routed across the board. Also, it

    would enforce spacing requirements in real time as you routed a trace

    (so you didn't find out that you have tracks closer than your design

    rules permit only after running a DRC).

     

     

     

    Hi,

     

    To change the orthogonal bend style when routing, you can use the right

    mouse button while you're drawing the trace.  Just keep cliking the right

    button to change the angle style to what you like.

     

    I don't know a way to enforce spacing from one wire to the next while

    routing, I've always controlled this with grid, track-width, and being very

    careful, but it's a pain.  PADs had a mode where it would "hold" the

    routing to design rule spacings as you were doing it, but I haven't found a

    way to do this in Eagle.

     

    If anyone knows, I'd be very interested too.

     

     

    Cheers,

     

    Alex

     

     

     

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 15 years ago in reply to autodeskguest

     

    "Michael Sansom" <mssansom@hotmail.com> wrote in message

    news:hpg1g0$lrj$1@cheetah.cadsoft.de...

    I like Eagle and think it is a hell of a value for the money, but it is a

    little frustrating that there are a few features found in other tools that

    are missing that would take Eagle to the next level and allow it to

    compete with almost any package out there.  Hopefully some of this will

    get addressed in future releases.

     

    People are not the same. Software is made by people for people. So it can't

    be an application to please everyone. Eagle is made for people that love and

    use Eagle. Some of them want to bring new features in this software, some of

    them wants to keep-it as it is (even changing the version number is an

    "almost acceptable change" for some of them image )

     

    And the "not so good" news is that Cadsoft is never hurry to implement

    changes in their software (maybe the effort is too heavy, or they can't, or

    they won't image )

     

    But as it is now, it's usable for much more than just routing a PCB with 3

    resistors and an IC.

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 15 years ago in reply to autodeskguest

    Alex Faveluke wrote:

    Quote:

    Allegro would let me constrain my tracks to be

    purely orthogonal with 45 degree bends, and would automatically keep

    tracks vertical/horizontal as you routed across the board. Also, it

    would enforce spacing requirements in real time as you routed a trace

    (so you didn't find out that you have tracks closer than your design

    rules permit only after running a DRC).

     

     

    Hi,

     

    To change the orthogonal bend style when routing, you can use the right

    mouse button while you're drawing the trace.  Just keep cliking the right

    button to change the angle style to what you like.

     

    I don't know a way to enforce spacing from one wire to the next while

    routing, I've always controlled this with grid, track-width, and being very

    careful, but it's a pain.  PADs had a mode where it would "hold" the

    routing to design rule spacings as you were doing it, but I haven't found a

    way to do this in Eagle.

     

    If anyone knows, I'd be very interested too.

     

     

    Cheers,

     

    Alex

     

     

     

    Yeah, I discovered the routing mode that enforced orthogonal tracks with

    45 degree bends, and that does help.  However, if after routing a track

    in this manner I then move/shove the track I loose my guarantee of

    orthogonal lines and 45 degree bends, which is a bummer.

     

    I've seen PADS and it's enforcement of spacing rules in real time while

    routing is very much like Allegro's.  That feature tremendously speeds

    manual routing and is a huge asset.  I don't believe that Eagle can

    support this as it stands.  I don't know how PADS works in this respect

    but Allegro would also enforce spacing rules when you moved/shoved

    tracks after initial routing. i.e. if you shoved a track too close to

    the adjacent track such that it violates the spacing constraints it

    would either shove the adjacent track over (if it could without it

    colliding with something else) or it would just not allow it to happen

    and the track you were shoving would "bounce" off.  Again, great asset

    to have when routing a dense board.  Both tools allowed you to easily

    optimize your routing channel such that every track in parallel was

    placed at the minimum spacing.

     

    I like Eagle and think it is a hell of a value for the money, but it is

    a little frustrating that there are a few features found in other tools

    that are missing that would take Eagle to the next level and allow it to

    compete with almost any package out there.  Hopefully some of this will

    get addressed in future releases.

     

    -Michael

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 15 years ago in reply to autodeskguest

    Michael Sansom wrote on Tue, 06 April 2010 15:19

    I've seen PADS and it's enforcement of spacing rules in real time while

     

    routing is very much like Allegro's.  That feature tremendously speeds

     

    manual routing and is a huge asset.  I don't believe that Eagle can

    support this as it stands.  I don't know how PADS works in this respect

     

    but Allegro would also enforce spacing rules when you moved/shoved

    tracks after initial routing. i.e. if you shoved a track too close to

    the adjacent track such that it violates the spacing constraints it

    would either shove the adjacent track over (if it could without it

    colliding with something else) or it would just not allow it to happen

     

    and the track you were shoving would "bounce" off.  Again, great asset

     

    to have when routing a dense board.  Both tools allowed you to easily

    optimize your routing channel such that every track in parallel was

    placed at the minimum spacing.

     

    I like Eagle and think it is a hell of a value for the money, but it is

     

    a little frustrating that there are a few features found in other tools

     

    that are missing that would take Eagle to the next level and allow it

    to

    compete with almost any package out there.  Hopefully some of this will

     

    get addressed in future releases.

     

    -Michael

     

     

    Yes, that's the feature of PADS that I miss from 10 yrs ago.  It would be a

    massive benefit to have this.

     

    One thing you might try is selecting the segments in a route by drawing a

    group around them, then moving the group as a whole in one direction.

    Maybe you already know this but Eagle lets you define a group by drawing an

    arbitrary surrounding shape around it... so it's possible to select

    arbitrary shaped collections of objects, not just rectangles.

     

    Cheers,

     

    Alex

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 15 years ago in reply to autodeskguest

    Michael Sansom wrote on Tue, 06 April 2010 15:19

    I've seen PADS and it's enforcement of spacing rules in real time while

     

    routing is very much like Allegro's.  That feature tremendously speeds

     

    manual routing and is a huge asset.  I don't believe that Eagle can

    support this as it stands.  I don't know how PADS works in this respect

     

    but Allegro would also enforce spacing rules when you moved/shoved

    tracks after initial routing. i.e. if you shoved a track too close to

    the adjacent track such that it violates the spacing constraints it

    would either shove the adjacent track over (if it could without it

    colliding with something else) or it would just not allow it to happen

     

    and the track you were shoving would "bounce" off.  Again, great asset

     

    to have when routing a dense board.  Both tools allowed you to easily

    optimize your routing channel such that every track in parallel was

    placed at the minimum spacing.

     

    I like Eagle and think it is a hell of a value for the money, but it is

     

    a little frustrating that there are a few features found in other tools

     

    that are missing that would take Eagle to the next level and allow it

    to

    compete with almost any package out there.  Hopefully some of this will

     

    get addressed in future releases.

     

    -Michael

     

     

    Yes, that's the feature of PADS that I miss from 10 yrs ago.  It would be a

    massive benefit to have this.

     

    One thing you might try is selecting the segments in a route by drawing a

    group around them, then moving the group as a whole in one direction.

    Maybe you already know this but Eagle lets you define a group by drawing an

    arbitrary surrounding shape around it... so it's possible to select

    arbitrary shaped collections of objects, not just rectangles.

     

    Cheers,

     

    Alex

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.