EAGLE User Support (English) connecting a Signal to a via in board editor
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
  • Replies 8 replies
  • Subscribers 178 subscribers
  • Views 2963 views
  • Users 0 members are here
Related

connecting a Signal to a via in board editor

autodeskguest
autodeskguest over 15 years ago

Hi,

 

Is there a trick to connect a signal to a via?  I can connect signals

between packages, but if I place a via and try to connect a signal to

it, it doesn't take. I had to create a pad as a part to get it to work.

 

Normal behavior?

 

v4.16

 

Thanks

Martin

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 15 years ago

    Hi MArtin,

     

    Martin Eder wrote:

    Is there a trick to connect a signal to a via?  I can connect signals

    between packages, but if I place a via and try to connect a signal to

    it, it doesn't take. I had to create a pad as a part to get it to work.

     

    reading the whole tread, especially your answer to Gary, I think I

    understand now what you are trying to do but didn't state explicitly

    anywhere 8-)

     

    You've placed a part in the schematic and now you want to connect one

    of its pins to a via you placed in the board, without this pin being

    connected to any net in the schematic.

     

    If that is the case you can't connect anything to that pin in the

    board (as you already stated) because there is no net to connect to.

     

    But you don't need a you pad as a part, just connect a short net stump

    to the pin in the schematic (and give it a name if you like). Then

    "via 'net-name'" (or placing the via and renaming it afterwards) gives

    you a via connected to that pin.

    You need to do a ratsnest to see the aitwire though.

    Or ctrl-click to start routing on either the pin or the via.

     

    I'm on 5.8 here, but I can't remember any change in behaviour in this

    area since 4.x

     

     

    On the other hand I prefer using a part because that documents the

    precense of the via (test points in my case) in the schematic.

    And placed as a part in the schematic I won't forget to place it in

    the board.

    --

     

    Lorenz

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 15 years ago

    Hi MArtin,

     

    Martin Eder wrote:

    Is there a trick to connect a signal to a via?  I can connect signals

    between packages, but if I place a via and try to connect a signal to

    it, it doesn't take. I had to create a pad as a part to get it to work.

     

    reading the whole tread, especially your answer to Gary, I think I

    understand now what you are trying to do but didn't state explicitly

    anywhere 8-)

     

    You've placed a part in the schematic and now you want to connect one

    of its pins to a via you placed in the board, without this pin being

    connected to any net in the schematic.

     

    If that is the case you can't connect anything to that pin in the

    board (as you already stated) because there is no net to connect to.

     

    But you don't need a you pad as a part, just connect a short net stump

    to the pin in the schematic (and give it a name if you like). Then

    "via 'net-name'" (or placing the via and renaming it afterwards) gives

    you a via connected to that pin.

    You need to do a ratsnest to see the aitwire though.

    Or ctrl-click to start routing on either the pin or the via.

     

    I'm on 5.8 here, but I can't remember any change in behaviour in this

    area since 4.x

     

     

    On the other hand I prefer using a part because that documents the

    precense of the via (test points in my case) in the schematic.

    And placed as a part in the schematic I won't forget to place it in

    the board.

    --

     

    Lorenz