EAGLE User Support (English) connecting a Signal to a via in board editor
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
  • Replies 8 replies
  • Subscribers 178 subscribers
  • Views 2948 views
  • Users 0 members are here
Related

connecting a Signal to a via in board editor

autodeskguest
autodeskguest over 15 years ago

Hi,

 

Is there a trick to connect a signal to a via?  I can connect signals

between packages, but if I place a via and try to connect a signal to

it, it doesn't take. I had to create a pad as a part to get it to work.

 

Normal behavior?

 

v4.16

 

Thanks

Martin

 

 

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 15 years ago

    On 4/12/2010 6:07 PM, Martin Eder wrote:

    Hi,

     

    Is there a trick to connect a signal to a via?  I can connect signals

    between packages, but if I place a via and try to connect a signal to

    it, it doesn't take. I had to create a pad as a part to get it to work.

     

    Normal behavior?

     

    v4.16

     

    Thanks

    Martin

     

     

    did you name the via to the same name as the net you connect it to??

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 15 years ago

     

    "Gary Gofstein" <nospam@use.forum.net> wrote in message

    news:hq0h2v$qc6$1@cheetah.cadsoft.de...

    On 4/12/2010 6:07 PM, Martin Eder wrote:

    Hi,

     

    Is there a trick to connect a signal to a via?  I can connect signals

    between packages, but if I place a via and try to connect a signal to

    it, it doesn't take. I had to create a pad as a part to get it to

    work.

     

    Normal behavior?

     

    v4.16

     

    Thanks

    Martin

     

     

    did you name the via to the same name as the net you connect it to??

     

    I Think I tried that, but the pin is part of a connector so you can't

    get the name of the pin.

    Any type of part will exhibit the same behavior, you cant signal it to a

    lone via.

     

    Cheers

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 15 years ago

     

    "Martin Eder" wrote

     

    Is there a trick to connect a signal to a via?  I can connect signals

    between packages, but if I place a via and try to connect a signal to

    it, it doesn't take. I had to create a pad as a part to get it to work.

     

    Normal behavior?

    v4.16

    Thanks

    Martin

     

    Martin

     

    You can connect a signal to a via. The via must have the same name as the

    signal for the attachment to take place. This has been said earlier. But

    once you are connected to that via you cannot continue on to your

    destination point. So this is not a really useful approach to take.

     

    Remember signals are abstract connections. They simply indicate points, on a

    common net, that will be phyically connected after you have done the

    routing.

    You appear to be approaching this in a single ended manner. i.e starting out

    from a pin and trying to connect to the via before heading off to the final

    connection point/pin.

     

    It's better to:

    1.  Attach the signal to the start and finish points so the signal is

    established .

    2. Determine the name of the signal.

    3. Drop in a via with the same name and if its close to the signal airwires

    they will snap to the via as you wished but can snap with your via on a

    branch.

     

    But even this is over working. Why not do the following

    1.  Attach the signal to the start and finish points so the signal is

    established .

    2. Commence routing this signal. When you change layers a via will be

    automatically placed.

    3. Finish the route to the destination or as much as you can do at that

    point.

     

    Hope this helps

    Warren

     

     

     

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 15 years ago

    On 4/12/2010 9:07 PM, Martin Eder wrote:

    Hi,

     

    Is there a trick to connect a signal to a via?  I can connect signals

    between packages, but if I place a via and try to connect a signal to

    it, it doesn't take. I had to create a pad as a part to get it to work.

     

    Normal behavior?

     

    v4.16

     

    Thanks

    Martin

     

     

     

    Hi Martin,

     

    I've run into this problem trying to route traces to Power pads that

    leave my board.

     

    You can run airwires between ICs and library components but not simple

    pads that you place on the board.

     

    My techniques is this:

     

    Let's say I have a Timer IC whose +V pin I need to connect to the +V pad

    on my board.

     

    1) Use airwires to connect the +V pin to some other pin or component

    (preferably one that not to close to the V+ pin).

    2)Use the Route command and start routing from pin +V, but head towards

    +V pad or via.

    3) Using the wire command start at the V+ PAD on the board and connect

    this wire to the traces you have already routed.

    4) Eagle will ask if the two signals go together, select the name you

    want the joined signal to have and click ok.

    5) Now if you check name you'll see that both the Timer +V pin and the

    +V pad are all one signal. If not then check the PAD signal name it

    should be the same the wire you used to connect it to the traces you routed.

    6) Now that the connection is complete you can delete the dummy airwire.

     

    Hope this helps.

     

    Jorge Garcia

    Cadsoft Computer

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 15 years ago

     

    "Jorge Garcia" <jorge@cadsoftusa.com> wrote in message

    news:hq2lfo$qr5$1@cheetah.cadsoft.de...

    On 4/12/2010 9:07 PM, Martin Eder wrote:

    Hi,

     

    Is there a trick to connect a signal to a via?  I can connect signals

    between packages, but if I place a via and try to connect a signal to

    it, it doesn't take. I had to create a pad as a part to get it to

    work.

     

    Normal behavior?

     

    v4.16

     

    Thanks

    Martin

     

     

     

    Hi Martin,

     

    I've run into this problem trying to route traces to Power pads that

    leave my board.

     

    You can run airwires between ICs and library components but not simple

    pads that you place on the board.

     

    My techniques is this:

     

    Let's say I have a Timer IC whose +V pin I need to connect to the +V

    pad on my board.

     

    1) Use airwires to connect the +V pin to some other pin or component

    (preferably one that not to close to the V+ pin).

    2)Use the Route command and start routing from pin +V, but head

    towards +V pad or via.

    3) Using the wire command start at the V+ PAD on the board and connect

    this wire to the traces you have already routed.

    4) Eagle will ask if the two signals go together, select the name you

    want the joined signal to have and click ok.

    5) Now if you check name you'll see that both the Timer +V pin and the

    +V pad are all one signal. If not then check the PAD signal name it

    should be the same the wire you used to connect it to the traces you

    routed.

    6) Now that the connection is complete you can delete the dummy

    airwire.

     

    Hope this helps.

     

    Jorge Garcia

    Cadsoft Computer

     

     

     

    I pondered this approach, but I found it easy to just create a pad as a

    part.  Thanks for the suggestion.

    I wasn’t expecting  such a road block with this. Thought there might be

    a easy way.

     

    FYI, I was just trying to connect connector shell mount/gnd signals to a

    pad so that there is a  option to ground them.

    Typically you don’t see them in net lists, at least the Netlist I have

    from a clients orcad.

     

    Cheers

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 15 years ago

    Hi MArtin,

     

    Martin Eder wrote:

    Is there a trick to connect a signal to a via?  I can connect signals

    between packages, but if I place a via and try to connect a signal to

    it, it doesn't take. I had to create a pad as a part to get it to work.

     

    reading the whole tread, especially your answer to Gary, I think I

    understand now what you are trying to do but didn't state explicitly

    anywhere 8-)

     

    You've placed a part in the schematic and now you want to connect one

    of its pins to a via you placed in the board, without this pin being

    connected to any net in the schematic.

     

    If that is the case you can't connect anything to that pin in the

    board (as you already stated) because there is no net to connect to.

     

    But you don't need a you pad as a part, just connect a short net stump

    to the pin in the schematic (and give it a name if you like). Then

    "via 'net-name'" (or placing the via and renaming it afterwards) gives

    you a via connected to that pin.

    You need to do a ratsnest to see the aitwire though.

    Or ctrl-click to start routing on either the pin or the via.

     

    I'm on 5.8 here, but I can't remember any change in behaviour in this

    area since 4.x

     

     

    On the other hand I prefer using a part because that documents the

    precense of the via (test points in my case) in the schematic.

    And placed as a part in the schematic I won't forget to place it in

    the board.

    --

     

    Lorenz

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 15 years ago

    On 4/13/2010 3:51 PM, Martin Eder wrote:

    "Jorge Garcia"<jorge@cadsoftusa.com>  wrote in message

    news:hq2lfo$qr5$1@cheetah.cadsoft.de...

    On 4/12/2010 9:07 PM, Martin Eder wrote:

    Hi,

     

    Is there a trick to connect a signal to a via?  I can connect signals

    between packages, but if I place a via and try to connect a signal to

    it, it doesn't take. I had to create a pad as a part to get it to

    work.

     

    Normal behavior?

     

    v4.16

     

    Thanks

    Martin

     

     

     

    Hi Martin,

     

    I've run into this problem trying to route traces to Power pads that

    leave my board.

     

    You can run airwires between ICs and library components but not simple

    pads that you place on the board.

     

    My techniques is this:

     

    Let's say I have a Timer IC whose +V pin I need to connect to the +V

    pad on my board.

     

    1) Use airwires to connect the +V pin to some other pin or component

    (preferably one that not to close to the V+ pin).

    2)Use the Route command and start routing from pin +V, but head

    towards +V pad or via.

    3) Using the wire command start at the V+ PAD on the board and connect

    this wire to the traces you have already routed.

    4) Eagle will ask if the two signals go together, select the name you

    want the joined signal to have and click ok.

    5) Now if you check name you'll see that both the Timer +V pin and the

    +V pad are all one signal. If not then check the PAD signal name it

    should be the same the wire you used to connect it to the traces you

    routed.

    6) Now that the connection is complete you can delete the dummy

    airwire.

     

    Hope this helps.

     

    Jorge Garcia

    Cadsoft Computer

     

     

     

    I pondered this approach, but I found it easy to just create a pad as a

    part.  Thanks for the suggestion.

    I wasn’t expecting  such a road block with this. Thought there might be

    a easy way.

     

    FYI, I was just trying to connect connector shell mount/gnd signals to a

    pad so that there is a  option to ground them.

    Typically you don’t see them in net lists, at least the Netlist I have

    from a clients orcad.

     

    Cheers

     

     

     

    I would create a pin on the part to connect the shell, and use a pad

    part as you did. there are pads and holes parts in the eagle libs, but

    you can easily create one as well. don't know if you use schematics or

    not, but I always show things like this in the schematic. good that you

    caught it missing in the netlist.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 15 years ago in reply to autodeskguest

    OK, how about this approach:

     

    Do a CTRL-route from some point on the signal where  you want to

    connect the via.  A CTRL-route allows you to start anywhere, even if

    there are no airwires or unconnected nets.  Continue with that

    CTRL-route to where you want to place a via.  Then change layers and

    continue a little ways further in the new layer, then hit ESC to stop

    the routing.  This will give you a trace, a via, and then a trace on

    the new layer that goes nowhere.  Now use rip-up to get rid of the

    trace on the new layer.  Finally, use INFO to change the properties of

    the via as needed to make it as big as a pad, or whatever you want to

    do with it.

     

     

    Robert Scott

    Real-Time Specialties

    Ypsilanti, Michigan