EAGLE User Support (English) connecting a Signal to a via in board editor
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
  • Replies 8 replies
  • Subscribers 178 subscribers
  • Views 2970 views
  • Users 0 members are here
Related

connecting a Signal to a via in board editor

autodeskguest
autodeskguest over 15 years ago

Hi,

 

Is there a trick to connect a signal to a via?  I can connect signals

between packages, but if I place a via and try to connect a signal to

it, it doesn't take. I had to create a pad as a part to get it to work.

 

Normal behavior?

 

v4.16

 

Thanks

Martin

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 15 years ago

    On 4/13/2010 3:51 PM, Martin Eder wrote:

    "Jorge Garcia"<jorge@cadsoftusa.com>  wrote in message

    news:hq2lfo$qr5$1@cheetah.cadsoft.de...

    On 4/12/2010 9:07 PM, Martin Eder wrote:

    Hi,

     

    Is there a trick to connect a signal to a via?  I can connect signals

    between packages, but if I place a via and try to connect a signal to

    it, it doesn't take. I had to create a pad as a part to get it to

    work.

     

    Normal behavior?

     

    v4.16

     

    Thanks

    Martin

     

     

     

    Hi Martin,

     

    I've run into this problem trying to route traces to Power pads that

    leave my board.

     

    You can run airwires between ICs and library components but not simple

    pads that you place on the board.

     

    My techniques is this:

     

    Let's say I have a Timer IC whose +V pin I need to connect to the +V

    pad on my board.

     

    1) Use airwires to connect the +V pin to some other pin or component

    (preferably one that not to close to the V+ pin).

    2)Use the Route command and start routing from pin +V, but head

    towards +V pad or via.

    3) Using the wire command start at the V+ PAD on the board and connect

    this wire to the traces you have already routed.

    4) Eagle will ask if the two signals go together, select the name you

    want the joined signal to have and click ok.

    5) Now if you check name you'll see that both the Timer +V pin and the

    +V pad are all one signal. If not then check the PAD signal name it

    should be the same the wire you used to connect it to the traces you

    routed.

    6) Now that the connection is complete you can delete the dummy

    airwire.

     

    Hope this helps.

     

    Jorge Garcia

    Cadsoft Computer

     

     

     

    I pondered this approach, but I found it easy to just create a pad as a

    part.  Thanks for the suggestion.

    I wasn’t expecting  such a road block with this. Thought there might be

    a easy way.

     

    FYI, I was just trying to connect connector shell mount/gnd signals to a

    pad so that there is a  option to ground them.

    Typically you don’t see them in net lists, at least the Netlist I have

    from a clients orcad.

     

    Cheers

     

     

     

    I would create a pin on the part to connect the shell, and use a pad

    part as you did. there are pads and holes parts in the eagle libs, but

    you can easily create one as well. don't know if you use schematics or

    not, but I always show things like this in the schematic. good that you

    caught it missing in the netlist.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 15 years ago

    On 4/13/2010 3:51 PM, Martin Eder wrote:

    "Jorge Garcia"<jorge@cadsoftusa.com>  wrote in message

    news:hq2lfo$qr5$1@cheetah.cadsoft.de...

    On 4/12/2010 9:07 PM, Martin Eder wrote:

    Hi,

     

    Is there a trick to connect a signal to a via?  I can connect signals

    between packages, but if I place a via and try to connect a signal to

    it, it doesn't take. I had to create a pad as a part to get it to

    work.

     

    Normal behavior?

     

    v4.16

     

    Thanks

    Martin

     

     

     

    Hi Martin,

     

    I've run into this problem trying to route traces to Power pads that

    leave my board.

     

    You can run airwires between ICs and library components but not simple

    pads that you place on the board.

     

    My techniques is this:

     

    Let's say I have a Timer IC whose +V pin I need to connect to the +V

    pad on my board.

     

    1) Use airwires to connect the +V pin to some other pin or component

    (preferably one that not to close to the V+ pin).

    2)Use the Route command and start routing from pin +V, but head

    towards +V pad or via.

    3) Using the wire command start at the V+ PAD on the board and connect

    this wire to the traces you have already routed.

    4) Eagle will ask if the two signals go together, select the name you

    want the joined signal to have and click ok.

    5) Now if you check name you'll see that both the Timer +V pin and the

    +V pad are all one signal. If not then check the PAD signal name it

    should be the same the wire you used to connect it to the traces you

    routed.

    6) Now that the connection is complete you can delete the dummy

    airwire.

     

    Hope this helps.

     

    Jorge Garcia

    Cadsoft Computer

     

     

     

    I pondered this approach, but I found it easy to just create a pad as a

    part.  Thanks for the suggestion.

    I wasn’t expecting  such a road block with this. Thought there might be

    a easy way.

     

    FYI, I was just trying to connect connector shell mount/gnd signals to a

    pad so that there is a  option to ground them.

    Typically you don’t see them in net lists, at least the Netlist I have

    from a clients orcad.

     

    Cheers

     

     

     

    I would create a pin on the part to connect the shell, and use a pad

    part as you did. there are pads and holes parts in the eagle libs, but

    you can easily create one as well. don't know if you use schematics or

    not, but I always show things like this in the schematic. good that you

    caught it missing in the netlist.