element14 Community
element14 Community
    Register Log In
  • Site
  • Search
  • Log In Register
  • About Us
  • Community Hub
    Community Hub
    • What's New on element14
    • Feedback and Support
    • Benefits of Membership
    • Personal Blogs
    • Members Area
    • Achievement Levels
  • Learn
    Learn
    • Ask an Expert
    • eBooks
    • element14 presents
    • Learning Center
    • Tech Spotlight
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
    • element14 presents Projects
    • Project14
    • Arduino Projects
    • Raspberry Pi Projects
    • Project Groups
  • Products
    Products
    • Arduino
    • Avnet Boards Community
    • Dev Tools
    • Manufacturers
    • Multicomp Pro
    • Product Groups
    • Raspberry Pi
    • RoadTests & Reviews
  • Store
    Store
    • Visit Your Store
    • Choose another store...
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
  • Settings
Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Newbee: howto make device with 2 GND pins
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 176 subscribers
  • Views 887 views
  • Users 0 members are here
Related

Newbee: howto make device with 2 GND pins

Former Member
Former Member over 15 years ago

Like SOT223 a device having 2 pins internally connected in the device.

Sot224 pin 2 and 4(cooling pad) are the same.

I supposed that connecting  one pin it is also connected to the other.

However, on the board a airwire still remains. This is also true for a

sot223 device from the library.

I tried the mailto:GND@1 etc. naming, but seems not to work.

What am I doing wrong?

 

 

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 15 years ago

    Am 27.04.2010 00:24, schrieb Gary Gofstein:

    On 4/26/2010 2:13 PM, Michael Sansom wrote:

    Joern Paschedag wrote:

    Am 25.04.2010 20:41, schrieb Rens:

    Like SOT223 a device having 2 pins internally connected in the device.

    Sot224 pin 2 and 4(cooling pad) are the same.

    I supposed that connecting one pin it is also connected to the other.

    However, on the board a airwire still remains. This is also true for a

    sot223 device from the library.

    I tried the mailto:GND@1 etc. naming, but seems not to work.

    What am I doing wrong?

     

     

     

    Eagle does not know internal connections. So the rule is one pin for

    one pad. Some SO8 transistors have four drains which are internally

    connected. They are named D, D@1, d@2, D@3 in the library in this

    example. It would be ok, if you connect just one of these pins in the

    schematic and eagle would do the same in board.

    BUT, why should a manufactorer add more pads, if one is enough?

    Because the chip is connected to the pads with bonding wires and one

    wire is not thick enough to carry the amount of current specified in

    the data sheet. So two or more connections are used in parallel to

    carry the current. So you should see that all equal named pins are

    connected externally to avoid a "slow blowing fuse" device.

     

     

    What is the significance (if any) of using the "@" symbol in the example

    above.

     

    BTW, what I do in this situation is have GND1, GND2, GND3, .... as pin

    names on the symbol and then connect them all independently to "GND" on

    the schematic. Works well.

     

    The part following the '@' is not shown so that each looks like the same

    label pin.

     

    ...and gnd1, gnd2 or vdd1 and vdd2 etc. are usually different nets if

    you use an isolation amplifier for example image

     

    --

    Gruß / regards

     

    Joern

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 15 years ago

    Am 27.04.2010 00:24, schrieb Gary Gofstein:

    On 4/26/2010 2:13 PM, Michael Sansom wrote:

    Joern Paschedag wrote:

    Am 25.04.2010 20:41, schrieb Rens:

    Like SOT223 a device having 2 pins internally connected in the device.

    Sot224 pin 2 and 4(cooling pad) are the same.

    I supposed that connecting one pin it is also connected to the other.

    However, on the board a airwire still remains. This is also true for a

    sot223 device from the library.

    I tried the mailto:GND@1 etc. naming, but seems not to work.

    What am I doing wrong?

     

     

     

    Eagle does not know internal connections. So the rule is one pin for

    one pad. Some SO8 transistors have four drains which are internally

    connected. They are named D, D@1, d@2, D@3 in the library in this

    example. It would be ok, if you connect just one of these pins in the

    schematic and eagle would do the same in board.

    BUT, why should a manufactorer add more pads, if one is enough?

    Because the chip is connected to the pads with bonding wires and one

    wire is not thick enough to carry the amount of current specified in

    the data sheet. So two or more connections are used in parallel to

    carry the current. So you should see that all equal named pins are

    connected externally to avoid a "slow blowing fuse" device.

     

     

    What is the significance (if any) of using the "@" symbol in the example

    above.

     

    BTW, what I do in this situation is have GND1, GND2, GND3, .... as pin

    names on the symbol and then connect them all independently to "GND" on

    the schematic. Works well.

     

    The part following the '@' is not shown so that each looks like the same

    label pin.

     

    ...and gnd1, gnd2 or vdd1 and vdd2 etc. are usually different nets if

    you use an isolation amplifier for example image

     

    --

    Gruß / regards

     

    Joern

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
No Data
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.