Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Best capacitor library symbol for 80-C315C104M5U from polybot project?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 187 subscribers
  • Views 2336 views
  • Users 0 members are here
Related

Best capacitor library symbol for 80-C315C104M5U from polybot project?

autodeskguest
autodeskguest over 16 years ago

 

Hi,

 

I am playing with the polybot project which recommends using Eagle for

developing  its  circuit  board.   The  project  using  Kemet  ceramic

capacitors 80-C315C104M5U 0.1uF as decouple capacitors for the circuit

board ICs.   The capacitor package type  is C315.  How  do I determine

which Eagle  library capacitor symbol is  the best fit to  use for the

capacitor?   The cap  has just  two wires  coming off  it  so probably

anything reasonable would work, but is there a preferred selection?

 

Thanks for any suggestions and pointers.

 

marc

 

--

 

 

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 16 years ago

    "Warren Brayshaw" <warrenbrayshaw@paradise.net.nz> writes:

     

    >Hi,

    >I am playing with the polybot project which recommends using Eagle for

    >developing  its  circuit  board.   The  project  using  Kemet  ceramic

    >capacitors 80-C315C104M5U 0.1uF as decouple capacitors for the circuit

    >board ICs.   The capacitor package type  is C315.  How  do I determine

    >which Eagle  library capacitor symbol is  the best fit to  use for the

    >capacitor?   The cap  has just  two wires  coming off  it  so probably

    >anything reasonable would work, but is there a preferred selection?

     

     

    To find something suitable in the libraries

     

    From the Kemet data sheet:

    The C315 package has the following characteristics:

    Lead spacing 2.54mm (0.1")

    Lead diameter 0.51mm (0.020")

    Package width 3.81mm (0.15")

    Package thickness Std Voltage 2.54mm (0.1") , High Voltage 3.18mm (0.15")

     

    In the library rcl.lib select your capacitor symbol preference of either

    C-EU or C-US

    From the listed capacitors the ones that fit you size requirements have the

    package C025-024X044

    C025 = Capacitor with lead spacing of 2.5mm

    024X044 = tPlace depiction of package size 2.5 x 4.4mm.  This is a suitable

    match for the datasheet values of  2.54  x 3.18mm.

     

    Opening the library, check the drill diameter of the pads. In my library its

    0.032" which would suit the lead diameter of 0.020".

     

    Hope this helps

    Warren

     

     

    Thanks very much for all the replies.  They are very helpful.  I think

    I  understand how  you picked  out  the relevant  analogous part.   It

    needed  three attributes  to match  the minimum  value or  be slightly

    larger than the actual part specification.  I appreciate the pointers

    and explanation.

     

    Thank you.

     

    marc

     

    --

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 16 years ago

     

    >Hi,

    >I am playing with the polybot project which recommends using Eagle for

    >developing  its  circuit  board.   The  project  using  Kemet  ceramic

    >capacitors 80-C315C104M5U 0.1uF as decouple capacitors for the circuit

    >board ICs.   The capacitor package type  is C315.  How  do I determine

    >which Eagle  library capacitor symbol is  the best fit to  use for the

    >capacitor?   The cap  has just  two wires  coming off  it  so probably

    >anything reasonable would work, but is there a preferred selection?

     

     

    To find something suitable in the libraries

     

    From the Kemet data sheet:

    The C315 package has the following characteristics:

    Lead spacing 2.54mm (0.1")

    Lead diameter 0.51mm (0.020")

    Package width 3.81mm (0.15")

    Package thickness Std Voltage 2.54mm (0.1") , High Voltage 3.18mm (0.15")

     

    In the library rcl.lib select your capacitor symbol preference of either

    C-EU or C-US

    From the listed capacitors the ones that fit you size requirements have the

    package C025-024X044

    C025 = Capacitor with lead spacing of 2.5mm

    024X044 = tPlace depiction of package size 2.5 x 4.4mm.  This is a suitable

    match for the datasheet values of  2.54  x 3.18mm.

     

    Opening the library, check the drill diameter of the pads. In my library its

    0.032" which would suit the lead diameter of 0.020".

     

    Hope this helps

    Warren

     

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 16 years ago in reply to autodeskguest

    On Fri, 21 May 2010 08:49:35 -0400, Olin Lathrop <eagle@embedinc.com>

    wrote:

     

    Marc D Ronell wrote on Thu, 20 May 2010 23:03

    The  project  using  Kemet  ceramic capacitors 80-C315C104M5U 0.1uF as

    decouple capacitors for the circuit board ICs.   The capacitor package

    type  is C315.

     

    I don't know what a C315 package type is (are you sure that's not the

    component designator?), but if these are really decoupling caps there is a

    wide range of parts that would work well.

     

    Nowadays I use mostly 1uF caps for decoupling.  A 0805 or 0603 1uF cap

    right at the supply pin with a short return back to a ground pin on the IC

    has better characteristics than the 100nF leaded caps of a few years ago.

     

    In any case, the point is there are many many 100nF to 1uF ceramic caps

    that will fill the decoupling role.  You might as well use some that are

    available, cheap, and in a common package, like 0805 or 0603.

     

    Apparently the OP wants to use through-hole caps.  The part number he

    shows above can be found on mouser.

     

    Robert Scott

    Real-Time Specialties

    Ypsilanti, Michigan

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 16 years ago

    On Thu, 20 May 2010 23:03:26 -0400, Marc D Ronell

    <mronell@alumni.upenn.edu> wrote:

     

     

    Hi,

     

    I am playing with the polybot project which recommends using Eagle for

    developing  its  circuit  board.   The  project  using  Kemet  ceramic

    capacitors 80-C315C104M5U 0.1uF as decouple capacitors for the circuit

    board ICs.   The capacitor package type  is C315.  How  do I determine

    which Eagle  library capacitor symbol is  the best fit to  use for the

    capacitor?   The cap  has just  two wires  coming off  it  so probably

    anything reasonable would work, but is there a preferred selection?

     

    The choice of schematic symbol is mostly one of personal preference.

    There are European and US style symbols.  If you want to make the best

    use of the Eagle library, then look through the rcl.lib library for a

    device that has the schematic symbol you prefer and the circuit board

    package that matches the capacitor you have choosen.   Everything else

    can be changed (like the part value) after the device is placed into

    your design.  It seems that the part you specified has leads .1"

    apart.  Just look at the through-hole packages in rcl to find one that

    provides this spacing and the proper clearance around the pins.  If

    you cannot find a close enough match, then copy a close device into a

    new temporary library and then edit that copy in the library to change

    what you need.  Then copy the revised part into a custom library that

    you create for this project.  But most likely you will find a stock

    part that fits your needs.

     

     

    Robert Scott

    Real-Time Specialties

    Ypsilanti, Michigan

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 16 years ago

    Marc D Ronell wrote on Thu, 20 May 2010 23:03

    The  project  using  Kemet  ceramic capacitors 80-C315C104M5U 0.1uF as

    decouple capacitors for the circuit board ICs.   The capacitor package

    type  is C315.

     

    I don't know what a C315 package type is (are you sure that's not the

    component designator?), but if these are really decoupling caps there is a

    wide range of parts that would work well.

     

    Nowadays I use mostly 1uF caps for decoupling.  A 0805 or 0603 1uF cap

    right at the supply pin with a short return back to a ground pin on the IC

    has better characteristics than the 100nF leaded caps of a few years ago.

     

    In any case, the point is there are many many 100nF to 1uF ceramic caps

    that will fill the decoupling role.  You might as well use some that are

    available, cheap, and in a common package, like 0805 or 0603.

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.