Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Best capacitor library symbol for 80-C315C104M5U from polybot project?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 187 subscribers
  • Views 2338 views
  • Users 0 members are here
Related

Best capacitor library symbol for 80-C315C104M5U from polybot project?

autodeskguest
autodeskguest over 16 years ago

 

Hi,

 

I am playing with the polybot project which recommends using Eagle for

developing  its  circuit  board.   The  project  using  Kemet  ceramic

capacitors 80-C315C104M5U 0.1uF as decouple capacitors for the circuit

board ICs.   The capacitor package type  is C315.  How  do I determine

which Eagle  library capacitor symbol is  the best fit to  use for the

capacitor?   The cap  has just  two wires  coming off  it  so probably

anything reasonable would work, but is there a preferred selection?

 

Thanks for any suggestions and pointers.

 

marc

 

--

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 16 years ago

     

    >Hi,

    >I am playing with the polybot project which recommends using Eagle for

    >developing  its  circuit  board.   The  project  using  Kemet  ceramic

    >capacitors 80-C315C104M5U 0.1uF as decouple capacitors for the circuit

    >board ICs.   The capacitor package type  is C315.  How  do I determine

    >which Eagle  library capacitor symbol is  the best fit to  use for the

    >capacitor?   The cap  has just  two wires  coming off  it  so probably

    >anything reasonable would work, but is there a preferred selection?

     

     

    To find something suitable in the libraries

     

    From the Kemet data sheet:

    The C315 package has the following characteristics:

    Lead spacing 2.54mm (0.1")

    Lead diameter 0.51mm (0.020")

    Package width 3.81mm (0.15")

    Package thickness Std Voltage 2.54mm (0.1") , High Voltage 3.18mm (0.15")

     

    In the library rcl.lib select your capacitor symbol preference of either

    C-EU or C-US

    From the listed capacitors the ones that fit you size requirements have the

    package C025-024X044

    C025 = Capacitor with lead spacing of 2.5mm

    024X044 = tPlace depiction of package size 2.5 x 4.4mm.  This is a suitable

    match for the datasheet values of  2.54  x 3.18mm.

     

    Opening the library, check the drill diameter of the pads. In my library its

    0.032" which would suit the lead diameter of 0.020".

     

    Hope this helps

    Warren

     

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 16 years ago

     

    >Hi,

    >I am playing with the polybot project which recommends using Eagle for

    >developing  its  circuit  board.   The  project  using  Kemet  ceramic

    >capacitors 80-C315C104M5U 0.1uF as decouple capacitors for the circuit

    >board ICs.   The capacitor package type  is C315.  How  do I determine

    >which Eagle  library capacitor symbol is  the best fit to  use for the

    >capacitor?   The cap  has just  two wires  coming off  it  so probably

    >anything reasonable would work, but is there a preferred selection?

     

     

    To find something suitable in the libraries

     

    From the Kemet data sheet:

    The C315 package has the following characteristics:

    Lead spacing 2.54mm (0.1")

    Lead diameter 0.51mm (0.020")

    Package width 3.81mm (0.15")

    Package thickness Std Voltage 2.54mm (0.1") , High Voltage 3.18mm (0.15")

     

    In the library rcl.lib select your capacitor symbol preference of either

    C-EU or C-US

    From the listed capacitors the ones that fit you size requirements have the

    package C025-024X044

    C025 = Capacitor with lead spacing of 2.5mm

    024X044 = tPlace depiction of package size 2.5 x 4.4mm.  This is a suitable

    match for the datasheet values of  2.54  x 3.18mm.

     

    Opening the library, check the drill diameter of the pads. In my library its

    0.032" which would suit the lead diameter of 0.020".

     

    Hope this helps

    Warren