Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Exporting pad data for Phoenix X-ray machine
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 188 subscribers
  • Views 1195 views
  • Users 0 members are here
Related

Exporting pad data for Phoenix X-ray machine

autodeskguest
autodeskguest over 12 years ago

Hi all, we have Phoenix Micromex 180 x-ray machine for PCB inspection at

my workplace. Its software can greatly automate creation of new

inspection programs for boards, but as an input, it requires data with

component and pad coordinates. Two separate files are needed: 1. one

which lists all components, their names, package type and coordinates.

2. one which lists pad shapes and coordinates (relative to package's

origin mark) for all package types used on a board. Here are shortened

examples of needed file contents:

 

Component file:

  1. Board dimensions: X size, Y size, layer height

DIMENSIONS: 130 90 1.6

  1. RefDes    PackageID    X-shift    Y-shift    ROT    PinCount   

Side    MountType

C7               27    30    50    0    2    TOP       THROUGH  

R7               26    121    51    0    2    TOP       THROUGH  

V18             19    23    40    0    3    TOP       SMD      

C58             14    99    7    90    2    TOP       SMD      

V30             16    6    63    0    2    TOP       SMD      

V15             19    23    20    0    3    TOP       SMD      

C8               27    30    45    0    2    TOP       THROUGH  

C43             13    104    77    0    2    TOP       SMD      

 

Pad coordinates file:

PackageID    label    X-shift    Y-shift    Rotation    Width   

Height    Shape

6    1    -0.65    0    0    0.9    0.7    RECTANGLE

6    2    0.65    0    0    0.9    0.7    RECTANGLE

15    A    -1.7    0    90    1.8    1.4    OBLONG

15    K    1.7    0    90    1.8    1.4    OBLONG

22    A1    -12.06    12.06    0    0.6    0    ROUND

22    A10    -0.63    12.06    0    0.6    0    ROUND

22    A11    0.63    12.06    0    0.6    0    ROUND

22    A12    1.9    12.06    0    0.6    0    ROUND

22    A13    3.17    12.06    0    0.6    0    ROUND

27    1    -1.25    0    0    1.3    0    ROUND

27    2    1.25    0    0    1.3    0    ROUND

 

Obviously, the most "clean" solution would be to write my own ULP to

generate the files. But that would be very time-consuming, so I want to

try some alternative solutions before I do that. I figured the component

file could be easily obtained by editing the standard Eagle partlist,

for example by a relatively simple MS Excel macro. But I found no way

how to obtain the pad data, or at least not in the format needed. I know

there is export-ict-netlist-pad-coordinates.ulp, but this one exports

the pad coordinates relative to the entire board, not relative to

package's origin mark. And the information about pad shape is missing

completely in it.

 

So my question is: *is there some existing ULP which can produce such

pad data*?

 

Just in case you were interested, here is some info about our x-ray

machine:

http://www.ge-mcs.com/en/radiography-x-ray/micro-and-nanofocus/micromex-dxr-hd.html

 

--

To view any images and attachments in this post, visit:

http://www.element14.com/community/message/93087#93087

 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 10 years ago

    In case anyone was interested, I tasked one of my students to create an ULP that does exactly this. It's named "export-phoenix-x-ray-cad-data.ulp" and can be found on Cadsoft's ULP download page.

     

    Perhaps more importantly, the same student also created free "ODB++ to Phoenix X-ray CAD data converter", which allows you to generate the Phoenix CAD data from many other PCB layout editors (Altium, Allegro, Orcad, Protel, Expedition...), as long as they have ODB++ export. The converter runs in Java, and you can download the latest version from his Github repository (you only need the ODBtoRTG.jar file):

     

    https://github.com/popelavojtech/ODB-to-Phoenix-X-ray-CAD-data-converter

     

    The converter itself is simple to use, but you may encounter several problems while generating the ODB++ data, particularly on Cadence products. So I created an English help page, which can be found here:

     

    http://odbconverter.xf.cz/

     

    The CAD data should work on all Phoenix/GE machines that run the Xact software. Currently, it's Phoenix Xaminer, Micromex and Nanomex, though there may be others I'm unaware of. Note that only Xact Pro version currently supports CAD data import.

     

    If you have any questions of feature requests, please contact the student directly. While I was his supervisor (and betatester), he is the sole creator of the converter itself.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 10 years ago

    In case anyone was interested, I tasked one of my students to create an ULP that does exactly this. It's named "export-phoenix-x-ray-cad-data.ulp" and can be found on Cadsoft's ULP download page.

     

    Perhaps more importantly, the same student also created free "ODB++ to Phoenix X-ray CAD data converter", which allows you to generate the Phoenix CAD data from many other PCB layout editors (Altium, Allegro, Orcad, Protel, Expedition...), as long as they have ODB++ export. The converter runs in Java, and you can download the latest version from his Github repository (you only need the ODBtoRTG.jar file):

     

    https://github.com/popelavojtech/ODB-to-Phoenix-X-ray-CAD-data-converter

     

    The converter itself is simple to use, but you may encounter several problems while generating the ODB++ data, particularly on Cadence products. So I created an English help page, which can be found here:

     

    http://odbconverter.xf.cz/

     

    The CAD data should work on all Phoenix/GE machines that run the Xact software. Currently, it's Phoenix Xaminer, Micromex and Nanomex, though there may be others I'm unaware of. Note that only Xact Pro version currently supports CAD data import.

     

    If you have any questions of feature requests, please contact the student directly. While I was his supervisor (and betatester), he is the sole creator of the converter itself.