Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) V7.5 slow graphics
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 189 subscribers
  • Views 1112 views
  • Users 0 members are here
Related

V7.5 slow graphics

Joop14
Joop14 over 10 years ago

I'm still using v6.60 but I decided (again) to give v7 a try so I installed v7.5.

 

I noticed immediately that the graphics engine is much slower.

Panning (keeping the middle mouse button pressed and moving the mouse) is super smooth with v6.60.

With v7.5 it's sluggish. I'm back to v6.60.

 

I hope you can fix this.

 

Kind Regards.

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 10 years ago

    Am 17.04.2016 um 09:44 schrieb Joop14:

    I'm still using v6.60 but I decided (again) to give v7 a try so I

    installed v7.5.

     

    I noticed immediately that the graphics engine is much slower.

    Panning (keeping the middle mouse button pressed and moving the mouse)

    is super smooth with v6.60.

    With v7.5 it's sluggish. I'm back to v6.60.

     

    I hope you can fix this.

     

    Kind Regards.

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/194924

     

     

     

    This is not a common problem. Could you give us some more details

    about operating system and graphics card and drivers?

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Joop14
    Joop14 over 10 years ago in reply to autodeskguest

    I tested it on two different brands of computers. One is a Fujitsu, the other one an Asus. Both have an Ati/AMD graphics card (5000 series).

     

    Software is the same for both computers: Opensuse 13.2 64-bit, graphics driver: radeon

     

    Eagle version is v7.5 64-bit.

     

    uname -a: Linux Joop 3.16.7-35-desktop #1 SMP PREEMPT Sun Feb 7 17:32:21 UTC 2016 (832c776) x86_64 x86_64 x86_64 GNU/Linux

     

    The output below is from the Fujitsu:

     

    01:00.0 VGA compatible controller [0300]: Advanced Micro Devices, Inc. [AMD/ATI] Park [Mobility Radeon HD 5430] [1002:68e1]

            Subsystem: PC Partner Limited / Sapphire Technology Caicos [Radeon HD 5450] [174b:6000]

            Kernel driver in use: radeon

            Kernel modules: radeon

     

     

    [1.778514] [drm] radeon kernel modesetting enabled.
    [1.778555] fb: switching to radeondrmfb from VESA VGA
    [1.778921] radeon 0000:01:00.0: VRAM: 1024M 0x0000000000000000 - 0x000000003FFFFFFF (1024M used)
    [1.778923] radeon 0000:01:00.0: GTT: 1024M 0x0000000040000000 - 0x000000007FFFFFFF
    [1.779365] [drm] radeon: 1024M of VRAM memory ready
    [1.779366] [drm] radeon: 1024M of GTT memory ready.
    [1.802386] [drm] radeon: dpm initialized
    [1.803065] [drm] enabling PCIE gen 2 link speeds, disable with radeon.pcie_gen2=0
    [1.836161] radeon 0000:01:00.0: WB enabled
    [1.836163] radeon 0000:01:00.0: fence driver on ring 0 use gpu addr 0x0000000040000c00 and cpu addr 0xffff880036c33c00
    [1.836164] radeon 0000:01:00.0: fence driver on ring 3 use gpu addr 0x0000000040000c0c and cpu addr 0xffff880036c33c0c
    [1.836953] radeon 0000:01:00.0: fence driver on ring 5 use gpu addr 0x000000000005c418 and cpu addr 0xffffc90010f1c418
    [1.836976] radeon 0000:01:00.0: irq 45 for MSI/MSI-X
    [1.836984] radeon 0000:01:00.0: radeon: using MSI.
    [1.837005] [drm] radeon: irq initialized.
    [2.357680] fbcon: radeondrmfb (fb0) is primary device
    [2.384926] radeon 0000:01:00.0: fb0: radeondrmfb frame buffer device
    [2.384927] radeon 0000:01:00.0: registered panic notifier
    [2.388014] [drm] Initialized radeon 2.39.0 20080528 for 0000:01:00.0 on minor 0

     

    Edit: I tested it with a 6 layer board with about 500 components. Most layers active, polygons (fill) ripped up.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcv
    mcv over 10 years ago in reply to Joop14

    Eagle is generally very slow for me when panning, but I noticed that only after I switched to 4K monitor. On 1080p it worked well for me. Hiding grid helps a little bit. I have Intel integrated graphics on a Broadwell CPU, running on Intel driver on Linux.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Joop14
    Joop14 over 10 years ago in reply to autodeskguest

    Thanks Richard, for confirming this.

     

    Regards.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to Joop14

    Am 26.04.2016 um 09:32 schrieb Joop14:

    Hello Jorge, I hope you are doing well.

     

    Thank you for looking into this.

     

    In order to reproduce the problem, install Opensuse 13.2 directly on a

    pc, without using a virtual machine.

     

    http://download.opensuse.org/distribution/13.2/iso/openSUSE-13.2-DVD-x86_64.iso

     

     

    Also, make sure your pc contains an Ati/AMD radeon graphics card.

     

    Kind Regards,

     

    Joop

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/195623

     

     

     

    Hi,

     

    there are differences between EAGLE 6.6 and 7 in Linux, true.

    It is a matter of the Qt development environment. The newer versions

    are not better here. We had some improvements with 7.3.0, but is not

    as it was before. We still have it on the radar. Even the latest Qt

    release did not solve the problem.

    I have a similar system (SuSe 13.2, Radeon graphics) and have the same

    experience.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 10 years ago in reply to Joop14

    Am 26.04.2016 um 09:32 schrieb Joop14:

    Hello Jorge, I hope you are doing well.

     

    Thank you for looking into this.

     

    In order to reproduce the problem, install Opensuse 13.2 directly on a

    pc, without using a virtual machine.

     

    http://download.opensuse.org/distribution/13.2/iso/openSUSE-13.2-DVD-x86_64.iso

     

     

    Also, make sure your pc contains an Ati/AMD radeon graphics card.

     

    Kind Regards,

     

    Joop

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/195623

     

     

     

    Hi,

     

    there are differences between EAGLE 6.6 and 7 in Linux, true.

    It is a matter of the Qt development environment. The newer versions

    are not better here. We had some improvements with 7.3.0, but is not

    as it was before. We still have it on the radar. Even the latest Qt

    release did not solve the problem.

    I have a similar system (SuSe 13.2, Radeon graphics) and have the same

    experience.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Joop14
    Joop14 over 10 years ago in reply to autodeskguest

    Thanks Richard, for confirming this.

     

    Regards.