EAGLE User Support (English) [Suggestions]Create oblong pad and oblong hole with any dimension
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
  • Replies 5 replies
  • Subscribers 179 subscribers
  • Views 1881 views
  • Users 0 members are here
Related

[Suggestions]Create oblong pad and oblong hole with any dimension

Former Member
Former Member over 10 years ago

Hello,

 

I have a suggestion for you. You should have a function that allows users can create oblong pad and oblong hole with any dimension like Orcad and Altium, for through-hole components. There are many components need oblong pad and oblong holes nowadays. For examples, this component need oblong pad and oblong hole.

http://www.shori.com.tw/eng/product_detial.php?id=19

 

With Orcad, users can adjust pad with and pad height of oblong pad. Sometimes, users only need oblong pad long and narrow, not too big like EALGE does.

b4.gif

With Altium, users can create hole, pad with any shape.

 

Support for Rectangular Pad Holes | Online Documentation for Altium Products

 

I think you really must have this function in new version if you don't want users use Altium replace EAGLE because you only don't have this function. Don't tell that the boardhouse can not create oblong hole to the users! They can!

 

A topic was created on Mar 10th, 2015, but there is no one reply that topic. [WISH] EAGLE has pad height, pad width option in new version

 

Waiting for your respond!

 

Thank you for reading!

 

Best regards!

  • Sign in to reply
  • Cancel
  • kikoun
    kikoun over 10 years ago

    Hi,

     

    For the oblong hole, we already can do it (metalized or not)  in eagle but it's not very simple (manually add drawing in milling layer, indications for PCB house to indicate that which milling line need to be plated and which don't  (there is only one layer for milling !) etc...)

     

    For the pad it self, we already can produce any shape, just by drawing a copper polygon around your pad !

     

    But you're right, the pad configuration could support little enhancement that would make it easier, and powerful too (separate diameter for top/bottom, separate Mask option for top/bottom etc...)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago

    Gabriel Gabriel wrote:

     

    Hello,

     

    I have a suggestion for you. You should have a function that allows

    users can create oblong pad and oblong hole with any dimension like

    Orcad and Altium, for through-hole components. There are many components

    need oblong pad and oblong holes nowadays. For examples, this component

    need oblong pad and oblong hole.

    http://www.shori.com.tw/eng/product_detial.php?id=19

     

    With Orcad, users can adjust pad with and pad height of oblong pad.

    Sometimes, users only need oblong pad long and narrow, not too big like

    EALGE does.

    With Altium, users can create hole, pad with any shape.

     

    Support for Rectangular Pad Holes | Online Documentation for Altium

    Products

     

    (http://techdocs.altium.com/display/ADOH/SupportforRectangularPadHoles)

     

    I think you really must have this function in new version if you don't

    want users use Altium replace EAGLE because you only don't have this

    function. Don't tell that the boardhouse can not create oblong hole to

    the users! They can!

     

    A topic was created on Mar 10th, 2015, but there is no one reply that

    topic.

     

    Waiting for your respond!

     

    Thank you for reading!

     

    Best regards!

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/162551

     

    In the past, oblong holes basically meant the holes had to be milled out

    (obviously one cannot drill oblong holes except by accident) at a usually

    significant extra cost. Where are you folks that are using oblong holes

    getting your boards made, and how much of a premium do you have to pay for

    using oblong holes? Are they primarily used by hobbyists doing their own

    milling, or by the military/industrial folks with unlimited budgets? Or is

    the increasing use of laser cutting making oblong holes an affordable option

    these days? I'd love to know. Thanks.

     

    Bob

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kikoun
    kikoun over 10 years ago in reply to autodeskguest

    Hi Bob,

     

    Oblong plated holes still have extra cost, because the milling need to be done before plating, so it can not be done while milling the outline of the board.

    If not plated, the oblong hole can be done during the milling the outline of the board, and there is no extra cost (if it can be done with same tool (same diameter)).

     

    I don't know about the laser cutting, but I think that don't solve the problem of doing it before the plating process. And I don't know if a laser cut is better than a milled one, because I know that one of the main problem with plating it to have  a very clean cut... if some one know ... it can tell us (I'm curious...)

     

    Anyway, I avoid plated oblong for that extra cost, but a couple of time I had to use them, since some connector need oblong, and I didn't had choice of the connector....

     

    The price of that extra cost depend on the house board, on how many board you buy etc....

     

    Guillaume.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to kikoun

    Guillaume barrey wrote:

     

    Hi Bob,

     

    Oblong plated holes still have extra cost, because the milling need to

    be done before plating, so it can not be done while milling the outline

    of the board.

    If not plated, the oblong hole can be done during the milling the

    outline of the board, and there is no extra cost (if it can be done with

    same tool (same diameter)).

     

    I don't know about the laser cutting, but I think that don't solve the

    problem of doing it before the plating process. And I don't know if a

    laser cut is better than a milled one, because I know that one of the

    main problem with plating it to have  a very clean cut... if some one

    know ... it can tell us (I'm curious...)

     

    Anyway, I avoid plated oblong for that extra cost, but a couple of time

    I had to use them, since some connector need oblong, and I didn't had

    choice of the connector....

     

    The price of that extra cost depend on the house board, on how many

    board you buy etc....

     

    Guillaume.

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/163585

     

    Thanks for the reply. Most oblong holes I've encountered on connectors are

    primarily an artifact of the manufacturing process of the connector; namely,

    the manufacturer uses a punched-out and bent piece of the sheet-metal shell

    as a leg. In most cases these are primarily shell ground connections and/or

    mounting tabs, and simply using the nearest round drill diameter that will

    fit the tab does the intended job. However, as these connectors get smaller

    and smaller, that extra radius can start blocking routing channels out of

    the connector pins, so I'm always interested in hearing from folks who may

    have found ways to manufacture non-round 'drills' at less cost than milling.

    Once that process is available, I'll be right there with you pushing Cadsoft

    to give us that oblong functionality.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kikoun
    kikoun over 10 years ago in reply to autodeskguest

    Hi,

    I don't expect a oblong hole functionality since in my several years experience I only used oblong holes twice !

    And it was small connector (a USB connector) )with a shell-leg, too near other pads, so a bigger round hole was impossible.

     

    I have the feeling that, connector manufacturers become aware that and now try to avoid  the need of oblong holes. It's just an feeling, I may be wrong...

    Any way, I'm aware of that, and I take in to account this kind of details in my designs when I choose connector (or other part).

     

    So I think it would certainly be easier to have a Oblong hole functionality, but I think it really not a priority, other improvements such as separate diameter for top/bottom, separate Mask option for top/bottom.... are more interesting....

     

    Guillaume