EAGLE User Support (English) [Suggestions]Create oblong pad and oblong hole with any dimension
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
  • Replies 5 replies
  • Subscribers 179 subscribers
  • Views 1885 views
  • Users 0 members are here
Related

[Suggestions]Create oblong pad and oblong hole with any dimension

Former Member
Former Member over 10 years ago

Hello,

 

I have a suggestion for you. You should have a function that allows users can create oblong pad and oblong hole with any dimension like Orcad and Altium, for through-hole components. There are many components need oblong pad and oblong holes nowadays. For examples, this component need oblong pad and oblong hole.

http://www.shori.com.tw/eng/product_detial.php?id=19

 

With Orcad, users can adjust pad with and pad height of oblong pad. Sometimes, users only need oblong pad long and narrow, not too big like EALGE does.

b4.gif

With Altium, users can create hole, pad with any shape.

 

Support for Rectangular Pad Holes | Online Documentation for Altium Products

 

I think you really must have this function in new version if you don't want users use Altium replace EAGLE because you only don't have this function. Don't tell that the boardhouse can not create oblong hole to the users! They can!

 

A topic was created on Mar 10th, 2015, but there is no one reply that topic. [WISH] EAGLE has pad height, pad width option in new version

 

Waiting for your respond!

 

Thank you for reading!

 

Best regards!

  • Sign in to reply
  • Cancel
Parents
  • kikoun
    kikoun over 10 years ago

    Hi,

     

    For the oblong hole, we already can do it (metalized or not)  in eagle but it's not very simple (manually add drawing in milling layer, indications for PCB house to indicate that which milling line need to be plated and which don't  (there is only one layer for milling !) etc...)

     

    For the pad it self, we already can produce any shape, just by drawing a copper polygon around your pad !

     

    But you're right, the pad configuration could support little enhancement that would make it easier, and powerful too (separate diameter for top/bottom, separate Mask option for top/bottom etc...)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • kikoun
    kikoun over 10 years ago

    Hi,

     

    For the oblong hole, we already can do it (metalized or not)  in eagle but it's not very simple (manually add drawing in milling layer, indications for PCB house to indicate that which milling line need to be plated and which don't  (there is only one layer for milling !) etc...)

     

    For the pad it self, we already can produce any shape, just by drawing a copper polygon around your pad !

     

    But you're right, the pad configuration could support little enhancement that would make it easier, and powerful too (separate diameter for top/bottom, separate Mask option for top/bottom etc...)