Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) re-touch:More than 16 layers
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 187 subscribers
  • Views 718 views
  • Users 0 members are here
Related

re-touch:More than 16 layers

autodeskguest
autodeskguest over 10 years ago

With the project I am working on, I'm starting to feel some pain about

the lack of more than 16 layers. I know I can most likely virtualize

some inner gnd-only layers (cloning the gerbers) but I'd like to ask

about the plans for this feature.

 

At the same time I know there are some challenges for the ones that work

with that many layers. First of all I'm thinking about polygon

processing speeds causing reluctance to do ratsnest until absolutely

necessary, but when doing power routing, it will need frequent fill

tests, but even doing ratsnest on a single net takes time. I wish this

function became more "live", so airwires would appeare instantly as you

place a via. My gut feeling as a programmer is that this is possbile to

speed up alot.

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 10 years ago

    Am 03.05.2016 um 12:27 schrieb Morten Leikvoll:

    On 02.05.2016 21:14, warrenbrayshaw wrote:

    On 3/05/2016 3:28 a.m., Richard Hammerl wrote:

    Am 29.04.2016 um 08:41 schrieb Morten Leikvoll:

    With the project I am working on, I'm starting to feel some pain about

    the lack of more than 16 layers. I know I can most likely virtualize

    some inner gnd-only layers (cloning the gerbers) but I'd like to ask

    about the plans for this feature.

     

    At the same time I know there are some challenges for the ones that

    work

    with that many layers. First of all I'm thinking about polygon

    processing speeds causing reluctance to do ratsnest until absolutely

    necessary, but when doing power routing, it will need frequent fill

    tests, but even doing ratsnest on a single net takes time. I wish this

    function became more "live", so airwires would appeare instantly as you

    place a via. My gut feeling as a programmer is that this is possbile to

    speed up alot.

     

     

    Currently we have no fixed plans for this. But we already put your

    request into our bugzilla system as a possible feature for V8.

     

     

     

    The discussion from Sept 2010 is well worth re-reading on this subject.

    Particularly James's words on the decision making process to purchase.

     

    http://www.eaglecentral.ca/index.php/mv/msg/38634/129058/736ed5d7e6ef3b087cee2f741a79e2e5/#msg_129058

     

     

    Thanks for linking this old thread. I was the actual first one to

    respond to this thread[, apparently with a too complex solution].

     

    If Klaus worries are still the main worry, I have a much simpler

    solution that allows Cadsoft wants to keep the old structure, and

    addresses some concerns from the old thread.

     

    New projects on a new buture version could have an checkable "extended

    layer" mode in the stack setup. This feature will shift layers like

    Klaus suggested in the old thread. If this checkbox is not set,

    everything should work as before. When old projects are loaded/imported,

    this checkbox will ofcourse be cleared.

     

    For projects in "extended layer mode", all ULP's that work with extended

    layer modes would need a "#using extended_layermode" at the top. If an

    ULP without this key is run on a board in extended mode, an error like

    "This ULP is unsuitable for extended layer mode." should pop up. An old

    ULP would run as before on a non-extended layermode design.

     

     

    If you wonder why I need 16+, its because I'm working on a rather dense

    design with a 1500+ pin FPGA, more than 9 rather high current voltage

    rails (0.95V, 1.00V, 1.2v, 1.5v, 1.8v, 2.5v, 3.3v, 5v and 12v) , 256 bit

    (16x16) wide DDR4 memory at state of the art speed, 48 gigabit

    tranceivers (diff lanes of 8 gigabit), and you simply dont experiment

    with layer crossing with that kind of routing, especially not whe using

    Eagle where the simulation is not built in. (Yes I do have some ULP's to

    help me out here)

    I will probably manage to crowbar this in to 16 layers on this project,

    but the added comfort and time and blood saved in trial and error would

    be much valuable. Switching to a new tool is even more painful/time

    consuming. I would have to replace the man drawing it too.

     

     

    We will discuss this again for V8. There would be a lot of

    incompatabilities with the new additional signal layers. But we will

    check Klaus' and your ideas and see what will come out. We do not have

    too many customers that want to use more layers, but let's see if the

    pros justify the cons.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to autodeskguest

    CadSoft Support wrote on Wed, 04 May 2016 07:16

    Am 03.05.2016 um 12:27 schrieb Morten Leikvoll:

    On 02.05.2016 21:14, warrenbrayshaw wrote:

    On 3/05/2016 3:28 a.m., Richard Hammerl wrote:

    Am 29.04.2016 um 08:41 schrieb Morten Leikvoll:

    With the project I am working on, I'm starting to feel some pain

    about

    the lack of more than 16 layers. I know I can most likely

    virtualize

    some inner gnd-only layers (cloning the gerbers) but I'd like to

    ask

    about the plans for this feature.

     

    At the same time I know there are some challenges for the ones

    that

    work

    with that many layers. First of all I'm thinking about polygon

    processing speeds causing reluctance to do ratsnest until

    absolutely

    necessary, but when doing power routing, it will need frequent

    fill

    tests, but even doing ratsnest on a single net takes time. I wish

    this

    function became more "live", so airwires would appeare instantly

    as you

    place a via. My gut feeling as a programmer is that this is

    possbile to

    speed up alot.

     

     

    Currently we have no fixed plans for this. But we already put

    your

    request into our bugzilla system as a possible feature for V8.

     

     

     

    The discussion from Sept 2010 is well worth re-reading on this

    subject.

    Particularly James's words on the decision making process to

    purchase.

     

     

    http://www.eaglecentral.ca/index.php/mv/msg/38634/129058/736ed5d7e6ef3b087c

    ee2f741a79e2e5/#msg_129058

     

    Thanks for linking this old thread. I was the actual first one to

    respond to this thread[, apparently with a too complex solution].

     

    If Klaus worries are still the main worry, I have a much simpler

    solution that allows Cadsoft wants to keep the old structure, and

    addresses some concerns from the old thread.

     

    New projects on a new buture version could have an checkable

    "extended

    layer" mode in the stack setup. This feature will shift layers

    like

    Klaus suggested in the old thread. If this checkbox is not set,

    everything should work as before. When old projects are

    loaded/imported,

    this checkbox will ofcourse be cleared.

     

    For projects in "extended layer mode", all ULP's that work with

    extended

    layer modes would need a "#using extended_layermode" at the top.

    If an

    ULP without this key is run on a board in extended mode, an error

    like

    "This ULP is unsuitable for extended layer mode." should pop up.

    An old

    ULP would run as before on a non-extended layermode design.

     

     

    If you wonder why I need 16+, its because I'm working on a rather

    dense

    design with a 1500+ pin FPGA, more than 9 rather high current

    voltage

    rails (0.95V, 1.00V, 1.2v, 1.5v, 1.8v, 2.5v, 3.3v, 5v and 12v) ,

    256 bit

    (16x16) wide DDR4 memory at state of the art speed, 48 gigabit

    tranceivers (diff lanes of 8 gigabit), and you simply dont

    experiment

    with layer crossing with that kind of routing, especially not whe

    using

    Eagle where the simulation is not built in. (Yes I do have some

    ULP's to

    help me out here)

    I will probably manage to crowbar this in to 16 layers on this

    project,

    but the added comfort and time and blood saved in trial and error

    would

    be much valuable. Switching to a new tool is even more

    painful/time

    consuming. I would have to replace the man drawing it too.

     

     

    We will discuss this again for V8. There would be a lot of

    incompatabilities with the new additional signal layers. But we will

    check Klaus' and your ideas and see what will come out. We do not have

    too many customers that want to use more layers, but let's see if the

    pros justify the cons.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

     

     

    That last statement is a self-fulfilling prophecy.  Most people who think

    they will have boards that approach and may exceed 16 layers simply choose

    another CAD package.  They aren't going to even consider EAGLE since they

    can't be sure that it will be able to handle their full requirements.

     

    That's the wrong question to ask.  The question to ask is how much market

    share can we add by increasing the number of layers i.e. how many people

    would choose EAGLE IF it supported more layers.  But that question misses

    too.  If you are routing 16+ layers then you most likely have many, many

    differential pairs and a bunch of length matching (like Morten's board

    above).  Until you have true, polished support for those design elements no

    one is going to choose EAGLE for those types of boards--the effort is

    simply too big when other tools do a lot to help.  So you have to address

    ALL of the design elements and then someone can consider EAGLE.  Until that

    happens you can't use stats from your current user base to see what support

    it would have because your current user base choose EAGLE in spite of it

    not supporting these requirements--so obviously they don't think it's

    important.

     

    James.

     

    --

    James Morrison  ~~~  Stratford Digital

     

    Order your EAGLE license from Stratford Digital at

    http://www.eaglelicenses.com

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 10 years ago in reply to autodeskguest

    CadSoft Support wrote on Wed, 04 May 2016 07:16

    Am 03.05.2016 um 12:27 schrieb Morten Leikvoll:

    On 02.05.2016 21:14, warrenbrayshaw wrote:

    On 3/05/2016 3:28 a.m., Richard Hammerl wrote:

    Am 29.04.2016 um 08:41 schrieb Morten Leikvoll:

    With the project I am working on, I'm starting to feel some pain

    about

    the lack of more than 16 layers. I know I can most likely

    virtualize

    some inner gnd-only layers (cloning the gerbers) but I'd like to

    ask

    about the plans for this feature.

     

    At the same time I know there are some challenges for the ones

    that

    work

    with that many layers. First of all I'm thinking about polygon

    processing speeds causing reluctance to do ratsnest until

    absolutely

    necessary, but when doing power routing, it will need frequent

    fill

    tests, but even doing ratsnest on a single net takes time. I wish

    this

    function became more "live", so airwires would appeare instantly

    as you

    place a via. My gut feeling as a programmer is that this is

    possbile to

    speed up alot.

     

     

    Currently we have no fixed plans for this. But we already put

    your

    request into our bugzilla system as a possible feature for V8.

     

     

     

    The discussion from Sept 2010 is well worth re-reading on this

    subject.

    Particularly James's words on the decision making process to

    purchase.

     

     

    http://www.eaglecentral.ca/index.php/mv/msg/38634/129058/736ed5d7e6ef3b087c

    ee2f741a79e2e5/#msg_129058

     

    Thanks for linking this old thread. I was the actual first one to

    respond to this thread[, apparently with a too complex solution].

     

    If Klaus worries are still the main worry, I have a much simpler

    solution that allows Cadsoft wants to keep the old structure, and

    addresses some concerns from the old thread.

     

    New projects on a new buture version could have an checkable

    "extended

    layer" mode in the stack setup. This feature will shift layers

    like

    Klaus suggested in the old thread. If this checkbox is not set,

    everything should work as before. When old projects are

    loaded/imported,

    this checkbox will ofcourse be cleared.

     

    For projects in "extended layer mode", all ULP's that work with

    extended

    layer modes would need a "#using extended_layermode" at the top.

    If an

    ULP without this key is run on a board in extended mode, an error

    like

    "This ULP is unsuitable for extended layer mode." should pop up.

    An old

    ULP would run as before on a non-extended layermode design.

     

     

    If you wonder why I need 16+, its because I'm working on a rather

    dense

    design with a 1500+ pin FPGA, more than 9 rather high current

    voltage

    rails (0.95V, 1.00V, 1.2v, 1.5v, 1.8v, 2.5v, 3.3v, 5v and 12v) ,

    256 bit

    (16x16) wide DDR4 memory at state of the art speed, 48 gigabit

    tranceivers (diff lanes of 8 gigabit), and you simply dont

    experiment

    with layer crossing with that kind of routing, especially not whe

    using

    Eagle where the simulation is not built in. (Yes I do have some

    ULP's to

    help me out here)

    I will probably manage to crowbar this in to 16 layers on this

    project,

    but the added comfort and time and blood saved in trial and error

    would

    be much valuable. Switching to a new tool is even more

    painful/time

    consuming. I would have to replace the man drawing it too.

     

     

    We will discuss this again for V8. There would be a lot of

    incompatabilities with the new additional signal layers. But we will

    check Klaus' and your ideas and see what will come out. We do not have

    too many customers that want to use more layers, but let's see if the

    pros justify the cons.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

     

     

    That last statement is a self-fulfilling prophecy.  Most people who think

    they will have boards that approach and may exceed 16 layers simply choose

    another CAD package.  They aren't going to even consider EAGLE since they

    can't be sure that it will be able to handle their full requirements.

     

    That's the wrong question to ask.  The question to ask is how much market

    share can we add by increasing the number of layers i.e. how many people

    would choose EAGLE IF it supported more layers.  But that question misses

    too.  If you are routing 16+ layers then you most likely have many, many

    differential pairs and a bunch of length matching (like Morten's board

    above).  Until you have true, polished support for those design elements no

    one is going to choose EAGLE for those types of boards--the effort is

    simply too big when other tools do a lot to help.  So you have to address

    ALL of the design elements and then someone can consider EAGLE.  Until that

    happens you can't use stats from your current user base to see what support

    it would have because your current user base choose EAGLE in spite of it

    not supporting these requirements--so obviously they don't think it's

    important.

     

    James.

     

    --

    James Morrison  ~~~  Stratford Digital

     

    Order your EAGLE license from Stratford Digital at

    http://www.eaglelicenses.com

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.