Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Eagle 7.6.0 Linux x64 Control Panel "Name" window resize issue
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 190 subscribers
  • Views 1214 views
  • Users 0 members are here
Related

Eagle 7.6.0 Linux x64 Control Panel "Name" window resize issue

craigarno
craigarno over 10 years ago

I'm running OpenSUSE 12.3 x64 and having a problem with Eagle Control

panel in versions 7.5.0 and 7.6.0 (7.4.0 works fine).

 

When I try to resize the "Name" panel by hovering over the vertical bar

until it turns into a bidirectional arrow, then try dragging this, the

problem shows.  The Name Window collapses to an even smaller size and

cannot be moved. This effectively hides all the names, making the

control panel unusable under Linux.

 

I tried the Windows version of Eagle 7.5.0 and 7.6.0 and they don't

display this problem.

 

--

Thanks,

Craig

 

  • Sign in to reply
  • Cancel
Parents
  • kikoun
    kikoun over 10 years ago

    Hello,

     

    I'm running Opensuse 13.2 x64, (KDE, Nvidia graphic driver) and I don't have any trouble like yours (all eagle 7,x.0 versions).

    Maybe there is some issues with some library of the 12.3 Opensuse version that are no more compatible with last Eagle version ...

    May I ask why you're using the 12.3 and not a more recent one ? I know that is not always a good idea to update to the latest  version but the 13.2 is very stable now.(unlike like the last 'leap' Opensuse version ...)...

     

    guillaume.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • craigarno
    craigarno over 10 years ago in reply to kikoun

    On 05/23/2016 12:15 PM, Guillaume barrey wrote:

    May I ask why you're using the 12.3 and not a more recent one ?

     

    Very simply, OpenSUSE has become quite unstable ever since Microsoft

    became a major shareholder and started directing development.

     

    I run a large number of services under Linux to support what I do.

    Upgrading usually means being out of business for 1 week to 1 month

    while I devote 100% of my time to fixing everything broken.  Last time I

    upgraded from 11 to 12, Asterisk didn't work for a week.  This meant I

    didn't have phone service for a week... not acceptable.  I listened

    carefully to others upgrading to 13 and heard all manner of woe, mostly

    email and php things breaking.  I rely heavily on email, run OwnCloud

    for Firefox Sync, Contact sync, Calendar sync to desktops, laptops, and

    phones... I use Dovecot for IMAPS to Thunderbird, SquirrelMail, etc.  I

    won't bother listing all the rest of what I run as it relates to heavy

    embedded systems development, hardware and software with revision

    control and database support. In other words I'm a heavy experienced

    user.  Linux is much more to me than a "Windows desktop replacement for

    my applications". It has to be stable and work, out of the box so I can

    do my own work instead of fixing someone elses work (which I do pro bono

    work occasionally for open source projects).

     

    From your description of 13.x stability it might be time to take the

    upgrade risk. I will have a backup plan, such as switching to Ubuntu or

    going back to 12.x if 13.x is still too messed up, or so heavily

    "modified" that I might as well be learning a new distribution... Kind

    of like why I switched from MS Office to OpenOffice/LibreOffice around

    2003, well that and OpenDocument format [international standard ISO/IEC

    26300].

     

    BTW, I really like Eagle, as it does a lot of things right.  That's why

    I'm here.

     

    Craig

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kikoun
    kikoun over 10 years ago in reply to craigarno

    Hi Craig

     

    I understand your point. At work, I think twice (or more) before asking for a soft, OS or computer update to the TI department because of the waste of time it can produce.

     

    Even at home, I don't change easily, that why I'm still running 13.2  and not the leap 42.1. I just tried it on a laptop I barely use so I could not risk to be stuck with bugs from an un-really tested version. I was right to test it on this old laptop: this Leap 42.1 that should be the Opensuse 'Stable' version wasn't very stable at all (Kwin crashes every 5 minutes, random dual screen configuration at each login etc...).

    On that point, you’re right, Opensuse really disappoints me : they didn't focus on the stability, but only on the 'shiny-brand-new-but-buggy-feature-that-I-don't-even-care'. They should reserved that for the tumbleweed version.

     

    I'm really happy with the 13.2, (that's why I asked), but I must admit that I'm not an advanced user like you (I use thunderbird/firefox/eagle/freecad, and dlna services, and it not for my job (at work I'm running that I'm told to run :windows7 (I would prefer linux image )...

     

    BTW I love eagle too image, but I'm helpless for your problem.

     

    Guillaume.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • kikoun
    kikoun over 10 years ago in reply to craigarno

    Hi Craig

     

    I understand your point. At work, I think twice (or more) before asking for a soft, OS or computer update to the TI department because of the waste of time it can produce.

     

    Even at home, I don't change easily, that why I'm still running 13.2  and not the leap 42.1. I just tried it on a laptop I barely use so I could not risk to be stuck with bugs from an un-really tested version. I was right to test it on this old laptop: this Leap 42.1 that should be the Opensuse 'Stable' version wasn't very stable at all (Kwin crashes every 5 minutes, random dual screen configuration at each login etc...).

    On that point, you’re right, Opensuse really disappoints me : they didn't focus on the stability, but only on the 'shiny-brand-new-but-buggy-feature-that-I-don't-even-care'. They should reserved that for the tumbleweed version.

     

    I'm really happy with the 13.2, (that's why I asked), but I must admit that I'm not an advanced user like you (I use thunderbird/firefox/eagle/freecad, and dlna services, and it not for my job (at work I'm running that I'm told to run :windows7 (I would prefer linux image )...

     

    BTW I love eagle too image, but I'm helpless for your problem.

     

    Guillaume.