I'm running OpenSUSE 12.3 x64 and having a problem with Eagle Control
panel in versions 7.5.0 and 7.6.0 (7.4.0 works fine).
When I try to resize the "Name" panel by hovering over the vertical bar
until it turns into a bidirectional arrow, then try dragging this, the
problem shows. The Name Window collapses to an even smaller size and
cannot be moved. This effectively hides all the names, making the
control panel unusable under Linux.
I tried the Windows version of Eagle 7.5.0 and 7.6.0 and they don't
display this problem.
--
Thanks,
Craig