Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Change layer during routing?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 24 replies
  • Subscribers 190 subscribers
  • Views 6384 views
  • Users 0 members are here
Related

Change layer during routing?

lix
lix over 10 years ago

Hello,

 

After intensively searching the manual and fiddling around with the assign command I could not find an alternate way to the thee buttons mouse "change layer" when manually routing a board. Is anybody out there that can help me define a combination key or mouse/key to this end?

 

Thanks.

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 10 years ago

    On 26/05/16 08:53, Lix Paulian wrote:

     

    After intensively searching the manual and fiddling around with the

    assign command I could not find an alternate way to the thee buttons

    mouse "change layer" when manually routing a board. Is anybody out there

    that can help me define a combination key or mouse/key to this end?

     

     

    Three buttons? I'm sure it's only one (two if more than two layers).

    Perhaps that got broken by the "new and improved" (ha!) "more intuitive"

    (as if!) "windows-style" GUI. Set the magic config to get the original

    UI back.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • lix
    lix over 10 years ago in reply to autodeskguest

    No, seriously. I don't want to get into the GUI issue now, I'm fighting with it on a daily basis.

     

    Now, changing layers while routing a net is said to be possible by clicking the middle button on a three button mouse. It can't be that there is no other way. However, I couldn't find this piece of information in the manual.

     

    Not only that I don't use a three button mouse, I don't use a mouse at all (since three years now). I know that many people can't believe this, but a multitouch track pad is (in my opinion and with some training) far superior to any mouse, no matter how many buttons it has. So don't tell me "buy a decent mouse".

     

    I can't believe that CadSoft has implemented no alternative to the middle button to change layers.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 10 years ago in reply to lix

    Lix Paulian wrote on Thu, 26 May 2016 21:51

    I can't believe that CadSoft has implemented no alternative to the

    middle button to change layers.

     

     

    Except of course the "LAYER" command?

     

    If you only have a small number of layers you could assign keyboard

    shortcuts to issue different "LAYER LayerNum;" commands.

     

    Ideally I guess a couple of keys to scroll backwards and forwards through

    the available layers would be nice. ULP does allow you to access which

    layers are available but I can't see an easy way of determining the

    currently selected layer at the moment otherwise it would be trivial to

    implement this functionality in ULP and assign that to shortcuts.

     

    Best Regards,

     

    Rachael

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 5 years ago in reply to rhormigo

    On 12.02.2021 22:29, Rick Hormigo wrote:

    I am sure that you may already know this after an infinite Trump era later, but in addition to Layer, many optical mouses these days have that "middle" button in the wheel. Pressuring the wheel down, that  sometimes is a pain since interferes with zoom in/out if you rotate the wheel as you push down.

    This also has an issue that I believe Eagle has poorly addressed, at least I am not aware of a way to set this: If the board has more than four routing layers, it won't toggle directly. Instead, shows a dialog to select first what layer you want to toggle to, in case of internal layers are used for routing. In my opinion this should be optional or setable somehow, otherwise you waste time in that. Most designs for Eagle I do are 2 or 4 layers that have minimal or not internal routing, mostly planes. And If I wan do more complex stuff with 6 or more layers and lots of tiny parts, I prefer a more serious tool with more basic features as multiple highlight nets and at least a database behind for parts.

     

    I had this issue with my Logitech M-U00007 mouse. The scrollwheel has a

    button to add "click" fricktion to the wheel, wich helps a bit. But my

    biggest problem was that this mouse has additional

    sideways click functionality on the scroll wheel. I had to open my mouse

    physically (like any electronic engineer would do I guess) and disable

    those switches to be able to work with Eagle (7.7).

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rhormigo
    rhormigo over 5 years ago in reply to lix

    I am sure that you may already know this after an infinite Trump era later, but in addition to Layer, many optical mouses these days have that "middle" button in the wheel. Pressuring the wheel down, that  sometimes is a pain since interferes with zoom in/out if you rotate the wheel as you push down.

    This also has an issue that I believe Eagle has poorly addressed, at least I am not aware of a way to set this: If the board has more than four routing layers, it won't toggle directly. Instead, shows a dialog to select first what layer you want to toggle to, in case of internal layers are used for routing. In my opinion this should be optional or setable somehow, otherwise you waste time in that. Most designs for Eagle I do are 2 or 4 layers that have minimal or not internal routing, mostly planes. And If I want to do more complex stuff with 6 or more layers and lots of tiny parts, I prefer a more serious tool with more basic features as multiple highlight nets and at least a database behind for parts.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rhormigo
    rhormigo over 5 years ago in reply to lix

    I am sure that you may already know this after an infinite Trump era later, but in addition to Layer, many optical mouses these days have that "middle" button in the wheel. Pressuring the wheel down, that  sometimes is a pain since interferes with zoom in/out if you rotate the wheel as you push down.

    This also has an issue that I believe Eagle has poorly addressed, at least I am not aware of a way to set this: If the board has more than four routing layers, it won't toggle directly. Instead, shows a dialog to select first what layer you want to toggle to, in case of internal layers are used for routing. In my opinion this should be optional or setable somehow, otherwise you waste time in that. Most designs for Eagle I do are 2 or 4 layers that have minimal or not internal routing, mostly planes. And If I want to do more complex stuff with 6 or more layers and lots of tiny parts, I prefer a more serious tool with more basic features as multiple highlight nets and at least a database behind for parts.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • autodeskguest
    autodeskguest over 5 years ago in reply to rhormigo

    On 12.02.2021 22:29, Rick Hormigo wrote:

    I am sure that you may already know this after an infinite Trump era later, but in addition to Layer, many optical mouses these days have that "middle" button in the wheel. Pressuring the wheel down, that  sometimes is a pain since interferes with zoom in/out if you rotate the wheel as you push down.

    This also has an issue that I believe Eagle has poorly addressed, at least I am not aware of a way to set this: If the board has more than four routing layers, it won't toggle directly. Instead, shows a dialog to select first what layer you want to toggle to, in case of internal layers are used for routing. In my opinion this should be optional or setable somehow, otherwise you waste time in that. Most designs for Eagle I do are 2 or 4 layers that have minimal or not internal routing, mostly planes. And If I wan do more complex stuff with 6 or more layers and lots of tiny parts, I prefer a more serious tool with more basic features as multiple highlight nets and at least a database behind for parts.

     

    I had this issue with my Logitech M-U00007 mouse. The scrollwheel has a

    button to add "click" fricktion to the wheel, wich helps a bit. But my

    biggest problem was that this mouse has additional

    sideways click functionality on the scroll wheel. I had to open my mouse

    physically (like any electronic engineer would do I guess) and disable

    those switches to be able to work with Eagle (7.7).