Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Change layer during routing?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 24 replies
  • Subscribers 190 subscribers
  • Views 6384 views
  • Users 0 members are here
Related

Change layer during routing?

lix
lix over 10 years ago

Hello,

 

After intensively searching the manual and fiddling around with the assign command I could not find an alternate way to the thee buttons mouse "change layer" when manually routing a board. Is anybody out there that can help me define a combination key or mouse/key to this end?

 

Thanks.

  • Sign in to reply
  • Cancel
Parents
  • rachaelp
    rachaelp over 10 years ago

    Hi Lix,

     

    I do think you raise some valid points, but there are a lot of things EAGLE does differently that work better than in other packages too. Just because they are different and unexpected doesn't mean they should change them if they work better.

     

    I've just done some experimenting on applications I have installed and many have a right mouse button context menu that doesn't require you to select something first. Web browsers are a prime example of this. More in line with EAGLE type apps I looked at Autodesk's Fusion 360 and this too has right click context menus that don't require you to select something with a selection tool first. I'm not sure how a separate selection tool would speed up the process of selecting the correct object for a context menu, it would still have the same limitations of the number of objects within the tools selection catchment area and you'd have to scroll through all the matching objects just the same.

     

    Adding in a step of having to choose the selection tool first and then having to choose the tool you want to use after selecting things seems counter productive to me as you have more mouse clicks per thing you actually want to do. Maybe I have misunderstood what you intended here.

     

    With regards to objects being glued to the cursor on move, yes I can see your point on that, it would be nice to be able to group select object and then just click and drag around without having to go "right-click->move group" for every adjustment. This does make it harder to just tweak a position slightly as it moves to your current cursor position when you select the menu option. The up side to this is you can't accidentally drop a block you are moving in the middle of somewhere else which can be really annoying with other tools, especially if there is a lot of scrolling involved as part of the move. I'm sure there are ways CADSoft can tweak this use case without having to rewrite the whole UI paradigm though.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 10 years ago in reply to rachaelp

    Lix Paulian wrote:

     

    I am not sure I can follow this idea of Eagle is doing certain operations better by not using a standard interface.

     

    Damn you are good at mis-quoting people aren't you?

     

    rpeterson wrote:

     

    I do think you raise some valid points, but there are a lot of things EAGLE does differently that work better than in other packages too.

     

    I said better than other packages, and by implication this would be other comparable packages. I've used a lot of ECAD packages and they all have their own UI quirks.

     

    Yes ideally a GUI expert would come along and help streamline the UI (btw, I did actually study interaction design as part of a course I did a few years back, it should be intuitive but the most important goal is to reduce the number of operations you need to take to perform an action to a minimum, for technical apps like CAD you can assume a certain level of user competence / ability to learn) but it's not as cut and dried as forcing it to confirm to a set of UI conventions (which UI conventions btw? Windows style conventions? If so that wouldn't be consistent on my Mac or on my Linux machines...) which were likely specified with typical office applications in mind and which have very different use case requirements to ECAD. With ECAD (or any other type of CAD) you are always going to have to learn the some of the UI paradigms otherwise operations are going to take longer to do with a lot more clicks.

     

    To be blunt, you're not doing yourself any favours here. I'm happy to help people who have genuine technical issues but if you continue whinging and complaining about everything you hate about the EAGLE's UI then people will soon get bored of listening to you and be less than willing to go out of their way to answer your questions.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rachaelp
    rachaelp over 10 years ago in reply to rachaelp

    Lix Paulian wrote:

     

    I am not sure I can follow this idea of Eagle is doing certain operations better by not using a standard interface.

     

    Damn you are good at mis-quoting people aren't you?

     

    rpeterson wrote:

     

    I do think you raise some valid points, but there are a lot of things EAGLE does differently that work better than in other packages too.

     

    I said better than other packages, and by implication this would be other comparable packages. I've used a lot of ECAD packages and they all have their own UI quirks.

     

    Yes ideally a GUI expert would come along and help streamline the UI (btw, I did actually study interaction design as part of a course I did a few years back, it should be intuitive but the most important goal is to reduce the number of operations you need to take to perform an action to a minimum, for technical apps like CAD you can assume a certain level of user competence / ability to learn) but it's not as cut and dried as forcing it to confirm to a set of UI conventions (which UI conventions btw? Windows style conventions? If so that wouldn't be consistent on my Mac or on my Linux machines...) which were likely specified with typical office applications in mind and which have very different use case requirements to ECAD. With ECAD (or any other type of CAD) you are always going to have to learn the some of the UI paradigms otherwise operations are going to take longer to do with a lot more clicks.

     

    To be blunt, you're not doing yourself any favours here. I'm happy to help people who have genuine technical issues but if you continue whinging and complaining about everything you hate about the EAGLE's UI then people will soon get bored of listening to you and be less than willing to go out of their way to answer your questions.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • lix
    lix over 10 years ago in reply to autodeskguest

    Last time I checked in Ubuntu, the terminal still needed a three button mouse to copy/paste text. But this is a very minor issue. Generally Ubuntu is a very decent OS; if I would have to choose between Windows an Ubuntu, I would go with the latter.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to lix

    On 27/05/16 19:53, Lix Paulian wrote:

    Linux may still have some strange quirks going back to X-Windows, but Macs and Windows are quite the same).

     

    What utter rot!

     

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • lix
    lix over 10 years ago in reply to rachaelp

    As I already wrote elsewhere, my hope is that the CadSoft guys would listen and do finally something. You don't have to take this personally. I much appreciate your help.

     

    And speaking about GUI conventions, meanwhile all major platforms came to a common denominator. Linux may still have some strange quirks going back to X-Windows, but Macs and Windows are quite the same).

     

    Best regards,

     

    Lix