Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) BC184L transistor component
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 20 replies
  • Subscribers 189 subscribers
  • Views 5140 views
  • Users 0 members are here
Related

BC184L transistor component

Andy Betts
Andy Betts over 10 years ago

I'm taking my first baby steps into circuit design, with the intention of making guitar effect pedals that are as close to the original vintage spec as possible... Here's my issue.

 

I'm laying out the schematic for the circuit, and went to the library to pull out a BC184L transistor and there wasn't one. The closest to it I could find was a BC109, however I would really like the 184L as that's the correct one for the circuit. can I just create a new one in the library from an existing component that's virtually the same, or is there a resource for obtaining the correct library file, or am I missing something blatantly obvious as a newbie.

 

 

Thanks for your patience in advance...

 

Andy

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 10 years ago

    Am 24.07.2016 um 12:04 schrieb Andy Betts:

    I'm taking my first baby steps into circuit design, with the intention of making guitar effect pedals that are as close to the original vintage spec as possible... Here's my issue.

     

    I'm laying out the schematic for the circuit, and went to the library to pull out a BC184L transistor and there wasn't one. The closest to it I could find was a BC109, however I would really like the 184L as that's the correct one for the circuit. can I just create a new one in the library from an existing component that's virtually the same, or is there a resource for obtaining the correct library file, or am I missing something blatantly obvious as a newbie.

     

     

    Thanks for your patience in advance...

     

    Andy

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/202196

     

     

    The manufacturing companies use  a lot  of different characters behind

    the actual number, sometimes half the alphabet image

    So you should check the internet for BC184 and BC184L data sheets and

    compare them.

     

    For your layout it is important that the case /pins are the same

    position as for the Transistor you want to use, for your schematics the

    name is not important. If the BC109 suits you, you can NAME it BC184L

    because in the schematics it a symbol only while the layout will become

    the real thing.

     

    If you insist to have a BC184L in a library then you should/must make

    your own libraries, because if you add your new device to a system

    library, be aware that your work will be lost on  the next update.

     

    You should also know that no layout program has all the devices ready

    which are available on the market, so it is a good practise to create

    your own devices (in your own libraries). Only then you can be certain

    that the footprint is correct.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to autodeskguest

    On 24/07/16 12:24, Joern Paschedag wrote:

     

    For your layout it is important that the case /pins are the same

    position as for the Transistor you want to use, for your schematics the

    name is not important. If the BC109 suits you, you can NAME it BC184L

    because in the schematics it a symbol only while the layout will become

    the real thing.

     

    If you're doing that, you should use a BC337 rather than a BC109,

    because the 337 is the same package as the 184 - although check pin-outs

    because the BC184L may differ from the BC184 without a suffix. Or you

    could use one of the generic "TO-92-EBC" type devices but beware because

    at least one of them is wrong.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to autodeskguest

    Am 24.07.2016 um 14:12 schrieb Rob Pearce:

    On 24/07/16 12:24, Joern Paschedag wrote:

     

    For your layout it is important that the case /pins are the same

    position as for the Transistor you want to use, for your schematics the

    name is not important. If the BC109 suits you, you can NAME it BC184L

    because in the schematics it a symbol only while the layout will become

    the real thing.

     

    If you're doing that, you should use a BC337 rather than a BC109,

    because the 337 is the same package as the 184 - although check pin-outs

    because the BC184L may differ from the BC184 without a suffix. Or you

    could use one of the generic "TO-92-EBC" type devices but beware because

    at least one of them is wrong.

     

     

    Hi Rob,

    since you mention the TO-92-ECB.

    This was imo the worst bullshit produced.

    In the eagle libraries always the pads are numbered  while the pins have

    the name.

    In the connect dialog of the devices the pin names are  connected to the

    corresponding pad numbers.

    So there is no need for ECB etc. at all.

    AFAIR someone else brought up this problem and the hope that cadsoft

    will clean up this.

    But that is a lot of work to check all the devices with a TO-92 body.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 10 years ago in reply to autodeskguest

    Am 24.07.2016 um 14:12 schrieb Rob Pearce:

    On 24/07/16 12:24, Joern Paschedag wrote:

     

    For your layout it is important that the case /pins are the same

    position as for the Transistor you want to use, for your schematics the

    name is not important. If the BC109 suits you, you can NAME it BC184L

    because in the schematics it a symbol only while the layout will become

    the real thing.

     

    If you're doing that, you should use a BC337 rather than a BC109,

    because the 337 is the same package as the 184 - although check pin-outs

    because the BC184L may differ from the BC184 without a suffix. Or you

    could use one of the generic "TO-92-EBC" type devices but beware because

    at least one of them is wrong.

     

     

    Hi Rob,

    since you mention the TO-92-ECB.

    This was imo the worst bullshit produced.

    In the eagle libraries always the pads are numbered  while the pins have

    the name.

    In the connect dialog of the devices the pin names are  connected to the

    corresponding pad numbers.

    So there is no need for ECB etc. at all.

    AFAIR someone else brought up this problem and the hope that cadsoft

    will clean up this.

    But that is a lot of work to check all the devices with a TO-92 body.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag