Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Manually routing from top   to bottom.
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 190 subscribers
  • Views 4278 views
  • Users 0 members are here
Related

Manually routing from top   to bottom.

autodeskguest
autodeskguest over 10 years ago

Hi,

 

Occasionally I find myself with a red wire on the top, a blue wire on the

bottom and a yellow 'unrouted' line between the two.

 

How do I manually route between the two?

 

If I select the normal 'route' tool, click on one end, and then click on

the other end I get a trace appearing between the two ends (as expected)

but instead of getting a via appearing I get a yellow 'X'(which i think

means I'm missing a 'via') I can manually place a via on the yellow 'X' but

it doesn't seem to actually connect - I can still pick up each end of my

track and move it interdependently, and I still have the yellow 'unrouted'

line between the two.

 

What am I doing wrong?

 

Thanks

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 10 years ago

    On 14/08/2016 12:50 a.m., Lima wrote:

     

    .....If I select the normal 'route' tool, click on one end, and then click on

    the other end I get a trace appearing between the two ends (as expected)

    but instead of getting a via appearing I get a yellow 'X'(which i think

    means I'm missing a 'via') I can manually place a via on the yellow 'X' but

    it doesn't seem to actually connect.....

     

    Rob has given you an answer. Using the middle mouse click to change layers.

     

    In the future you may well find yourself in the same situation.

    The 'X' is a zero length airwire, or to think of it another way it's a

    vertical airwire. The wires that connect to that airwire are on the same

    X Y  coordinate. If you then place an via at that coordinate, they

    should connect. i.e. the via will be given a signal name that matches

    that of the airwire and route wires.

     

    Use the ratsnest function to have eagle re-calulate airwires and get rid

    of the 'X' once the via is placed.

     

    FROM THE MANUAL *****************

    Airwires with length of 0 (for example, from Top to Bottom layer) are

    drawn as a cross in layer 19, Unrouted.

    Ending a wire at the same position where another wire of the same signal

    but in another layer already exists and pressing the Shift key at the

    same time causes EAGLE to place a via. Otherwise it won't.

     

    HTH

    Warren

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • supuflounder
    supuflounder over 8 years ago in reply to autodeskguest

    I have a Mac AirBook.  I see no mouse here.  I see no middle button on the non-mouse.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 8 years ago in reply to supuflounder

    Hi Joseph,

     

    Manually changing layers is possible too, from the toolbar. But it sounds extremely inconvenient to want to use a CAD package without a mouse. Anything else is a compromise.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 8 years ago in reply to shabaz

    shabaz  wrote:

     

    But it sounds extremely inconvenient to want to use a CAD package without a mouse. Anything else is a compromise.

     

    I'd have agreed with this before I started using a Mac. The trackpad on the Macbook Pro was so good with EAGLE that I replaced my mouse with a Magic Trackpad on my iMac.

     

    In EAGLE now you can change layers in the route command using the space bar to go through the available routing layers in the top to bottom direction or shift+space to go through the layers in the bottom to top direction. Remember that it'll now expect you to choose where to place the via before it'll let you continue routing on the chosen layer, it's not like it was pre-v8 and can take a bit of getting used to if you've used v7 or earlier a lot. As you cycle through the layers with the space bar the chosen next layer is shown in the status bar at the bottom, it's not very obvious and previously you'd have seen the obvious change in the Layer dropdown so you'd be excused for thinking nothing was happening if you were expecting the same visual feedback you were used to as it only changes there after the via is placed.

     

    Best Regards,


    Rachael

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rachaelp
    rachaelp over 8 years ago in reply to shabaz

    shabaz  wrote:

     

    But it sounds extremely inconvenient to want to use a CAD package without a mouse. Anything else is a compromise.

     

    I'd have agreed with this before I started using a Mac. The trackpad on the Macbook Pro was so good with EAGLE that I replaced my mouse with a Magic Trackpad on my iMac.

     

    In EAGLE now you can change layers in the route command using the space bar to go through the available routing layers in the top to bottom direction or shift+space to go through the layers in the bottom to top direction. Remember that it'll now expect you to choose where to place the via before it'll let you continue routing on the chosen layer, it's not like it was pre-v8 and can take a bit of getting used to if you've used v7 or earlier a lot. As you cycle through the layers with the space bar the chosen next layer is shown in the status bar at the bottom, it's not very obvious and previously you'd have seen the obvious change in the Layer dropdown so you'd be excused for thinking nothing was happening if you were expecting the same visual feedback you were used to as it only changes there after the via is placed.

     

    Best Regards,


    Rachael