EAGLE User Support (English) Ultraedit as external text editor
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
  • Replies 19 replies
  • Subscribers 180 subscribers
  • Views 1741 views
  • Users 0 members are here
Related

Ultraedit as external text editor

autodeskguest
autodeskguest over 9 years ago

Hi, is anyone else successfully using "UltraEdit" as an eagle external

text editor?

 

Glenn

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 9 years ago

    On 14.08.2016 18:57, Glenn Jones wrote:

    Hi, is anyone else successfully using "UltraEdit" as an eagle external

    text editor?

     

    I do use ultraedit as my main text editor, but I rarely need it for

    eagle work. What need do you have for text editor in Eagle?

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 9 years ago in reply to autodeskguest

    CadSoft Guest wrote:

     

    On 14.08.2016 18:57, Glenn Jones wrote:

    Hi, is anyone else successfully using "UltraEdit" as an eagle external

    text editor?

     

    I do use ultraedit as my main text editor, but I rarely need it for

    eagle work. What need do you have for text editor in Eagle?

     

     

    I imagine the OP would be using it for writing ULP. Ideally it would have ULP language syntax set up and it would integrate with the tool such that when a ULP generated an error it would open UltraEdit at the right file with the cursor on the right line/column. I don't have UltraEdit so can't add anything on it's suitability for EAGLE ULP but if there is a syntax file available or it's easy to create your own language syntax, and if you can launch it via a command line and pass it parameters for the file, line number and optionally column then it should work.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to rachaelp

    On 15.08.2016 10:27, rachaelp wrote:

    CadSoft Guest wrote:

     

    On 14.08.2016 18:57, Glenn Jones wrote:

    Hi, is anyone else successfully using "UltraEdit" as an eagle external

    text editor?

     

    I do use ultraedit as my main text editor, but I rarely need it for

    eagle work. What need do you have for text editor in Eagle?

     

     

    I imagine the OP would be using it for writing ULP. Ideally it would have ULP language syntax set up and it would integrate with the tool such that when a ULP generated an error it would open UltraEdit at the right file with the cursor on the right line/column. I don't have UltraEdit so can't add anything on it's suitability for EAGLE ULP but if there is a syntax file available or it's easy to create your own language syntax, and if you can launch it via a command line and pass it parameters for the file, line number and optionally column then it should work.

     

    Ah, of course. I do write ULP's in ultraedit but never bothered enter it

    as external editor, simply because I didn't find the magic parameter to

    pass line and col number. Now I found it and tested it.

     

    The command line field works with:

    uedit64 %F -l%L -c%C

     

    If you use the 32 bit version, you should use uedit32 of course.

     

    Thanks for bumping this functionality image

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    On 15.08.2016 11:05, Morten Leikvoll wrote:

    On 15.08.2016 10:27, rachaelp wrote:

    CadSoft Guest wrote:

     

    On 14.08.2016 18:57, Glenn Jones wrote:

    Hi, is anyone else successfully using "UltraEdit" as an eagle external

    text editor?

     

    I do use ultraedit as my main text editor, but I rarely need it for

    eagle work. What need do you have for text editor in Eagle?

     

     

    I imagine the OP would be using it for writing ULP. Ideally it would

    have ULP language syntax set up and it would integrate with the tool

    such that when a ULP generated an error it would open UltraEdit at the

    right file with the cursor on the right line/column. I don't have

    UltraEdit so can't add anything on it's suitability for EAGLE ULP but

    if there is a syntax file available or it's easy to create your own

    language syntax, and if you can launch it via a command line and pass

    it parameters for the file, line number and optionally column then it

    should work.

     

    Ah, of course. I do write ULP's in ultraedit but never bothered enter it

    as external editor, simply because I didn't find the magic parameter to

    pass line and col number. Now I found it and tested it.

     

    The command line field works with:

    uedit64 %F -l%L -c%C

     

    If you use the 32 bit version, you should use uedit32 of course.

     

    Thanks for bumping this functionality image

     

     

    I forgot to mention that you can also tell ultraedit ro use "c" style

    highlighting for .ulp files in the configuration window.

    Add *.ulp to "'C'Files under" under "File types".

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 9 years ago in reply to autodeskguest

    Hi Morten,

     

    Do you have the ULP language syntax set up properly for UltraEdit so you

    get all keyword highlighting etc?

     

    I've still not found an editor I am 100% happy with for ULP, currently

    using Atom but I haven't spent the time to get the language syntax set up

    so it colours everything nicely.

     

    Best Regards,

     

    Rachael

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 9 years ago in reply to autodeskguest

    Morten Leikvoll wrote on Mon, 15 August 2016 10:08

    I forgot to mention that you can also tell ultraedit ro use "c" style

    highlighting for .ulp files in the configuration window.

    Add *.ulp to "'C'Files under" under "File types".

     

     

    Ok you just answered my question before I asked it image Thanks!

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to rachaelp

    On 8/15/2016 5:15 AM, Rachael wrote:

    Hi Morten,

     

    Do you have the ULP language syntax set up properly for UltraEdit so you

    get all keyword highlighting etc?

     

    I've still not found an editor I am 100% happy with for ULP, currently

    using Atom but I haven't spent the time to get the language syntax set up

    so it colours everything nicely.

     

    Best Regards,

     

    Rachael

     

     

    Hi All,

     

    We have language files for Notepad++ and Geany so that you get syntax

    highlighting on the ULP keywords.

     

    It use to be up on our site under tools and converters. If anyone would

    like them let me know, I still have them.

     

    Best Regards,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 9 years ago in reply to autodeskguest

    Hi Jorge,

    CadSoft Guest wrote:

     

    We have language files for Notepad++ and Geany so that you get syntax

    highlighting on the ULP keywords.

     

    Following on from the posts earlier, I went and fixed my Atom editor (https://atom.io/ ) to use C syntax highlighting as per what Morten does with UltraEdit and that works ok but it doesn't highlight built in EAGLE objects or anything like that. I will probably try and sort it so it has a dedicated EAGLE ULP language add in at some point but as it stands it works pretty well with EAGLE as it is.

     

    The problem with Notepad++ is it's windows only and whilst Geany does work across platform, it's a little rough around the edges and clunky in some ways and I don't really like it so it would be nice if there was a really good cross platform option that integrates really nicely with EAGLE on all platforms.

     

    CadSoft Guest wrote:

     

    It use to be up on our site under tools and converters. If anyone would

    like them let me know, I still have them.

    Please can you email them to me as I may use them as a starting point for creating a dedicated ULP integration for Atom :-)

     

    Many thanks,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    Hi,

     

    On Mon, 15 Aug 2016 12:23:35 -0400, Jorge Garcia wrote:

     

    We have language files for Notepad++ and Geany so that you get syntax

    highlighting on the ULP keywords.

     

    It use to be up on our site under tools and converters. If anyone would

    like them let me know, I still have them.

     

    It would be great if you could put them in the new website, perhaps in

    the ULP area if the Misc category is not reinstated. 

     

    An early release of a ULP language file for Notepad++ still exists on the

    FTP server, ftp://ftp.cadsoft.de/eagle/userfiles/misc/

     

    ftp://ftp.cadsoft.de/eagle/userfiles/misc/notepad+

    +_userdefinedlanguage_ulp.zip

     

    Jorge is likely to have the most recent version that was updated for

    Eagle 5/6 ULP changes.

     

    Kind regards

    Neil

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    On 16/08/2016 9:12 a.m., Neil Allison wrote:

    Hi,

     

    On Mon, 15 Aug 2016 12:23:35 -0400, Jorge Garcia wrote:

     

    We have language files for Notepad++ and Geany so that you get syntax

    highlighting on the ULP keywords.

     

    It use to be up on our site under tools and converters. If anyone would

    like them let me know, I still have them.

     

    It would be great if you could put them in the new website, perhaps in

    the ULP area if the Misc category is not reinstated.

     

    An early release of a ULP language file for Notepad++ still exists on the

    FTP server, ftp://ftp.cadsoft.de/eagle/userfiles/misc/

     

    ftp://ftp.cadsoft.de/eagle/userfiles/misc/notepad+

    +_userdefinedlanguage_ulp.zip

     

    Jorge is likely to have the most recent version that was updated for

    Eagle 5/6 ULP changes.

     

    Kind regards

    Neil

     

     

     

    Attached is the syntax file I created over two years ago for TextPad. At

    that time the Notepad++ one was missing a few keywords and this one I

    created included them so it may be of use as a reference list.

     

    Personally I preferred Notepad++ for reasons I now forget so didn't

    spend much time with TextPad after creating the syntax file.

     

    The file shows the keywords in different groups /classes

    The display colour of these groups are determined by TextPad

    configuration settings for the language.Image attached.

     

    HTH

    Warren

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>