EAGLE User Support (English) Ultraedit as external text editor
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
  • Replies 19 replies
  • Subscribers 180 subscribers
  • Views 1740 views
  • Users 0 members are here
Related

Ultraedit as external text editor

autodeskguest
autodeskguest over 9 years ago

Hi, is anyone else successfully using "UltraEdit" as an eagle external

text editor?

 

Glenn

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    On 16/08/2016 9:12 a.m., Neil Allison wrote:

    Hi,

     

    On Mon, 15 Aug 2016 12:23:35 -0400, Jorge Garcia wrote:

     

    We have language files for Notepad++ and Geany so that you get syntax

    highlighting on the ULP keywords.

     

    It use to be up on our site under tools and converters. If anyone would

    like them let me know, I still have them.

     

    It would be great if you could put them in the new website, perhaps in

    the ULP area if the Misc category is not reinstated.

     

    An early release of a ULP language file for Notepad++ still exists on the

    FTP server, ftp://ftp.cadsoft.de/eagle/userfiles/misc/

     

    ftp://ftp.cadsoft.de/eagle/userfiles/misc/notepad+

    +_userdefinedlanguage_ulp.zip

     

    Jorge is likely to have the most recent version that was updated for

    Eagle 5/6 ULP changes.

     

    Kind regards

    Neil

     

     

     

    Attached is the syntax file I created over two years ago for TextPad. At

    that time the Notepad++ one was missing a few keywords and this one I

    created included them so it may be of use as a reference list.

     

    Personally I preferred Notepad++ for reasons I now forget so didn't

    spend much time with TextPad after creating the syntax file.

     

    The file shows the keywords in different groups /classes

    The display colour of these groups are determined by TextPad

    configuration settings for the language.Image attached.

     

    HTH

    Warren

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    On 8/15/2016 5:05 AM, Morten Leikvoll wrote:

    On 15.08.2016 10:27, rachaelp wrote:

    CadSoft Guest wrote:

     

    On 14.08.2016 18:57, Glenn Jones wrote:

    Hi, is anyone else successfully using "UltraEdit" as an eagle external

    text editor?

     

    I do use ultraedit as my main text editor, but I rarely need it for

    eagle work. What need do you have for text editor in Eagle?

     

     

    I imagine the OP would be using it for writing ULP. Ideally it would

    have ULP language syntax set up and it would integrate with the tool

    such that when a ULP generated an error it would open UltraEdit at the

    right file with the cursor on the right line/column. I don't have

    UltraEdit so can't add anything on it's suitability for EAGLE ULP but

    if there is a syntax file available or it's easy to create your own

    language syntax, and if you can launch it via a command line and pass

    it parameters for the file, line number and optionally column then it

    should work.

     

    Ah, of course. I do write ULP's in ultraedit but never bothered enter it

    as external editor, simply because I didn't find the magic parameter to

    pass line and col number. Now I found it and tested it.

     

    The command line field works with:

    uedit64 %F -l%L -c%C

     

    If you use the 32 bit version, you should use uedit32 of course.

     

    Thanks for bumping this functionality image

     

    Morten, thanks for that info. I think Windows UAC is getting in my way

    as I get a failed to run error when launched from Eagle.

     

    Glenn

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    On 8/15/2016 5:05 AM, Morten Leikvoll wrote:

    On 15.08.2016 10:27, rachaelp wrote:

    CadSoft Guest wrote:

     

    On 14.08.2016 18:57, Glenn Jones wrote:

    Hi, is anyone else successfully using "UltraEdit" as an eagle external

    text editor?

     

    I do use ultraedit as my main text editor, but I rarely need it for

    eagle work. What need do you have for text editor in Eagle?

     

     

    I imagine the OP would be using it for writing ULP. Ideally it would

    have ULP language syntax set up and it would integrate with the tool

    such that when a ULP generated an error it would open UltraEdit at the

    right file with the cursor on the right line/column. I don't have

    UltraEdit so can't add anything on it's suitability for EAGLE ULP but

    if there is a syntax file available or it's easy to create your own

    language syntax, and if you can launch it via a command line and pass

    it parameters for the file, line number and optionally column then it

    should work.

     

    Ah, of course. I do write ULP's in ultraedit but never bothered enter it

    as external editor, simply because I didn't find the magic parameter to

    pass line and col number. Now I found it and tested it.

     

    The command line field works with:

    uedit64 %F -l%L -c%C

     

    If you use the 32 bit version, you should use uedit32 of course.

     

    Thanks for bumping this functionality image

     

    Morten, thanks for that info. I think Windows UAC is getting in my way

    as I get a failed to run error when launched from Eagle.

     

    Glenn

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    On 16.08.2016 14:16, Glenn Jones wrote:

    On 8/15/2016 5:05 AM, Morten Leikvoll wrote:

    On 15.08.2016 10:27, rachaelp wrote:

    CadSoft Guest wrote:

     

    On 14.08.2016 18:57, Glenn Jones wrote:

    Hi, is anyone else successfully using "UltraEdit" as an eagle external

    text editor?

     

    I do use ultraedit as my main text editor, but I rarely need it for

    eagle work. What need do you have for text editor in Eagle?

     

     

    I imagine the OP would be using it for writing ULP. Ideally it would

    have ULP language syntax set up and it would integrate with the tool

    such that when a ULP generated an error it would open UltraEdit at the

    right file with the cursor on the right line/column. I don't have

    UltraEdit so can't add anything on it's suitability for EAGLE ULP but

    if there is a syntax file available or it's easy to create your own

    language syntax, and if you can launch it via a command line and pass

    it parameters for the file, line number and optionally column then it

    should work.

     

    Ah, of course. I do write ULP's in ultraedit but never bothered enter it

    as external editor, simply because I didn't find the magic parameter to

    pass line and col number. Now I found it and tested it.

     

    The command line field works with:

    uedit64 %F -l%L -c%C

     

    If you use the 32 bit version, you should use uedit32 of course.

     

    Thanks for bumping this functionality image

     

    Morten, thanks for that info. I think Windows UAC is getting in my way

    as I get a failed to run error when launched from Eagle.

     

    My guess is that ue needs to be in the PATH environmentvariable and

    yours probably isnt. Try writing the full path. As long as you can start

    ultraedit, I guess you should be able to launch it from Eagle.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    On 8/16/2016 8:36 AM, Morten Leikvoll wrote:

    On 16.08.2016 14:16, Glenn Jones wrote:

    On 8/15/2016 5:05 AM, Morten Leikvoll wrote:

    On 15.08.2016 10:27, rachaelp wrote:

    CadSoft Guest wrote:

     

    On 14.08.2016 18:57, Glenn Jones wrote:

    Hi, is anyone else successfully using "UltraEdit" as an eagle

    external

    text editor?

     

    I do use ultraedit as my main text editor, but I rarely need it for

    eagle work. What need do you have for text editor in Eagle?

     

     

    I imagine the OP would be using it for writing ULP. Ideally it would

    have ULP language syntax set up and it would integrate with the tool

    such that when a ULP generated an error it would open UltraEdit at the

    right file with the cursor on the right line/column. I don't have

    UltraEdit so can't add anything on it's suitability for EAGLE ULP but

    if there is a syntax file available or it's easy to create your own

    language syntax, and if you can launch it via a command line and pass

    it parameters for the file, line number and optionally column then it

    should work.

     

    Ah, of course. I do write ULP's in ultraedit but never bothered enter it

    as external editor, simply because I didn't find the magic parameter to

    pass line and col number. Now I found it and tested it.

     

    The command line field works with:

    uedit64 %F -l%L -c%C

     

    If you use the 32 bit version, you should use uedit32 of course.

     

    Thanks for bumping this functionality image

     

    Morten, thanks for that info. I think Windows UAC is getting in my way

    as I get a failed to run error when launched from Eagle.

     

    My guess is that ue needs to be in the PATH environmentvariable and

    yours probably isnt. Try writing the full path. As long as you can start

    ultraedit, I guess you should be able to launch it from Eagle.

     

     

    I tried the full path - no go. When you run Ultraedit normally are you

    prompted by UAC?

     

    Glenn

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    >> > Morten, thanks for that info. I think Windows UAC is getting in my way

    as I get a failed to run error when launched from Eagle.

     

    My guess is that ue needs to be in the PATH environmentvariable and

    yours probably isnt. Try writing the full path. As long as you can start

    ultraedit, I guess you should be able to launch it from Eagle.

     

     

    I tried the full path - no go. When you run Ultraedit normally are you

    prompted by UAC?

     

    I have full access to my computer, so I cant compare with your scenario.

     

    My installation of ue is in "C:\Program Files\IDM Computer

    Solutions\UltraEdit\uedit64.exe" If I enter my full path with quotes on

    the executable, it works too:

    "C:\Program Files\IDM Computer Solutions\UltraEdit\uedit64" %F -l%L -c%C

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    >> > Morten, thanks for that info. I think Windows UAC is getting in my way

    as I get a failed to run error when launched from Eagle.

     

    My guess is that ue needs to be in the PATH environmentvariable and

    yours probably isnt. Try writing the full path. As long as you can start

    ultraedit, I guess you should be able to launch it from Eagle.

     

     

    I tried the full path - no go. When you run Ultraedit normally are you

    prompted by UAC?

     

    I have full access to my computer, so I cant compare with your scenario.

     

    My installation of ue is in "C:\Program Files\IDM Computer

    Solutions\UltraEdit\uedit64.exe" If I enter my full path with quotes on

    the executable, it works too:

    "C:\Program Files\IDM Computer Solutions\UltraEdit\uedit64" %F -l%L -c%C

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    On 08/15/2016 05:12 PM, Neil Allison wrote:

    Hi,

     

    On Mon, 15 Aug 2016 12:23:35 -0400, Jorge Garcia wrote:

     

    We have language files for Notepad++ and Geany so that you get syntax

    highlighting on the ULP keywords.

     

    It use to be up on our site under tools and converters. If anyone would

    like them let me know, I still have them.

     

    It would be great if you could put them in the new website, perhaps in

    the ULP area if the Misc category is not reinstated.

     

    An early release of a ULP language file for Notepad++ still exists on the

    FTP server, ftp://ftp.cadsoft.de/eagle/userfiles/misc/

     

    ftp://ftp.cadsoft.de/eagle/userfiles/misc/notepad+

    +_userdefinedlanguage_ulp.zip

     

    Jorge is likely to have the most recent version that was updated for

    Eagle 5/6 ULP changes.

     

    Kind regards

    Neil

     

     

     

     

    A little late to this thread (vacation), but I've been using UltraEdit for years with Eagle and I have wordfiles for ULP

    and SCR files. I can't give any advice on launching in a windows environment as I'm lucky enough to not have to use

    windows at work or home anymore.

     

    The SCR wordfile allows code-folding for regions starting with '#+' and ending with '#-'; I've had some really long

    eagle.scr files. Code folding, function, and variable recognition for ULP files work like it would with coding in C.

     

    If you use these you will probably need to change your syntax coloring to match your style. These are current up to

    Eagle 6. Eagle 7 only requires a few additions.

     

    Eric

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    On 08/15/2016 05:12 PM, Neil Allison wrote:

    Hi,

     

    On Mon, 15 Aug 2016 12:23:35 -0400, Jorge Garcia wrote:

     

    We have language files for Notepad++ and Geany so that you get syntax

    highlighting on the ULP keywords.

     

    It use to be up on our site under tools and converters. If anyone would

    like them let me know, I still have them.

     

    It would be great if you could put them in the new website, perhaps in

    the ULP area if the Misc category is not reinstated.

     

    An early release of a ULP language file for Notepad++ still exists on the

    FTP server, ftp://ftp.cadsoft.de/eagle/userfiles/misc/

     

    ftp://ftp.cadsoft.de/eagle/userfiles/misc/notepad+

    +_userdefinedlanguage_ulp.zip

     

    Jorge is likely to have the most recent version that was updated for

    Eagle 5/6 ULP changes.

     

    Kind regards

    Neil

     

     

     

     

    A little late to this thread (vacation), but I've been using UltraEdit for years with Eagle and I have wordfiles for ULP

    and SCR files. I can't give any advice on launching in a windows environment as I'm lucky enough to not have to use

    windows at work or home anymore.

     

    The SCR wordfile allows code-folding for regions starting with '#+' and ending with '#-'; I've had some really long

    eagle.scr files. Code folding, function, and variable recognition for ULP files work like it would with coding in C.

     

    If you use these you will probably need to change your syntax coloring to match your style. These are current up to

    Eagle 6. Eagle 7 only requires a few additions.

     

    Eric

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<