Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) How to design a board with ICs with their own ground and power plane
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 190 subscribers
  • Views 955 views
  • Users 0 members are here
Related

How to design a board with ICs with their own ground and power plane

nikoly
nikoly over 10 years ago

Hi to everyone,

I'm designing a 2 board layer using Eagle Cad.

This board is composed by different ICs (mainly LDO and step-up) that I have to put one next to the other in order to get the right voltage I need.

Every IC is equipped with its own demoboard and each demoboard (as you can see from attached file) has its own ground and power plane.

My doubt is how could I consider the whole board; I mean , do I have to draw each ground and power plane of each IC or can I draw one whole ground and power plane for the entire board ?

 

I have this doubt since my fear is to lose all benefits(noise rejection, thermal issues etc) in each IC I use in the board.

 

 

Hope you can give me an advice since this is the first board of this type I design

 

 

Thanks

nico

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    michaelkellett over 10 years ago

    Designing boards is not trivial and your chances of getting this right first time are not good so my first advice is that you shouldn't plan to get it right the first time - expect iterations.

     

    I'm assuming this board will have no more than 4 layers.

     

    If it's for home use and won't need to comply with any EMC regulations then just use a common ground plane  - if one power rail is dominant (connected to the largest number of nodes) then it may be good to use a power plane - sometimes I try to group parts according to the power they need so that I can reasonably have more than one power plane on the same layer. For good EMC performance the power plane should be decoupled to the ground plane in many places with small ceramic caps.

    If power planes don't look feasible then make the two inner layers both ground planes but run the power as tracks in one inner layer (filling in all the spaces with ground with lots and lots of little vias to link to the other ground plane).

    At the power switching chips then copy the demo board layout as closely as you can - identify the high current loops in the circuit and make sure that the high currents do not flow thought the main ground plane but are all on the component layer of the board.  Anchor the ground area on the top layer to the ground plane with many vias close together but aiming for as close to a single point connection as you can. Keep the area of the high current loops as small as you can.

    You should NOT use a power plane for the power input to the switching chips - use track (until you get tot the chip and its power input capacitor) - the inductance of the track will maintain some separation of input noise between the chips which will help them work better and their input high current loop should be through he local capacitor between Vin on the top layer and Ground on the top layer.

    Fill any blank areas of board near the power chips on all layers with ground - the more copper in the board the better it gets the heat away. Don't let the PCB cad system out thermal reliefs in the ground vias.

     

    If you need to comply with any EMC regs - do all the above, build a prototype, measure it with a spectrum analyzer and a a simple setup like  a TEM cell  - it will usually fail the tests (unless you are very good at this work) - use a near field probe and other tricks to work out where the unwanted emissions come from and fix the problem. There are no shortcuts round this and no way round needing to actually measure emissions.

     

    People will suggest that you could buy a ready made board very cheaply on eBay - I did so recently because a customers design has big issues with an LTC3780 based design and I wanted to compare. The customer design is so noisy that the GB Ethernet on the same board doesn't work properly - the eBay board is even worse (volts of HF noise on the output !!)  - and it doesn't regulate properly either !!

     

    I've designed a little board to see if I can get the LTC3780 to work right - I'll have the boards built by the end of next week and I'll post some details then.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to michaelkellett

    Thanks for the great explanation michael. Found this really helpful.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to michaelkellett

    Thanks for the great explanation michael. Found this really helpful.