Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Trouble copying part to l ibrary
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 187 subscribers
  • Views 789 views
  • Users 0 members are here
Related

Trouble copying part to l ibrary

autodeskguest
autodeskguest over 10 years ago

I'm running Eagle 4.16r2 (am I the last one?).  I created a part and

mistakenly saved it to a new library.  I'd like to move or copy it to

another one.  I open the destination library then right-click on the part

to be copied and select Copy to Library from the popup menu.  The part

appears in the board window for the destination library, but when I try to

save the part I get an error, "Can't create backup copy of file [path and

name of the destination library]."  When I click OK I get a warning, "Can't

remove old version of ."  What am

I doing wrong?

 

I should also point out that while Eagle lists the new library (and part)

in the Library listing of the Control Panel, and I can add the part to a

schematic, the library doesn't appear on disk with the rest of the Eagle

libraries.  You can see http://i.imgur.com/mLUpFGr.jpg that Eagle is

looking in the right place for the library (flip digits.lbr), but it's not

showing up (it should be between fifo.lbr and fox-electronics.libr).

 

Thanks for your help.

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 10 years ago

    Am 06.09.2016 um 04:20 schrieb Karl Lautman:

    I'm running Eagle 4.16r2 (am I the last one?).  I created a part and

    mistakenly saved it to a new library.  I'd like to move or copy it to

    another one.  I open the destination library then right-click on the part

    to be copied and select Copy to Library from the popup menu.  The part

    appears in the board window for the destination library, but when I try to

    save the part I get an error, "Can't create backup copy of file [path and

    name of the destination library]."  When I click OK I get a warning, "Can't

    remove old version of ."  What am

    I doing wrong?

     

    I should also point out that while Eagle lists the new library (and part)

    in the Library listing of the Control Panel, and I can add the part to a

    schematic, the library doesn't appear on disk with the rest of the Eagle

    libraries.  You can see http://i.imgur.com/mLUpFGr.jpg that Eagle is

    looking in the right place for the library (flip digits.lbr), but it's not

    showing up (it should be between fifo.lbr and fox-electronics.libr).

     

    Thanks for your help.

     

     

    Some times new libraries do not appear in alphabetical order, so check

    ALL names.

    Do a "use *" (use all) and check if the library is accessible now.

    If you have access to the new library you can also export it as script

    to a destination eagle has access to.

    Open your destination library and import the script.

    Some of this should work.

     

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to autodeskguest

    Thanks for the suggestions, Joern and Rob.  The library with the new part

    shows up in Eagle but not in Windows Explorer (I'm running Win7 x64 Pro),

    so "use all" doesn't apply.  I exported it as a script and ran it within

    the destination library to produce the part, but got the same error as

    before when I tried to save it.  In fact, I recreated the part from scratch

    within the destination library (as I should have originally) and got the

    error when trying to save, so it looks like a problem with the destination

    library, which is write-enabled for all users. 

     

    This library contains all the parts I create myself so it's easy to back up

    everything I create.  I had to reinstall Eagle after a system crash several

    months ago and just copied the backed up library into the lib directory, so

    maybe that's part of the issue.  I can access it from within Eagle and add

    parts from it to a schematic, though, so it's not totally ruined.  I should

    point out that the library with the new part (not the destination library)

    appears with a lock icon on its name in the library list in the Use library

    dialog, but this doesn't stop me from using the part in it.

     

    Any other tips?

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to autodeskguest

    Am 06.09.2016 um 18:37 schrieb Karl Lautman:

    Thanks for the suggestions, Joern and Rob.  The library with the new part

    shows up in Eagle but not in Windows Explorer (I'm running Win7 x64 Pro),

    so "use all" doesn't apply.  I exported it as a script and ran it within

    the destination library to produce the part, but got the same error as

    before when I tried to save it.  In fact, I recreated the part from scratch

    within the destination library (as I should have originally) and got the

    error when trying to save, so it looks like a problem with the destination

    library, which is write-enabled for all users.

     

    This library contains all the parts I create myself so it's easy to back up

    everything I create.  I had to reinstall Eagle after a system crash several

    months ago and just copied the backed up library into the lib directory, so

    maybe that's part of the issue.  I can access it from within Eagle and add

    parts from it to a schematic, though, so it's not totally ruined.  I should

    point out that the library with the new part (not the destination library)

    appears with a lock icon on its name in the library list in the Use library

    dialog, but this doesn't stop me from using the part in it.

     

    Any other tips?

     

     

    Then it seems that Bob is right and it is a problem of the windows

    rights management.

    Do you have full access to the directories you use for all eagle files?

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to autodeskguest

    Try to start eagle as administrator

     

    That did it.  Thanks!

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 10 years ago in reply to autodeskguest

    Try to start eagle as administrator

     

    That did it.  Thanks!

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.