Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) How to search in schema tic?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 188 subscribers
  • Views 1296 views
  • Users 0 members are here
Related

How to search in schema tic?

Joop14
Joop14 over 10 years ago

I have a (system on a) module with 200 pins.

In the library, I divided these pins over 7 symbols in the device.

Those symbols are all in different schematic sheets. There are 15 sheets

so it's impossible to remember where is what.

 

Sometimes I need to find a certain pin of this module but I don't remember

on

which sheet it is.

My question is, is there a way to find out? I tried "run find" but it

doesn't offer what I'm looking for.

 

Thanks.

 

 

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
  • Joop14
    Joop14 over 10 years ago

    Well, that looks like the usual problem with Eagle.

    Every new version brakes one or more ulp's and, even after reporting,

    they keep on shipping them with newer versions.

     

    If you ask for a feature, they point you to a ulp.

    If you complain about a broken ulp, it has no priority because it's not

    part of the (core) Eagle program.

     

    Then there's another thing. I have difficulties reading other people's

    code.

    For me, it's usually faster to write something new from scratch instead of

    patching something

    existing.

     

    Thanks for helping.

     

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to autodeskguest

    On 12.09.2016 13:46, Morten Leikvoll wrote:

    On 12.09.2016 12:50, Joop wrote:

    Morten Leikvoll wrote on Mon, 12 September 2016 10:16

    I use "run find pad <padname>".

     

    That doesn't work for me:

     

    /data/novazembla/Eagle-660/ulp/find.ulp(1138):

     

    Multiple contacts on pin, use contacts() instead

     

    Ah! I remember that bug. It should have been fixed in lastest beta, but

    if you look back in some old posts (by me), the bugfix to the find.ulp

    script is posted there.

    The problem was the ulp was not updated after eagle started to support

    symbols with merged pads.

     

     

    Just to help you out, this was posted back in April, after initially

    pointing at the bug in Dec 2015.

    -


    Since this is a very easy fix and hasnt been fixed on 7.5.3 beta, I will

    help you:

     

     

    On line 1138,1139 of the original find.ulp:

    1138:if (P.contact) {

    1139:if (P.contact.name == Find) {

     

    Replace this with:

    1138:P.contacts(C) {

    1139:if (C.name == Find) {

     

     

    And this will work also with symbols having multiple pads assigned to a pin.

    -


     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to Joop14

    On 12.09.2016 12:50, Joop wrote:

    Morten Leikvoll wrote on Mon, 12 September 2016 10:16

    I use "run find pad <padname>".

     

    That doesn't work for me:

     

    /data/novazembla/Eagle-660/ulp/find.ulp(1138):

     

    Multiple contacts on pin, use contacts() instead

     

    Ah! I remember that bug. It should have been fixed in lastest beta, but

    if you look back in some old posts (by me), the bugfix to the find.ulp

    script is posted there.

    The problem was the ulp was not updated after eagle started to support

    symbols with merged pads.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Joop14
    Joop14 over 10 years ago in reply to autodeskguest

    Morten Leikvoll wrote on Mon, 12 September 2016 10:16

    I use "run find pad <padname>".

     

     

    That doesn't work for me:

     

    /data/novazembla/Eagle-660/ulp/find.ulp(1138):

     

    Multiple contacts on pin, use contacts() instead

     

     

    Morten Leikvoll wrote on Mon, 12 September 2016 10:16

    You can also use "run find pin <pinname>" if you know the symbol pin

    name,

     

     

    I don't know that, that's the problem.

    Also, it's impossible for an algorithm to find the right pin if you don't

    provide

    at least two parameters. How else to solve the problem when two instances

    have the same pad name?

     

    Anyway, it's solved now, my new ulp works fine.

     

    Thanks to everybody for helping.

     

     

     

     

     

     

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago

    On 09.09.2016 19:35, Joop wrote:

    I have a (system on a) module with 200 pins.

    In the library, I divided these pins over 7 symbols in the device.

    Those symbols are all in different schematic sheets. There are 15 sheets

    so it's impossible to remember where is what.

     

    Sometimes I need to find a certain pin of this module but I don't remember

    on

    which sheet it is.

    My question is, is there a way to find out? I tried "run find" but it

    doesn't offer what I'm looking for.

     

    I use "run find pad " if you know the symbol pin

    name, but you also have to include an optional hidden @ extension in

    this name. Maybe the find ulp should be modified to ignore this extension.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Joop14
    Joop14 over 10 years ago

    Done. I wrote myself an ulp that searches in the schematic for a certain

    pin.

    It requires two parameters, a part number (e.g. IC308) and a pad name.

    If the combination of the two parameters exists, it opens that sheet,

    centers to the pin, zooms in and highlights the net connected to that pin.

    Works like a charm.

     

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Joop14
    Joop14 over 10 years ago in reply to autodeskguest

    Rob Pearce wrote on Sat, 10 September 2016 17:49

    On 10/09/16 13:12, Joop wrote:

     

    In other words, the contact member, as opposed to the contacts()

    iterator, only makes sense in the context of a single pad being

    connected to a pin. This used to be the rule - if you wanted more than

    one GND pad on a package then either the device needed multiple

    symbols

    with a GND pin or the symbol needed pins called GND@1, GND@2 etc.

    Newer

    versions of Eagle allow multiple package pads to be assigned to the

    same

    symbol pin, which has a number of benefits for components that, for

    example, have four GND pins in SO8 but only one in TO-92. However, it

    breaks the "contact" data member in ULPs.

     

     

    I understand. The thing is, I didn't read carefully so I didn't notice

    that

    "contact" and "contacts()" where different things... my mistake.

     

    With the contacts() iterator I should be able to write an ulp that does

    what I what.

     

    Thanks for pointing out.

     

     

     

     

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Joop14
    Joop14 over 10 years ago in reply to autodeskguest

    Rob Pearce wrote on Sat, 10 September 2016 17:49

    On 10/09/16 13:12, Joop wrote:

     

    In other words, the contact member, as opposed to the contacts()

    iterator, only makes sense in the context of a single pad being

    connected to a pin. This used to be the rule - if you wanted more than

    one GND pad on a package then either the device needed multiple

    symbols

    with a GND pin or the symbol needed pins called GND@1, GND@2 etc.

    Newer

    versions of Eagle allow multiple package pads to be assigned to the

    same

    symbol pin, which has a number of benefits for components that, for

    example, have four GND pins in SO8 but only one in TO-92. However, it

    breaks the "contact" data member in ULPs.

     

     

    I understand. The thing is, I didn't read carefully so I didn't notice

    that

    "contact" and "contacts()" where different things... my mistake.

     

    With the contacts() iterator I should be able to write an ulp that does

    what I what.

     

    Thanks for pointing out.

     

     

     

     

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to Joop14

    On 10/09/16 13:12, Joop wrote:

    The question arises, why is that data member deprecated??

     

    Am I overlooking something?

     

     

    I think the answer to that lies in:

     

    From the manual:

     

    It will work for backwards

    compatibility and as long as only one pad has been connected to the pin,

    but will cause

    a runtime error when used with a pin that is connected to more than one

    pad.

     

    In other words, the contact member, as opposed to the contacts()

    iterator, only makes sense in the context of a single pad being

    connected to a pin. This used to be the rule - if you wanted more than

    one GND pad on a package then either the device needed multiple symbols

    with a GND pin or the symbol needed pins called GND@1, GND@2 etc. Newer

    versions of Eagle allow multiple package pads to be assigned to the same

    symbol pin, which has a number of benefits for components that, for

    example, have four GND pins in SO8 but only one in TO-92. However, it

    breaks the "contact" data member in ULPs.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Joop14
    Joop14 over 10 years ago in reply to autodeskguest

    Joern Paschedag wrote on Sat, 10 September 2016 10:38

    Try INVOKE (device name) for example and you get a list of pages the

    device is on.

     

     

    Thank you Joern, unfortunately it doesn't help much.

     

    It doesn't show me on which sheet I'll find the pin I'm looking for.

     

    I guess the problem is that, in order to write an ulp that can find the pin

    in the schematic,

    based on the pin-number of the package which can be made visible in the

    board editor,

    one must use the deprecated data member "contact" in the object "UL_PIN".

     

    The question arises, why is that data member deprecated??

     

    Am I overlooking something?

     

    Thanks.

     

    From the manual:

     

    Note

    The contacts() loop member loops through the contacts that have been

    assigned to the

    pin through a CONNECT command. This only makes sense in a UL_DEVICE context

    (in

    other cases the loop is empty).

    The contact data member returns the contact that has been assigned to the

    pin through a

    CONNECT command. This member is deprecated! It will work for backwards

    compatibility and as long as only one pad has been connected to the pin,

    but will cause

    a runtime error when used with a pin that is connected to more than one

    pad.

     

     

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    Attachments:
    image
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>