Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) How to search in schema tic?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 188 subscribers
  • Views 1299 views
  • Users 0 members are here
Related

How to search in schema tic?

Joop14
Joop14 over 10 years ago

I have a (system on a) module with 200 pins.

In the library, I divided these pins over 7 symbols in the device.

Those symbols are all in different schematic sheets. There are 15 sheets

so it's impossible to remember where is what.

 

Sometimes I need to find a certain pin of this module but I don't remember

on

which sheet it is.

My question is, is there a way to find out? I tried "run find" but it

doesn't offer what I'm looking for.

 

Thanks.

 

 

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 10 years ago

    Am 09.09.2016 um 19:35 schrieb Joop:

    I have a (system on a) module with 200 pins.

    In the library, I divided these pins over 7 symbols in the device.

    Those symbols are all in different schematic sheets. There are 15 sheets

    so it's impossible to remember where is what.

     

    Sometimes I need to find a certain pin of this module but I don't remember

    on

    which sheet it is.

    My question is, is there a way to find out? I tried "run find" but it

    doesn't offer what I'm looking for.

     

    Thanks.

     

     

     

    Try INVOKE (device name) for example and you get a list of pages the

    device is on.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Joop14
    Joop14 over 10 years ago in reply to autodeskguest

    Joern Paschedag wrote on Sat, 10 September 2016 10:38

    Try INVOKE (device name) for example and you get a list of pages the

    device is on.

     

     

    Thank you Joern, unfortunately it doesn't help much.

     

    It doesn't show me on which sheet I'll find the pin I'm looking for.

     

    I guess the problem is that, in order to write an ulp that can find the pin

    in the schematic,

    based on the pin-number of the package which can be made visible in the

    board editor,

    one must use the deprecated data member "contact" in the object "UL_PIN".

     

    The question arises, why is that data member deprecated??

     

    Am I overlooking something?

     

    Thanks.

     

    From the manual:

     

    Note

    The contacts() loop member loops through the contacts that have been

    assigned to the

    pin through a CONNECT command. This only makes sense in a UL_DEVICE context

    (in

    other cases the loop is empty).

    The contact data member returns the contact that has been assigned to the

    pin through a

    CONNECT command. This member is deprecated! It will work for backwards

    compatibility and as long as only one pad has been connected to the pin,

    but will cause

    a runtime error when used with a pin that is connected to more than one

    pad.

     

     

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    Attachments:
    image
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Joop14
    Joop14 over 10 years ago in reply to autodeskguest

    Joern Paschedag wrote on Sat, 10 September 2016 10:38

    Try INVOKE (device name) for example and you get a list of pages the

    device is on.

     

     

    Thank you Joern, unfortunately it doesn't help much.

     

    It doesn't show me on which sheet I'll find the pin I'm looking for.

     

    I guess the problem is that, in order to write an ulp that can find the pin

    in the schematic,

    based on the pin-number of the package which can be made visible in the

    board editor,

    one must use the deprecated data member "contact" in the object "UL_PIN".

     

    The question arises, why is that data member deprecated??

     

    Am I overlooking something?

     

    Thanks.

     

    From the manual:

     

    Note

    The contacts() loop member loops through the contacts that have been

    assigned to the

    pin through a CONNECT command. This only makes sense in a UL_DEVICE context

    (in

    other cases the loop is empty).

    The contact data member returns the contact that has been assigned to the

    pin through a

    CONNECT command. This member is deprecated! It will work for backwards

    compatibility and as long as only one pad has been connected to the pin,

    but will cause

    a runtime error when used with a pin that is connected to more than one

    pad.

     

     

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    Attachments:
    image
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Joop14
    Joop14 over 10 years ago in reply to autodeskguest

    Rob Pearce wrote on Sat, 10 September 2016 17:49

    On 10/09/16 13:12, Joop wrote:

     

    In other words, the contact member, as opposed to the contacts()

    iterator, only makes sense in the context of a single pad being

    connected to a pin. This used to be the rule - if you wanted more than

    one GND pad on a package then either the device needed multiple

    symbols

    with a GND pin or the symbol needed pins called GND@1, GND@2 etc.

    Newer

    versions of Eagle allow multiple package pads to be assigned to the

    same

    symbol pin, which has a number of benefits for components that, for

    example, have four GND pins in SO8 but only one in TO-92. However, it

    breaks the "contact" data member in ULPs.

     

     

    I understand. The thing is, I didn't read carefully so I didn't notice

    that

    "contact" and "contacts()" where different things... my mistake.

     

    With the contacts() iterator I should be able to write an ulp that does

    what I what.

     

    Thanks for pointing out.

     

     

     

     

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Joop14
    Joop14 over 10 years ago in reply to autodeskguest

    Rob Pearce wrote on Sat, 10 September 2016 17:49

    On 10/09/16 13:12, Joop wrote:

     

    In other words, the contact member, as opposed to the contacts()

    iterator, only makes sense in the context of a single pad being

    connected to a pin. This used to be the rule - if you wanted more than

    one GND pad on a package then either the device needed multiple

    symbols

    with a GND pin or the symbol needed pins called GND@1, GND@2 etc.

    Newer

    versions of Eagle allow multiple package pads to be assigned to the

    same

    symbol pin, which has a number of benefits for components that, for

    example, have four GND pins in SO8 but only one in TO-92. However, it

    breaks the "contact" data member in ULPs.

     

     

    I understand. The thing is, I didn't read carefully so I didn't notice

    that

    "contact" and "contacts()" where different things... my mistake.

     

    With the contacts() iterator I should be able to write an ulp that does

    what I what.

     

    Thanks for pointing out.

     

     

     

     

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to Joop14

    On 10/09/16 13:12, Joop wrote:

    The question arises, why is that data member deprecated??

     

    Am I overlooking something?

     

     

    I think the answer to that lies in:

     

    From the manual:

     

    It will work for backwards

    compatibility and as long as only one pad has been connected to the pin,

    but will cause

    a runtime error when used with a pin that is connected to more than one

    pad.

     

    In other words, the contact member, as opposed to the contacts()

    iterator, only makes sense in the context of a single pad being

    connected to a pin. This used to be the rule - if you wanted more than

    one GND pad on a package then either the device needed multiple symbols

    with a GND pin or the symbol needed pins called GND@1, GND@2 etc. Newer

    versions of Eagle allow multiple package pads to be assigned to the same

    symbol pin, which has a number of benefits for components that, for

    example, have four GND pins in SO8 but only one in TO-92. However, it

    breaks the "contact" data member in ULPs.