Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Why do I need to draw the same symbol N times?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 189 subscribers
  • Views 2818 views
  • Users 0 members are here
Related

Why do I need to draw the same symbol N times?

autodeskguest
autodeskguest over 10 years ago

More often than not the same chip is available in different packages,

quite often with different number of pins and the packages with fewer

pins omit some of the lesser used signals.

 

Currently, you need to create a different symbol for every package: if

you have a chip that comes in 5 different packages, with a few pin

differences, you need a symbol drawn for ABC1234-SOIC, ABC1234-BGA,

ABC1234-TSOP and so on. It's the same damn chip, just on some packages

some pins are missing.

 

I wonder if I'm alone with the wish of having just one symbol, with

every possible signal drawn. Then, when it gets placed to the schematic

with a package selected, the not bonded pins grey out and don't allow

wires to be connected to them?

--

Zoltán Kócsi

Bendor Research Pty. Ltd.

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 10 years ago

    On Fri, 23 Sep 2016 08:47:48 +0200

    Morten Leikvoll <mleikvol@yahoo.nospam> wrote:

     

    You dont need to redraw the symbol. You just create a new component

    and add the symbol + all the packages that work with this symbol at

    the same component, then connect them correctly. This works, even if

    some packages have more gnd/shield pins, cause every package is

    connected separately.

     

    As Rik Steenwinkel pointed out, that doesn't work with very many chips.

    Microcontrollers, FPGAs, power supply chips being ominous examples.

    Micros more often than not drop/gain a few port pins between package

    variants. FPGAs ditto. Power supply chips often drop rarely used

    feature pins. SPI FLASH chips tend to have a 'BUSY' signal on the higher

    pincount package, which is dropped if you go to the smallest

    pincount/footprint one. So the list is quite long.

     

    In my original post I was specifically talking about packages with

    different pin counts and signal pins going missing in the smaller

    package.

     

    But currently (7.x), if the symbol differs slightly betweeen

    packages, you have to copy/make a new symbol, and add/remove pins.

     

    Exactly. As it has always been the case. Hence my request: I'd like to

    draw only one symbol and assign a package, even if the symbol has

    more pins than the package. Then the schematics could grey out or even

    completely hide the pins that are not available on the package.

     

    In the software world copy-paste-massage-ing code is one of the cardinal

    sins, and rightly so, why am I forced to do it with my hardware?

    --

    Zoltán Kócsi

    Bendor Research Pty. Ltd.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to autodeskguest

    zoltan wrote on Sun, 25 September 2016 01:53

    Hence my request: I'd like to

    draw only one symbol and assign a package, even if the symbol has

    more pins than the package. Then the schematics could grey out or even

    completely hide the pins that are not available on the package.

     

     

    By the time you specify which pins should be greyed out, you might as well

    have made the minor modifications from the symbol with a little more or

    little less pins.  If you're only changing a few pins, there isn't really a

    problem to solve here.

     

    You don't want Eagle to just assume that you intentionally used a symbol

    with too many pins and not show you the remaining ones.  That would

    circumvent useful error checking.  Also, if a different chip has fewer

    pins, you most likely want to draw the symbol differently.  You may want to

    make it a little smaller, change some of the labeling inside the symbol,

    etc.

     

    A good example is a voltage regulator.  The simple 3-pin variety can be

    drawn more simply and smaller than one with a shutdown input, for example.

    I wouldn't want the simple 3-pin version burdened with a greyed out

    shutdown input.  I also wouldn't want it drawn bigger with inexplicable

    extra space in the 3-pin usage case.

     

    If the symbols are similar except for a few pins, then there isn't really a

    problem here.  Copy and edit works fine.  If the symbols are substantially

    different, then you're going to have to do some work for each case one way

    or the other.

     

    Quote:

    In the software world copy-paste-massage-ing code is one of the

    cardinal

    sins, and rightly so,

     

     

    Exactly.  This is the same thing.  Just like with software, you copy and

    paste, then make a few minor edits to adapt to details of the situation.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to autodeskguest

    On Sun, 25 Sep 2016 17:32:32 -0400

    Olin Lathrop <eagle9304@embedinc.com> wrote:

     

    By the time you specify which pins should be greyed out, you might as

     

    Um, all of them which I did not assign to a package pin? What else

    should I specify in some time-consuming manner?

     

    You don't want Eagle to just assume that you intentionally used a

    symbol with too many pins and not show you the remaining ones. That

    would circumvent useful error checking.

     

    So, maybe a message box asking me whether I really want to assign this

    package to this chip could be a good solution?

     

    Also, if a different chip

    has fewer pins, you most likely want to draw the symbol differently.

     

    Most definitely not, especially not for microcontrollers or FPGAs or

    anything with 20 or 50 or 100 or 200 or more pins of which a few

    percentage may or may not be present on any particular package variant.

    It is not a different chip, it is the same chip, except that some of

    its pins on the silicon are not connected to package pins.

     

    A good example is a voltage regulator.  The simple 3-pin variety can

    be drawn more simply and smaller than one with a shutdown input, for

    example. I wouldn't want the simple 3-pin version burdened with a

    greyed out shutdown input.  I also wouldn't want it drawn bigger with

    inexplicable extra space in the 3-pin usage case.

     

    And how about the 24-pin variety (a switch mode), which is also

    available in a 21 pin variety, being exactly the same except that a

    normally left open pin, only used for synchronising multiple chips, is

    not available (the other 3 missing pins are the ground pins, which are

    now all on the central tab under the chip)?

     

    Quote:

    In the software world copy-paste-massage-ing code is one of the

    cardinal

    sins, and rightly so,

     

    Exactly.  This is the same thing.  Just like with software, you copy

    and paste, then make a few minor edits to adapt to details of the

    situation.

     

    I don't think you understood what you quoted and said 'Exactly' to.

    Cardinal sin means something that one should never, ever do. It has

    religious origins, the 'cardinal sins' are the '7 deadly sins' of

    Christianity, like murder. Copy-paste-massage is known to be the source

    of bugs too numerous to mention and is generally considered a very bad

    way of doing software.

    --

    Zoltán Kócsi

    Bendor Research Pty. Ltd.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 10 years ago in reply to autodeskguest

    On Sun, 25 Sep 2016 17:32:32 -0400

    Olin Lathrop <eagle9304@embedinc.com> wrote:

     

    By the time you specify which pins should be greyed out, you might as

     

    Um, all of them which I did not assign to a package pin? What else

    should I specify in some time-consuming manner?

     

    You don't want Eagle to just assume that you intentionally used a

    symbol with too many pins and not show you the remaining ones. That

    would circumvent useful error checking.

     

    So, maybe a message box asking me whether I really want to assign this

    package to this chip could be a good solution?

     

    Also, if a different chip

    has fewer pins, you most likely want to draw the symbol differently.

     

    Most definitely not, especially not for microcontrollers or FPGAs or

    anything with 20 or 50 or 100 or 200 or more pins of which a few

    percentage may or may not be present on any particular package variant.

    It is not a different chip, it is the same chip, except that some of

    its pins on the silicon are not connected to package pins.

     

    A good example is a voltage regulator.  The simple 3-pin variety can

    be drawn more simply and smaller than one with a shutdown input, for

    example. I wouldn't want the simple 3-pin version burdened with a

    greyed out shutdown input.  I also wouldn't want it drawn bigger with

    inexplicable extra space in the 3-pin usage case.

     

    And how about the 24-pin variety (a switch mode), which is also

    available in a 21 pin variety, being exactly the same except that a

    normally left open pin, only used for synchronising multiple chips, is

    not available (the other 3 missing pins are the ground pins, which are

    now all on the central tab under the chip)?

     

    Quote:

    In the software world copy-paste-massage-ing code is one of the

    cardinal

    sins, and rightly so,

     

    Exactly.  This is the same thing.  Just like with software, you copy

    and paste, then make a few minor edits to adapt to details of the

    situation.

     

    I don't think you understood what you quoted and said 'Exactly' to.

    Cardinal sin means something that one should never, ever do. It has

    religious origins, the 'cardinal sins' are the '7 deadly sins' of

    Christianity, like murder. Copy-paste-massage is known to be the source

    of bugs too numerous to mention and is generally considered a very bad

    way of doing software.

    --

    Zoltán Kócsi

    Bendor Research Pty. Ltd.