Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Why do I need to draw the same symbol N times?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 189 subscribers
  • Views 2805 views
  • Users 0 members are here
Related

Why do I need to draw the same symbol N times?

autodeskguest
autodeskguest over 10 years ago

More often than not the same chip is available in different packages,

quite often with different number of pins and the packages with fewer

pins omit some of the lesser used signals.

 

Currently, you need to create a different symbol for every package: if

you have a chip that comes in 5 different packages, with a few pin

differences, you need a symbol drawn for ABC1234-SOIC, ABC1234-BGA,

ABC1234-TSOP and so on. It's the same damn chip, just on some packages

some pins are missing.

 

I wonder if I'm alone with the wish of having just one symbol, with

every possible signal drawn. Then, when it gets placed to the schematic

with a package selected, the not bonded pins grey out and don't allow

wires to be connected to them?

--

Zoltán Kócsi

Bendor Research Pty. Ltd.

 

 

  • Sign in to reply
  • Cancel
Parents
  • rachaelp
    rachaelp over 10 years ago

    zoltan wrote on Fri, 23 September 2016 05:29

    I wonder if I'm alone with the wish of having just one symbol, with

    every possible signal drawn. Then, when it gets placed to the

    schematic

    with a package selected, the not bonded pins grey out and don't allow

    wires to be connected to them?

     

     

    Morten Leikvoll wrote on Fri, 23 September 2016 07:47

    But currently (7.x), if the symbol differs slightly betweeen packages,

     

    you have to copy/make a new symbol, and add/remove pins. Sometimes it

    would have been nice if unconnected pins at the symbol were hidden at

    the schematics, if they are not user/connected to the chosen package.

     

     

    Yes I think this would be nice. For a lot of cases the existing system

    works fine but being able to have a single device which deals with the

    entire part in all its variants rather than having to have duplicate parts

    with slightly different symbols would be a big benefit in terms of having

    much tidier and easier to use libraries. I like the idea of greying out or

    hiding unconnected pins but sometimes that might not be enough as a variant

    can possibly change a pin function (i.e. it bonds the pin to another

    function internally). For this reason I think being able to specify

    alternative symbols within the device as well as alternative packages would

    be a big benefit too.

     

    Best Regards,

     

    Rachael

     

     

     

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to rachaelp

    Hi All,

     

    This is definitely a pretty split topic it would be hard to make a

    suggestion either way.

     

    To answer the original question, the way I would handle this is a I

    would create one symbol which would represent the smallest( the one with

    the fewest pads) of the packages.

     

    I would create a device for the smallest package using just that symbol.

     

    Let's say that the next package up has 4 extra pins. I would create a

    new symbol with just those 4 pins. When I go to make the device for this

    package, I would add this symbol plus the symbol with the 4 extra pins.

     

    Repeat this for as many packages as necessary. Basically, instead of

    subtracting pins from the largest package configuration, we add pins to

    the lowest. You can adjust the add levels to make the two symbols come

    in together.

     

    I don't like the idea of greying out pins in the schematic or x-ing them

    out in some way. I think it makes the schematic untidy and adds

    unnecessary additional info.

     

    hth,

    Jorge Garica

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to autodeskguest

    On 27.09.2016 18:36, Jorge Garcia wrote:

    Hi All,

     

    This is definitely a pretty split topic it would be hard to make a

    suggestion either way.

     

    To answer the original question, the way I would handle this is a I

    would create one symbol which would represent the smallest( the one with

    the fewest pads) of the packages.

     

    I would create a device for the smallest package using just that symbol.

     

    Let's say that the next package up has 4 extra pins. I would create a

    new symbol with just those 4 pins. When I go to make the device for this

    package, I would add this symbol plus the symbol with the 4 extra pins.

     

    Repeat this for as many packages as necessary. Basically, instead of

    subtracting pins from the largest package configuration, we add pins to

    the lowest. You can adjust the add levels to make the two symbols come

    in together.

     

    I don't like the idea of greying out pins in the schematic or x-ing them

    out in some way. I think it makes the schematic untidy and adds

    unnecessary additional info.

     

    hth,

    Jorge Garica

     

     

     

    I don't want to suggest a complete solution for this, but rather throw

    in options.

     

    Devices may consist of several symbols, and maybe a symbol could

    be optional for each package. Like if a mcu/fpga or similar comes in

    packages without a set of IO, you can put that package specific IO in a

    separate symbol and connect it to those packages that has it. This would

    keep some of the symbol-package consistancy check that exist today.

     

    On the other hand, I'd like to see changes to pin directions wich has

    been discussed across several topics before. This includes the current

    problematic sup/pwr directions and an additional "project dependant

    programmable" directions (for fpga/mcu). I think this can be solved

    easily by introducing new io directions, and keep the current ones as is.

     

    Since I am a FPGA man, I'd also see the need for symbols to change

    visible pin text depending on usage. The symbols gets very large if you

    want to include every special function of a single pin. To give an

    example, for an Altera Arria10 fpga, in a 1517pin package, a single pin

    (G20) has one of these functions, depending on configuration/project usage:

    -PLL_2L_CLKOUT0p (lvds clock output from a pll, positive pin)

    -PLL_2L_CLKOUT0 (single end clock output from the above pll)

    -PLL_2L_FB0 (feedback input to the above pll)

    -LVDS2L_15p, with no soft CDR support, for dedicated LVDS high speed io.

    -DQ4 for a 4 bit DDR memory lane

    -DQ2 for a 8 bit DDR memory lane

    -DQ1 for a 16 bit DDR memory lane

    -DQ0 for a 32 bit DDR memory lane

    To further complicate this, the IO's may even have special functions

    before it is configured, so the function of the io in some design may be

    double.

     

    Now try to get all that into a single symbol. Of course that is not

    practical. This suggests the need for "symbol" configuration, and it

    will be needed pr pin. Also note that every project specific function

    have a assigned direction, wich would be nice if it could go into the

    ERC. But tbh, I think this is a bit far into the future, but nice to

    keep in mind when looking ahead.

     

    For now, I draw application specific symbols.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 10 years ago in reply to autodeskguest

    On 27.09.2016 18:36, Jorge Garcia wrote:

    Hi All,

     

    This is definitely a pretty split topic it would be hard to make a

    suggestion either way.

     

    To answer the original question, the way I would handle this is a I

    would create one symbol which would represent the smallest( the one with

    the fewest pads) of the packages.

     

    I would create a device for the smallest package using just that symbol.

     

    Let's say that the next package up has 4 extra pins. I would create a

    new symbol with just those 4 pins. When I go to make the device for this

    package, I would add this symbol plus the symbol with the 4 extra pins.

     

    Repeat this for as many packages as necessary. Basically, instead of

    subtracting pins from the largest package configuration, we add pins to

    the lowest. You can adjust the add levels to make the two symbols come

    in together.

     

    I don't like the idea of greying out pins in the schematic or x-ing them

    out in some way. I think it makes the schematic untidy and adds

    unnecessary additional info.

     

    hth,

    Jorge Garica

     

     

     

    I don't want to suggest a complete solution for this, but rather throw

    in options.

     

    Devices may consist of several symbols, and maybe a symbol could

    be optional for each package. Like if a mcu/fpga or similar comes in

    packages without a set of IO, you can put that package specific IO in a

    separate symbol and connect it to those packages that has it. This would

    keep some of the symbol-package consistancy check that exist today.

     

    On the other hand, I'd like to see changes to pin directions wich has

    been discussed across several topics before. This includes the current

    problematic sup/pwr directions and an additional "project dependant

    programmable" directions (for fpga/mcu). I think this can be solved

    easily by introducing new io directions, and keep the current ones as is.

     

    Since I am a FPGA man, I'd also see the need for symbols to change

    visible pin text depending on usage. The symbols gets very large if you

    want to include every special function of a single pin. To give an

    example, for an Altera Arria10 fpga, in a 1517pin package, a single pin

    (G20) has one of these functions, depending on configuration/project usage:

    -PLL_2L_CLKOUT0p (lvds clock output from a pll, positive pin)

    -PLL_2L_CLKOUT0 (single end clock output from the above pll)

    -PLL_2L_FB0 (feedback input to the above pll)

    -LVDS2L_15p, with no soft CDR support, for dedicated LVDS high speed io.

    -DQ4 for a 4 bit DDR memory lane

    -DQ2 for a 8 bit DDR memory lane

    -DQ1 for a 16 bit DDR memory lane

    -DQ0 for a 32 bit DDR memory lane

    To further complicate this, the IO's may even have special functions

    before it is configured, so the function of the io in some design may be

    double.

     

    Now try to get all that into a single symbol. Of course that is not

    practical. This suggests the need for "symbol" configuration, and it

    will be needed pr pin. Also note that every project specific function

    have a assigned direction, wich would be nice if it could go into the

    ERC. But tbh, I think this is a bit far into the future, but nice to

    keep in mind when looking ahead.

     

    For now, I draw application specific symbols.