Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Changing normal vias to b lind or burred vias
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 187 subscribers
  • Views 2210 views
  • Users 0 members are here
Related

Changing normal vias to b lind or burred vias

autodeskguest
autodeskguest over 10 years ago

I'm developing my first 4-layer board in v4.16.  My plan is to prototype it

with Osh Park before doing a pilot run with the final vendor.  For

aesthetic reasons (this is for a piece of functional sculpture), I'd like

the final version to use blind and, possibly, buried vias (so one side of

the PCB will be "unblemished"), but Osh only supports normal ones that go

all the way through.  It's not clear to me from the Eagle docs

 

1.  How to specify which type of via is created when routing on an internal

layer, or

 

2.  How to change a normal via to a blind or buried one later. 

 

Any tips on either or both of these issues appreciated.  I'm wondering how

big a chore it's going to be to go back and change all the normal vias for

the production version.

 

Thanks.

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 10 years ago

    On 23.09.2016 01:04, Karl Lautman wrote:

    I'm developing my first 4-layer board in v4.16.  My plan is to prototype it

    with Osh Park before doing a pilot run with the final vendor.  For

    aesthetic reasons (this is for a piece of functional sculpture), I'd like

    the final version to use blind and, possibly, buried vias (so one side of

    the PCB will be "unblemished"), but Osh only supports normal ones that go

    all the way through.  It's not clear to me from the Eagle docs

    1.  How to specify which type of via is created when routing on an internal

    layer, or

     

    2.  How to change a normal via to a blind or buried one later.

     

    Any tips on either or both of these issues appreciated.  I'm wondering how

    big a chore it's going to be to go back and change all the normal vias for

    the production version.

     

    Blind vias are vias you dont see, cause they are internal only, in your

    case between layer 2 and 3. They normally need microvias between L1-2

    and in your case, maybe between L3-4 too.

     

    I'm not sure if I understand you, but if you want it to be "free of

    holes", there are easier and cheaper ways than using blind vias.

     

    1-If there is nothing on the board but hole mounted components, you can

    just add two outer layers of nothing. A 6 layer board may be cheaper

    than what you are trying to do. You will also get some artistic freedom

    to draw art on the outer layers image

     

    2-Just fill the vias with solder.

     

    3-Stop filled holes, make the diameter as small as possible, and

    under DRC->Masks, set the "Limit" parameter larger than your via drill

    parameter to make eagle remove stop mask over them. Also talk to your

    manufacturer to make sure they can fill them. The end result will not be

    as flat as when using 2 or blind+microvias, but sufficient to keep

    dirt/humidity out.

     

    4-Copper filled vias. You need to find a manufacturer that can do that

    and actually talk to them about it. If your design has PAD's, you need

    to make your own CAM file to output VIAs in a separate file, so they

    don't fill your PADs too.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 10 years ago

    On 23.09.2016 01:04, Karl Lautman wrote:

    I'm developing my first 4-layer board in v4.16.  My plan is to prototype it

    with Osh Park before doing a pilot run with the final vendor.  For

    aesthetic reasons (this is for a piece of functional sculpture), I'd like

    the final version to use blind and, possibly, buried vias (so one side of

    the PCB will be "unblemished"), but Osh only supports normal ones that go

    all the way through.  It's not clear to me from the Eagle docs

    1.  How to specify which type of via is created when routing on an internal

    layer, or

     

    2.  How to change a normal via to a blind or buried one later.

     

    Any tips on either or both of these issues appreciated.  I'm wondering how

    big a chore it's going to be to go back and change all the normal vias for

    the production version.

     

    Blind vias are vias you dont see, cause they are internal only, in your

    case between layer 2 and 3. They normally need microvias between L1-2

    and in your case, maybe between L3-4 too.

     

    I'm not sure if I understand you, but if you want it to be "free of

    holes", there are easier and cheaper ways than using blind vias.

     

    1-If there is nothing on the board but hole mounted components, you can

    just add two outer layers of nothing. A 6 layer board may be cheaper

    than what you are trying to do. You will also get some artistic freedom

    to draw art on the outer layers image

     

    2-Just fill the vias with solder.

     

    3-Stop filled holes, make the diameter as small as possible, and

    under DRC->Masks, set the "Limit" parameter larger than your via drill

    parameter to make eagle remove stop mask over them. Also talk to your

    manufacturer to make sure they can fill them. The end result will not be

    as flat as when using 2 or blind+microvias, but sufficient to keep

    dirt/humidity out.

     

    4-Copper filled vias. You need to find a manufacturer that can do that

    and actually talk to them about it. If your design has PAD's, you need

    to make your own CAM file to output VIAs in a separate file, so they

    don't fill your PADs too.